Contents

Overview

A range test in wireless communications generally refers to the distance covered by a wireless link between a transmitter and a receiver, with acceptable packet loss and without breaking the link. The higher the operating frequency the lower the range will be, as high-frequency signals are more attenuated by free space than low-frequency signals are (e.g.: 2.4 GHz signals are attenuated more than Sub-1 GHz signals). So, if two signals (2.4 GHz and Sub-1 GHz) of the same Tx power are transmitted, the Sub-1 GHz signal (915 MHz or 868 MHz) will reach a longer distance than the 2.4 GHz signal. There is another factor that affects the range: antenna size. High-frequency signals (2.4 GHz) need a smaller antenna than lower-frequency signals (915 MHz) as the antenna size (e.g.: λ/4 for monopole antenna) is directly proportional to the wavelength of a signal and the wavelength is inversely proportional to the operating frequency. λ/4 is the required length for a monopole antenna to achieve long range. If a λ/10 size antenna is used for that application, the range will be reduced.

Next, the range of the same Tx & Rx differs based on the test environments (free space, office, industry, hospital, etc.) as there will be different obstacles that affect the signal strength by reflection, diffraction, and scattering; the range will be different for different environments. Here, we focused on two methods of measurement. The first one is based on a conducted test setup using cables and attenuators in between Tx and Rx DUTs placed within Gigahertz Transverse Electro Magnetic (GTEM) Cells. The communication link between the GTEM cell’s input port and Device Under Test (DUT) is radiated. The second one has been measured in an open area in a suburban environment, which is one of the real use cases.

Link budget measurement by GTEM cell

Test Setup

GTEM cells are used for link budget measurement including Antenna Gains (Tx & Rx)

Antenna Gain Test Setup

Sheilding Room

Back to top

RF Path Loss Description

Back to top

WLR089U and SAMR34 XPRO Settings

 915 MHz868 MHz
WLR089 XPro155 dB152 dB
SAMR34 XPro156 dB152 dB

Both WLR089 XPro and SAMR34 Xplained Pro have similar performance in the Link Budget measurement.

Back to top

Formula

Friis equation in decibel form:
PR (dB) =−20log(4πλ)−10nlog(d)+GT+GR+PT
Link budget = 20log(4πλ)+10nlog(d)+Fm

Fm= Fading margin, at least 15 dB
d=distance (in m), n=2.5 for open field
For 915 MHz and 868 MHz, 20log(4πλ) = ~32 dB

Back to top

Fm = 15 dB915 MHz868 MHz
WLR089 XPro20.9 km15.8 km
SAMR34 XPro22.9 km15.8 km
  1. Note that the calculated range from the link-budget is ideal, 1 dB difference in the link budget would not have a significant difference in the actual range. Thus, the performance of the WLR089U and SAMR34 XPro is similar.
  2. The UFL antenna used with the WLR089 XPro has a ~15 cm UFL cable, which introduces additional loss when compared to the SAMR34 XPro using an SMA antenna. So, it is expected for the WLR089U to have a slightly lower link budget.

Back to top

Better Range Projection by Real Range Measurement at 1.5 km

1.5 km RSSI test :

Read the average Received Signal Strength Indicator (RSSI) value in RX at a distance of 1.5 km from TX. Next, calculate the sensitivity margin to estimate the range. DUT is placed at a height of 1.5 m from the ground.

1.5Km Test Photograph

This is an extrapolated range estimation based on the measured RSSI value at 1.5 km. The actual range will vary based on the test environments.

Back to top

Recommended Range Test Setup

It is suggested to test in an open area with fewer to no obstacles between Tx and Rx.

Recomended Setup

Back to top

Tested Samples

Samples under Test

Back to top

Antenna Used in the Measurement

Used antenna in WLR089U:

Used antenna in SAMR34 XPro:

Back to top

Learn More

Back to top