The framework files are ready. Now we need to code the application.
The contents of the Microchip Web Demo are available in the dev_files\tcpip_test\ folder from the downloaded ZIP.
Run MPFS Generator Utility
The TCP/IP stack comes with a utility that converts the contents of a folder into a C file that will contain the code of the file system in the MCU flash.
The utility is called MPFS Generator and can be found in the Harmony installation in the net\utilities\mpfs_generator\ folder. Since the application is using the http_net module, the mpfs_net.jar utility should be used. The application is written in Java, so the Java Runtime Engine should be installed on the user’s machine.
In case there is no Java installation available, then the Java from the MPLAB® X IDE installation could be used in the command/terminal interface of the PC.
Navigate into the terminal at the MPFS generator utility location, e.g.:
Run the java with the command:
The application will open:
Update MPFS Generator Settings
The generator needs to be configured with the source and destination folders and the output type of the generated content. For this test, these will be:
After the generation ends, the following output windows will appear:
The pins used for LEDs and switches on the PIC32MZ EF Curiosity 2.0 board are automatically added by the PIC32MZ EF Curiosity BSP component. Those are:
LED4 – RGB LED:
LEDs:
SWITCHES:
Those are already defined by the BSP and the definitions are available in the bsp.h file generated by MCC Harmony. Open the file to familiarize yourself with it.
Test TCP/IP Application Code
The dev_files\tcpip_test\ folder contains a list of .c and .h files that need to be copied manually into your pic32mzef_web_photo_frame\firmware\src\ folder of the generated application. Overwrite the app.c, app.h and main.c files.
After this, the newly added files need to be manually added to the project.
Add Source files (.c)
Right-click on the logical folder called Source Files in your project and choose Add Existing Item.
Then point to the src\ folder of the project and add the .c files:
Adding Header files (.h)
Right-click on the logical folder called Header Files in your project and choose Add Existing Item.
Then point to the src\ folder in your project and add the .h files:
This is how it should look after adding the files.
Build and Program the Board
Connect USB to UART bridge
Place the USB I2C Click board™ from Mikroe into mikroBUS™ 2 slot and connect to the PC with a USB mini cable.
Connect Ethernet
Option 1: Using a Router
Place the KSZ8061 RMII Daughter Board into the ETHERNET PHY MODULE and connect with a CAT5/CAT6 Ethernet cable to a router. The PC should be connected to the same router.
This option was used while building this documentation.
Option 2: Direct connection with the PC
There is an option to have the board directly connected to the PC with an Ethernet Cable.
The static IP address default configuration is 192.168.100.10 and the netmask is 255.255.255.0. This is configured into the MAC instance of the NETCONFIG component (see NETCONFIG – Instance 0 for details).
The Ethernet port of the PC should be in the same address range with netmask 255.255.255.0. or example, 192.168.100.11.
Setup Terminal
Tera Term can be used as a terminal for the console.
Open Tera Term and connect the COM port where the USB I2C Click board resides. Set the Speed to 115200 baud.
Program the board
The PC should be connected to the board debugger using a micro USB cable from the PC to the DEBUG USB connector on the board (J700)
In the MPLAB X IDE toolbar, click the Make and Program Device Main Project button.
When the programming finishes, LED1 (red) should illuminate. After a bit of time, LED2 should illuminate and LED3 should blink.
In Tera Term the following should appear:
Verify Outcome
Open a browser and type the IP address that appeared in the console into the address bar.
The standard Microchip web server demo should start.
If all this happens, then the web server part of this application will work.
There are other changes to be made to the web server, but we will do this after we add the graphics part.