Bluetooth® Low Energy (BLE) Physical Layer
BLE/PHY
The Bluetooth® Low Energy (BLE) physical layer (PHY) contains the analog communications circuitry responsible for the translation of digital symbols over the air. It is the lowest layer of the protocol stack and provides its services to the link layer.

Frequency Bands
The radio uses the 2.4 GHz Industrial, Scientific, and Medical (ISM) band to communicate and divides this band into 40 channels on 2 MHz spacing from 2.4000 GHz to 2.4835 GHz, starting at 2402 MHz:

Channel Arrangement
The 40 channels are divided into three advertising channels (Ch. 37, 38, and 39), and 37 data channels (Ch. 0-36).
Advertising Channel Usage
- Device discovery
- Connection establishment
- Broadcast transmissions
Data Channel Usage
- Bidirectional communication between connected devices
- Adaptive frequency hopping used for subsequent connection events
Modulation and Data Rate
When transmitting data, the BLE radio transmits at 1 Mbps, with 1 bit per symbol. The radio is optimized for sending small chunks of data quickly.
BLE protocol overhead limits overall data throughput to significantly less than 1 Mbps.
The BLE radio uses Gaussian Frequency-Shift Keying (GFSK), whereby the data pulses are filtered with a Gaussian filter before being applied to alter the carrier frequency, in order to make the frequency transitions smoother.
Co-existence with 802.11/Wi-Fi®
Since the advertising channels form the basis for how BLE operates, they have been assigned center frequencies that minimize overlapping with the most common 802.11 channels, as shown: