Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Connect PIC18F47Q10 Curiosity Nano Board to Computer
Connect the USB Micro-B cable from the Curiosity Nano Base for Click Boards to the computer. MPLAB® X Integrated Development Environment (IDE) will use this connection to program and debug the MCU.
Verify Hardware Setup
Here’s how the setup should look after all connections have been made:
Install MCC
If needed, install MCC. We will use it to graphically create peripheral drivers for this tutorial.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.