Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Demonstrating 8-bit I2C Controller Read, Step 7: Create and Setup for ATmega4809
Last modified by Microchip on 2024/06/24 06:33
Connect ATmega4809 Curiosity Nano Board to Computer
Connect the USB Micro-B cable from the Curiosity Nano Base for Clicks board™ to the computer. MPLAB® X IDE will use this connection to program and debug the MCU.
Verify Hardware Setup
Here’s how the setup should look after all connections have been made:
Create Project
Create an MPLAB X IDE project for the ATmega4809 using the MPLAB XC8 compiler.
Information
Note: We’ll refer to your chosen project location as <your MPLAB X IDE project folder>.
You can refer to "Create a Standalone Project" if you would like detailed steps on how to create an MPLAB X IDE project.
Menu
Microchip Support
Query Microchip Forums and get your questions answered by our community:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.