Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Setup Instructions - Serial Terminal (Linux® PC)
Last modified by Microchip on 2026/03/30 10:15
To set up the serial terminal on a Linux® PC with picocom:
Identify the serial USB connection by monitoring the last lines of the dmesg command (may need sudo rights).
The /dev/ttyUSBx number will be used to configure the terminal emulator.
Assuming the serial USB interface is /dev/ttyUSB0, run the following command:
sudo picocom -b 115200/dev/ttyUSB0 (sudo rights may be needed)
Menu
Microchip Support
Query Microchip Forums and get your questions answered by our community:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.