Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Setup Instructions - Serial Terminal (Windows PC)
Last modified by Microchip on 2026/03/30 11:14
To set up the serial terminal on a Windows PC with PuTTY:
Open Windows Device Manager to identify the correct COM port.
Connect and disconnect the serial-to-USB dongle, and note which COMxx port appears and disappears (for example, COM10 is used in this guide; please use the COM port that matches your setup).
Open PuTTY and go to Category > Connection > Serial.
Configure the serial connection parameters as shown in the accompanying image, making sure to select the COM port that corresponds to your local setup.
Go to Terminal and enable the Implicit CR in every LF option.
Go to Category > Session and choose Serial for Connection type, then press Open.
Menu
Microchip Support
Query Microchip Forums and get your questions answered by our community:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.