SAM9X75 Curiosity
SoC Features
The SAM9X7 Series microprocessors are high-performance and cost-optimized Arm926EJ-S CPU-based embedded microprocessors (MPU) running up to 800 MHz. The devices integrate powerful peripherals for connectivity and user interface applications, including MIPI-DSI, LVDS, RGB and 2D graphics, MIPI-CSI-2 camera , Gigabit Ethernet with TSN and CAN-FD. Advanced security functions are offered, such as tamper detection, secure boot, secure key storage, TRNG, PUF as well as high-performance crypto accelerators for AES and SHA. The SAM9X7 Series is supported by Microchip MPLAB®-X development tools, Harmony, Linux® distributions and the Ensemble Graphics Toolkit.
Microchip offers for different supply configurations, fully tested power management solutions respecting the SAM9X7 power sequencing specifications that are referenced in the product specification.
Kit Information
Kit Overview
The SAM9X75-Curiosity documents can be found on microchip website, as following:
![]() |
Access the console
The usual serial communication parameters are 115200 8-N-1 :
| Baud rate | 115200 |
| Data | 8 bits |
| Parity | None |
| Stop | 1 bit |
| Flow control | None |
Access the console on DEBUG serial port
The serial console can be accessed from two connectors. One is from the DEBUG port with the help of a TTL-to-USB serial cable (marked as DEBUG J11), another is from micro-A USB connector that gives access to the on-board serial-to-USB converter (marked as J1 USB_A).
Using DEBUG on TTL-to-USB connector (DEBUG J11)
- For Microsoft Windows users: Install the driver of your USB TTL serial cable. FTDI-based ones are the most popular, have a look to this page to get the driver: https://www.ftdichip.com/Drivers/VCP.htm
- Be sure to connect a 3.3V compatible cable and identify its GND pin. Place it properly according to the silkscreen and connect the cable to the board (J11)
- Make sure the jumpers J14 and J15 are closed on the side marked as DBGU for the UART to work as Debug console.
- For Microsoft Windows users: Identify the USB connection that is established, USB Serial Port should appear in Device Manager. The COMxx number will be used to configure the terminal emulator.

- For Linux users: Identify the serial USB connection by monitoring the last lines of dmesg command. The /dev/ttyUSBx number will be used to configure the terminal emulator.A /dev/ttyUSB0 node has been created.[605576.562740] usb 1-1.1.2: new full-speed USB device number 17 using ehci-pci
[605576.660920] usb 1-1.1.2: New USB device found, idVendor=0403, idProduct=6001
[605576.660933] usb 1-1.1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[605576.660939] usb 1-1.1.2: Product: TTL232R-3V3
[605576.660944] usb 1-1.1.2: Manufacturer: FTDI
[605576.660958] usb 1-1.1.2: SerialNumber: FTGNVZ04
[605576.663092] ftdi_sio 1-1.1.2:1.0: FTDI USB Serial Device converter detected
[605576.663120] usb 1-1.1.2: Detected FT232RL [605576.663122] usb 1-1.1.2: Number of endpoints 2
[605576.663124] usb 1-1.1.2: Endpoint 1 MaxPacketSize 64
[605576.663126] usb 1-1.1.2: Endpoint 2 MaxPacketSize 64 [605576.663128] usb 1-1.1.2: Setting MaxPacketSize 64
[605576.663483] usb 1-1.1.2: FTDI USB Serial Device converter now attached to ttyUSB0
- Now open your favorite terminal emulator with appropriate settings
Demo
Demo archives
| Media type | Board | Features | Binary | Description |
|---|---|---|---|---|
| Yocto Project / Poky based demo | ||||
| NAND Flash | SAM9X75 CURIOSITY | Headless | linux4microchip-oecore-sam9x75_curiosity-headless-2025.10.zip (~ 165 MB) md5: 256874b8f5815215692bf22431cfee12 | Linux4SAM Yocto Project / Poky based demo compiled from tag linux4microchip-2025.10 Follow procedure: #Flash_the_demo |
| Graphics | linux4microchip-oecore-sam9x75_curiosity-graphics-2025.10.zip (~ 285 MB) md5: b366bb8a209ef05355ded2c30a097b39 | |||
| SD Card image | SAM9X75 CURIOSITY | Headless | linux4microchip-oecore-sam9x75_curiosity-headless-2025.10.img.bz2 (~ 125 MB) md5: b5030ba5031cd0348079cfedf43d07d4 | Linux4SAM Yocto Project / Poky based demo compiled from tag linux4microchip-2025.10 Follow procedure: #Create_a_SD_card_with_the_demo |
| Graphics | linux4microchip-oecore-sam9x75_curiosity-graphics-2025.10.img.bz2 (~ 229 MB) md5: 5e57946add67d149fe3d249fd97ff9ef | |||
| BuildRoot based demo | ||||
| NAND Flash | SAM9X75 CURIOSITY | Headless | linux4microchip-buildroot-sam9x75_curiosity-headless-2025.10.zip (~ 85 MB) md5: 3036282c36f4425ee0286cc91da5c931 | Linux4SAM BuildRoot based demo compiled from tag linux4microchip-2025.10 Follow procedure: #Flash_the_demo |
| Graphics | linux4microchip-buildroot-sam9x75_curiosity-graphics-2025.10.zip (~ 223 MB) md5: be86a9142c5956b4e65923a8248b45bf | |||
| SD Card image | SAM9X75 CURIOSITY | Headless | linux4microchip-buildroot-sam9x75_curiosity-headless-2025.10.img.bz2 (~ 68 MB) md5: a751619af5e569f3480ce487e67c7c93 | Linux4SAM BuildRoot based demo compiled from tag linux4microchip-2025.10 Follow procedure: #Create_a_SD_card_with_the_demo |
| Graphics | linux4microchip-buildroot-sam9x75_curiosity-graphics-2025.10.img.bz2 (~ 187 MB) md5: fffe3aa84e71a61cb015b6af274ea0dc | |||
You need a 1 GB (or larger) SD card and to download the image of the demo. The image is compressed to reduce the amount of data to download. This image contains:
- a FAT32 partition with the AT91Bootstrap, U-Boot and the Linux Kernel (zImage and dtb), and
- an EXT4 partition for the rootfs.
Multi-Platform Procedure
To write the compressed image on the SD card, you will have to download and install balenaEtcher. This open-source software tool is useful for obtaining a compressed image as input. Additional information and support can be found on the balenaEtcher website.
Insert your SD card and launch Etcher:
Select the demo image.
Select the device corresponding to your SD card (Etcher suggests the devices that are removable to avoid erasing your system disk).
Click on the Flash! button.
On Linux, Etcher finally asks you to enter your root password because it needs access to the hardware (your SD card reader or USB to SD card converter).
Then the flashing process begins followed by a verification phase (optional).

Once writing is done, Etcher asks you if you want to burn another demo image:

Flash the demo
Connect the USB to the board before launching SAM-BA
- Ensure SDCARD is not inserted
- Make sure that J8 NAND BOOT jumper is kept closed
- Press RESET = reset button to boot from on-chip Boot ROM
- For Microsoft Windows users: verify that the USB connection is well established
AT91 USB to Serial Converter should appear in Device Manager. If it shows a unknown device you need to download and install the driver: AT91SAM USB CDC driver
- For Linux users: check /dev/ttyACMx by monitoring the last lines of dmesg command:
- For Microsoft Windows users: verify that the USB connection is well established
[172677.792677] usb 2-1.4.4: not running at top speed; connect to a high speed hub
[172677.793418] usb 2-1.4.4: New USB device found, idVendor=03eb, idProduct=6124
[172677.793424] usb 2-1.4.4: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[172677.793897] cdc_acm 2-1.4.4:1.0: This device cannot do calls on its own. It is not a modem.
[172677.793924] cdc_acm 2-1.4.4:1.0: ttyACM0: USB ACM device
idVendor=03eb, idProduct=6124: from this message you can see it's Microchip board USB connection.
Run script to flash the demo
- download the demo package for the board. They are marked as "Media type: NAND Flash " in the table above
- extract the demo package
- run your usual terminal emulator and enter the demo directory
- make sure that the sam-ba application is in your Operating System path so that you can reach it from your demo package directory
- for Microsoft Windows users: Launch the demo_linux_nandflash.bat file
- for Linux users: Launch the demo_linux_nandflash.sh file
- this script runs SAM-BA 3 and the associated QML sam-ba script (demo_linux_nandflash_usb.qml) with proper parameters
- when you reach the end of the flashing process (this will take a few minutes), the following line is written:
-I- === Done. === - connect a serial link on DBGU and open the terminal emulator program as explained just above
- power cycle the board
- monitor the system while it's booting on the LCD screen or through the serial line
Build From source code
Setup ARM Cross Compiler
Download the Arm GNU toolchain:
Add the Arm GNU toolchain to your system:
export CROSS_COMPILE=`pwd`/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf/bin/arm-none-linux-gnueabihf-
or
export CROSS_COMPILE=arm-none-linux-gnueabihf-
export PATH=$PATH:/YOUR/PATH/TO/arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-linux-gnueabihf/bin/
If you already have an old Arm GNU toolchain, you need to clean up the PATH with:
Build AT91Bootstrap from sources
This section describes how to get source code from the git repository, how to configure with the default configuration, how to customize AT91Bootstrap based on the default configuration and finally to build AT91Bootstrap to produce the binary. take the default configuration to download U-Boot from NandFlash for example.
Get AT91Bootstrap Source Code
You can easily download AT91Bootstrap source code on the at91bootstrap git repository.
To get the source code, you should clone the repository by doing:
Cloning into 'at91bootstrap'...
remote: Enumerating objects: 17621, done.
remote: Counting objects: 100% (3324/3324), done.
remote: Compressing objects: 100% (1029/1029), done.
remote: Total 17621 (delta 2465), reused 3102 (delta 2285), pack-reused 14297
Receiving objects: 100% (17621/17621), 5.65 MiB | 4.65 MiB/s, done.
Resolving deltas: 100% (13459/13459), done.
$ cd at91bootstrap/
Configure AT91Bootstrap
Assuming you are at the AT91Bootstrap root directory, you will find a configs folder which contains several default configuration files:
sam9x75_curiositysd_uboot_defconfig
sam9x75_curiositydf_qspi_uboot_defconfig
You can configure AT91Bootstrap to load U-Boot binary from SD Card by doing:
$ make sam9x75_curiositysd_uboot_defconfig
If the configuring process is successful, the .config file can be found at AT91Bootstrap root directory.
Customize AT91Bootstrap
If the default configuration doesn't meet your need, after configuring with the default configuration, you can customize it by doing:
Now, in the menuconfig dialog, you can easily add or remove some features to/from AT91Bootstrap as the same way as kernel configuration.
Move to <Exit> with arrows and press this button hitting the Enter key to exit from this screen.
Build AT91Bootstrap
Then you can build the AT91Bootstrap binary by doing:
If the building process is successful, the final .bin image is build/binaries/at91bootstrap.bin.
Build U-Boot from sources
Getting U-Boot sources
Dedicated page on U-Boot wiki: http://www.denx.de/wiki/U-Boot/SourceCode
You can easily download U-Boot source code from Linux4Microchip GitHub U-Boot repository:
- clone the Linux4microchip GitHub U-Boot repository$ git clone https://github.com/linux4microchip/u-boot-mchp.git
Cloning into 'u-boot-mchp'...
remote: Enumerating objects: 951876, done.
remote: Counting objects: 100% (17718/17718), done.
remote: Compressing objects: 100% (5735/5735), done.
remote: Total 951876 (delta 12391), reused 15314 (delta 11846), pack-reused 934158
Receiving objects: 100% (951876/951876), 164.77 MiB | 401.00 KiB/s, done.
Resolving deltas: 100% (790362/790362), done.
$ cd u-boot-mchp/
- The source code has been taken from the master branch which is pointing to the latest branch we use. If you want to use the other branch, you can list them and use one of them by doing:$ git branch -r
origin/HEAD -> origin/master
origin/dev/tony/sama7g5ek_optee
origin/master
origin/sam9x60_curiosity_early
origin/sam9x60_early
origin/sam9x60_iar
origin/sam9x7_early
origin/sama5d27wlsom1ek_ear
origin/sama7g5_early
origin/u-boot-2012.10-at91
origin/u-boot-2013.07-at91
origin/u-boot-2014.07-at91
origin/u-boot-2015.01-at91
origin/u-boot-2016.01-at91
origin/u-boot-2016.03-at91
origin/u-boot-2017.03-at91
origin/u-boot-2018.07-at91
origin/u-boot-2019.04-at91
origin/u-boot-2020.01-at91
origin/u-boot-2021.04-at91
origin/u-boot-2022.01-at91
origin/u-boot-2023.07-mchp
origin/u-boot-2024.07-mchp
origin/uboot_5series_1.x
$ git checkout origin/u-boot-2024.07-mchp -b u-boot-2024.07-mchp
Branch 'u-boot-2024.07-mchp' set up to track remote branch 'u-boot-2024.07-mchp' from 'origin'.
Switched to a new branch 'u-boot-2024.07-mchp'
Cross-compiling U-Boot
Before compiling the U-Boot, you need setup cross compile toolchain in the Setup ARM Cross Compiler above.
Once the AT91 U-Boot sources available, cross-compile U-Boot is made in two steps: configuration and compiling. Check the Configuration chapter in U-Boot reference manual.
The U-Boot environment variables can be stored in different media, above config files can specify where to store the U-Boot environment.
sam9x75_curiosity_nandflash_defconfig
# To put environment variables in SD/MMC card:
sam9x75_curiosity_mmc_defconfig
Here are the building steps for the SAM9X75-Curiosity board:
make sam9x75_curiosity_mmc_defconfig
make
The result of these operations is a fresh U-Boot binary called u-boot.bin corresponding to the binary ELF file u-boot.
- u-boot.bin is the file you should store on the board
- u-boot is the ELF format binary file you may use to debug U-Boot through a JTag link for instance.
Build Kernel from sources
Required packages
You must install essential host packages on your build host. These requirements are listed in the Linux kernel documentation with the chapter Install build requirements. You must follow this process which includes, but not limited to, the following packages:
- build-essential
- flex
- bison
- git
- perl-base
- libssl-dev
- libncurses5-dev
- libncursesw5-dev
- ncurses-dev
Getting Kernel sources
To get the source code, you have to clone the repository:
Cloning into 'linux'...
remote: Enumerating objects: 8587836, done.
remote: Total 8587836 (delta 0), reused 0 (delta 0), pack-reused 8587836
Receiving objects: 100% (8587836/8587836), 3.49 GiB | 13.44 MiB/s, done.
Resolving deltas: 100% (7117887/7117887), done.
Updating files: 100% (70687/70687), done.
$ cd linux
The source code has been taken from the master branch which is pointing on the latest branch we use.
$ git remote update linux4microchip
Fetching linux4microchip
From https://github.com/linux4microchip/linux
* [new branch] linux-6.6-mchp -> linux4microchip/linux-6.6-mchp
* [new branch] linux-6.12-mchp -> linux4microchip/linux-6.12-mchp
* [new branch] master -> linux4microchip/master
If you want to use another branch, you can list them and use one of them by doing this:
linux4microchip/linux-6.1-mchp
linux4microchip/linux-6.1-mchp+fpga
linux4microchip/linux-6.6-mchp
linux4microchip/linux-6.6-mchp+fpga
linux4microchip/linux-6.12-mchp
linux4microchip/master
$ git checkout -b linux-6.12-mchp --track remotes/linux4microchip/linux-6.12-mchp
Branch linux-6.12-mchp set up to track remote branch linux-6.12-mchp from linux4microchip.
Switched to a new branch 'linux-6.12-mchp'
Setup ARM Cross Compiler
First step is to dowload the ARM GNU Toolchain:
wget -c https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
Next step is to add the ARM GNU Toolchain into your system:
tar -xf arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
export CROSS_COMPILE=`pwd`/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf/bin/arm-none-linux-gnueabihf-or
tar -xf arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
export CROSS_COMPILE=arm-none-linux-gnueabihf-
export PATH=$PATH:/YOUR/PATH/TO/arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-linux-gnueabihf/bin/- export PATH=${PATH/':/YOUR/PATH/TO/arm-gnu-toolchain-VERSION-x86_64-arm-none-linux-gnueabihf/bin/'/}
Configure and Build the Linux kernel
Now you have to configure the Linux kernel according to your hardware. We have two default configuration at91 SoC in arch/arm/configs
arch/arm/configs/at91_dt_defconfig
arch/arm/configs/sama5_defconfig
arch/arm/configs/sama7_defconfig- at91_dt_defconfig: for SAM9 (ARM926) series chips
- sama5_defconfig: for SAMA5 series chips
- sama7_defconfig: for SAMA7 series chips
You can add or remove some features in the menuconfig dialog. Once done, use the arrows to navigate to <Exit> and press this button with the Enter key to exit from this screen.
Build the Linux kernel image, but before you build, you need to set up the cross compile toolchain. Check the "Set Up Arm Cross Compiler" section.
[..]
Kernel: arch/arm/boot/Image is ready
Kernel: arch/arm/boot/zImage is ready
Now you have a usable compressed kernel image zImage.
If you need a uImage, you can run this additional step:
[..]
Kernel: arch/arm/boot/Image is ready
Kernel: arch/arm/boot/zImage is ready
UIMAGE arch/arm/boot/uImage
Image Name: Linux-6.12.22-linux4microchip-20
Created: Thu May 22 18:05:21 2025
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 5688984 Bytes = 5555.65 KiB = 5.43 MiB
Load Address: 20008000
Entry Point: 20008000
Kernel: arch/arm/boot/uImage is ready
[..]
DTC arch/arm/boot/dts/microchip/at91-sama5d27_som1_ek.dtb
DTC arch/arm/boot/dts/microchip/at91-sama5d27_wlsom1_ek.dtb
DTC arch/arm/boot/dts/microchip/at91-sama5d29_curiosity.dtb
DTC arch/arm/boot/dts/microchip/at91-sama5d2_icp.dtb
DTC arch/arm/boot/dts/microchip/at91-sama5d3_eds.dtb
DTC arch/arm/boot/dts/microchip/at91-sama7d65_curiosity.dtb
DTC arch/arm/boot/dts/microchip/at91-sama7g54_curiosity.dtb
DTC arch/arm/boot/dts/microchip/at91-sama7g5ek.dtb
[..]
If the building process is successful, the final images can be found under the arch/arm/boot/ directory.
Build Yocto Project rootfs from sources
Support for the Microchip MPU SoC family is included in a particular Yocto Project™ layer, meta-mchp. The source for this layer is hosted on the Linux4Microchip GitHub® account on the Microchip Yocto Project BSP page.
Building Environment
A step-by-step, comprehensive installation is explained on the "Yocto Project Quick Build" page. The following lines should be considered as an add-on that is MPU-specific, or that can facilitate your setup.
Step-by-Step Build Procedure
OpenEmbedded™/Yocto Project BSP Layer for Microchip's SoCs
- Description
- The meta-mchp-common layer consolidates common Board Support Package (BSP) components and metadata for Microchip platforms, streamlining development across various Microchip devices for use with OpenEmbedded and/or Yocto Project.
- Supported Machines
- The meta-mchp-common layer provides support for various Microchip platforms. For detailed information about supported machines, please refer to the documentation in the relevant sub-layers:
- Prerequisites
- Before starting, please refer to the "Required Packages for Build Host" section in the Yocto Project documentation to install the required dependencies for the build environment:
For instance, on Ubuntu or Debian, these packages need to be installed on your development host:
build-essential chrpath socat cpio python3 python3-pip python3-pexpect \
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
pylint3 xterm repo
Usage
- To integrate this layer into your Yocto Project build environment:
Clone the necessary repositories.
Create an empty directory to hold the workspace:
mkdir yocto-dev
cd yocto-devUse the repo tool to fetch all the required repositories.
repo init -u https://github.com/linux4microchip/meta-mchp-manifest.git -b <branch> -m <target>/default.xmlReplace and with the Yocto Project release branch and the manifest required. For example:
repo init -u https://github.com/linux4microchip/meta-mchp-manifest.git -b scarthgap -m mpu/default.xmlFetch all the required repositories using the following repo command:
repo syncInitialize the build environment.
The meta-mchp repository provides sample configuration templates that help set up BitBake™ layers and key configuration files in the Yocto Project build directory.
Set the TEMPLATECONF environment variable to point to the appropriate configuration template before initializing the build environment:
export TEMPLATECONF=${TEMPLATECONF:-../meta-mchp/<meta-layer>/conf/templates/default}Replace meta-layer above with the desired layer based on your target platform. For example:
export TEMPLATECONF=${TEMPLATECONF:-../meta-mchp/meta-mchp-mpu/meta-mchp-mpu-apps/conf/templates/default}Then initialize the Yocto Project build environment:
source openembedded-core/oe-init-build-envSet the target machine and build the image.
MACHINE=<machine> bitbake core-image-minimalEach sub-layer provides several images that include demos and applications tailored for its respective platform.
For more information on the supported images, please refer to the MPU layer README.
Layer Dependencies
This layer depends on the following layers:
- meta-openembedded
- URI: git://git.openembedded.org/meta-openembedded
- Layers: meta-oe, meta-networking, meta-python
- openembedded-core
- URI: git://git.openembedded.org/openembedded-core
- Layers: meta
For information on the specific revisions used, refer to the meta-mchp manifest repository.
- Licensing
- The contents of this layer are licensed under the MIT License. See COPYING.MIT for details.
- Contributing
- If you want to contribute changes, you can send GitHub pull requests.
Using SAM-BA to flash components to board
NAND Flash Demo - Memory Map

Install SAM-BA Software In Your PC
We maintain information about SAM-BA in the "SoftwareTools" page.
Launch SAM-BA tools
- According to the Connect the USB to the board before launching SAM-BA section of this page make sure that the chip can execute the SAM-BA Monitor.
In addition to the Qt® 5 QML language for scripting used for flashing the demos, the most common SAM-BA software actions can be done using the SAM-BA software command line.
For browsing information on the SAM-BA software command line usage, please see the command line documentation available in the SAM-BA software installation directory, doc/index.html or doc/cmdline.html.
SAM-BA software includes a command-line interface that provides support for the most common actions:
- Reading/writing to arbitrary memory addresses and/or peripherals
- Uploading applets and using them to erase/read/write external memories
The command line interface is designed to be self-documenting.
The main commands can be listed using the --help command:
Copyright 2025 Microchip Technology
Usage: sam-ba [options]
Options:
-v, --version Displays version information.
-h, --help Displays this help.
-l, --loglevel <log_level[:options:...]> Set verbose log level.
-x, --execute <script.qml> Execute script <script.qml>.
-p, --port <port[:options:...]> Communicate with device using
<port>.
-d, --device <device[:options:...]> Connected device is <device>.
-b, --board <board[:options:...]> Connected board is <board>.
-m, --monitor <command[:options:...]> Run monitor command <command>.
-a, --applet <applet[:options:...]> Load and initialize applet
<applet>.
-c, --command <command[:args:...]> Run command <command>.
-t, --tracelevel <trace_level> Set applet trace level to
<trace_level>.
-L, --applet-buffer-limit <SIZE> Set applet buffer limit to <SIZE>
bytes (default 131072).
-w, --working-directory <DIR> Set working directory to <DIR>.
-u, --utils <tool[:args:...]> Launch a tool <tool> .
If you get the following error, it indicates a symbol mismatch or unresolved symbol when the sam-ba executable is being loaded:
sam-ba: symbol lookup error: sam-ba: undefined symbol: _ZdlPvm, version Qt_5
Check for Qt libraries inside the extracted SAM-BA software directory.
$ export LD_LIBRARY_PATH=$(pwd)/lib:$LD_LIBRARY_PATH
Additional help can be obtained for most commands by supplying a "help" parameter that will display their usage.
For example, "sam-ba --port help" will display:
Commands that take an argument with options (port, monitor, applet) will display even more documentation when called with "help" as the option value.
For example, "sam-ba --port serial:help" will display:
serial:[<port>]:[<baudrate>]
Examples:
serial serial port (will use first AT91 USB if found otherwise first serial port)
serial:COM80 serial port on COM80
serial:ttyUSB0:57600 serial port on /dev/ttyUSB0, baudrate 57600
Configure NAND ECC
Using default PMECC parameters
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 12288 bytes (3 pages) at address 0x003085a0.
NAND header value is 0xc2605007.
Supported erase block sizes: 256KB
Executing command 'read:test.bin:0:1'
Read 1 bytes at address 0x00000000 (100.00%)
Connection closed.
You can figure out that the default PMECC parameter for this == board is 0xc2605007.
Initializing NAND ioSet1 Bus Width 8
PMECC configuration: 0xc2605007
Sector size: 512
Sectors per page: 8
Spare size: 256
ECC bits: 8
ECC offset: 152
ECC size: 104
PMECC enabled
Buffer Address: 0x003085a0
Buffer Size: 12288 bytes
NAND applet initialized successfully.
If you want to change the default PMECC parameters you can simply specify another value on the SAM-BA command line with the -a nandflash argument as shown below:
Syntax: nandflash:[<ioset>]:[<bus_width>]:[<header>]
Parameters:
ioset I/O set
bus_width NAND bus width (8/16)
header NAND header value
Examples:
nandflash use default board settings
nandflash:2:8:0xc0098da5 use fully custom settings (IOSET2, 8-bit bus, header is 0xc0098da5)
nandflash:::0xc0098da5 use default board settings but force header to 0xc0098da5
For information on NAND header values, please refer to SAMA5D4 datasheet section \"12.4.4 Detailed Memory Boot Procedures\".
By reading this in-line documentation we can specify the NAND PMECC parameter with this command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc2605007.
Supported erase block sizes: 256KB
Connection closed.
Programming components into NAND
Program AT91Bootstrap binary
Run SAM-BA with USB connection (equivalent to serial) and erase the beginning of the NAND flash and then write AT91Bootstrap binary:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc2605007.
Supported erase block sizes: 256KBt
Executing command 'erase::0x40000'
Erased 262144 bytes at address 0x00000000 (100.00%)
Executing command 'writeboot:at91bootstrap-.bin'
Prepended NAND header prefix (0xc1e04e07)
Appending 4008 bytes of padding to fill the last written page
Wrote 20480 bytes at address 0x00000000 (83.33%)
Wrote 4096 bytes at address 0x00005000 (100.00%)
Connection closed.
Program U-Boot binary
Run SAM-BA with USB connection (equivalent to serial) and erase the U-Boot section in the NAND flash memory map and then write U-Boot binary:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc2605007.
Supported erase block sizes: 256KB
Executing command 'erase:0x40000:0x80000'
Erased 262144 bytes at address 0x00040000 (50.00%)
Erased 262144 bytes at address 0x00080000 (100.00%)
Executing command 'write:u-boot-sam9x60-curiosity.bin:0x40000'
Appending 3137 bytes of padding to fill the last written page
Wrote 20480 bytes at address 0x00040000 (4.59%)
Wrote 20480 bytes at address 0x00045000 (9.17%)
Wrote 20480 bytes at address 0x0004a000 (13.76%)
[..]
Wrote 20480 bytes at address 0x00094000 (81.65%)
Wrote 20480 bytes at address 0x00099000 (86.24%)
Wrote 20480 bytes at address 0x0009e000 (90.83%)
Wrote 20480 bytes at address 0x000a3000 (95.41%)
Wrote 20480 bytes at address 0x000a8000 (100.00%)
Connection closed.
Recent FAQ
- Unable to build gst1-at91-gstreamer plug-in in Buildroot
- Crypto Hardware Acceleration
- Image Sensor Controller White balance features
- Capturing Images Using libcamera in Microchip Platforms
- Media Controller Pipeline For Image Acquisition and SAM MPU Products
- How to patch Device Tree Blob in U-boot using Overlays
- How to use Pulse Width Modulation driver
- Using the SAMA5D2-compatible ADC device
- SAMA7G5 Image Acquisition Pipeline
- SD card boot for AT91SAM SoC
- Using systemd
- U-Boot FAQ
- USB Gadget Configuration
- How to use the Atmel KMS/DRM LCD driver
- Using MaxTouch
- Using I2SC (Inter-IC Sound Controller)
- External Component on External Bus Interface