SAMA7D65-Curiosity

Last modified by Microchip on 2025/10/02 07:12

SoC Features

The SAMA7D65 MPU is a high-performance ARM Cortex-A7 CPU-based embedded MPU running up to 1GHz.

The board allows evaluation of powerful peripherals for connectivity, audio and user interface applications, including MIPI-DSI and LVDS w/ 2D graphics, dual Gigabit Ethernet w/ TSN and CAN-FD.

The MPUs offer advanced security functions, like tamper detection, secure boot, secure key stoarge, TRNG, PUF as well as higher-performance crypto accelerators for AES and SHA.

Kit Information

Kit Overview

The SAMA7D65-Curiosity documents can be found on microchip website, as following:

Kit Overview

sama7d65_curiosity_board_presentation.jpg

Access the console

Access the console on DEBUG serial port

The serial console can be accessed from the DEBUG port with the help of a TTL-to-USB serial cable (marked as DEBUG J35).

sama7d65_uart_debug_J35.jpg

Using DEBUG on TTL-to-USB connector (DEBUG J35)

  • For Microsoft Windows users: Install the driver of your USB TTL serial cable.
  • Be sure to connect a 3.3V compatible cable and identify its GND pin. Place it properly according to the silkscreen and connect the cable to the board (J35)
  • For Microsoft Windows users: Identify the USB connection that is established, USB Serial Port should appear in Device Manager. The COMxx number will be used to configure the terminal emulator.
    USB serial line
  • For Linux users: Identify the serial USB connection by monitoring the last lines of dmesg command. The /dev/ttyUSBx number will be used to configure the terminal emulator.
    usb 1-1.1.2: new full-speed USB device number 17 using ehci-pci
    usb 1-1.1.2: New USB device found, idVendor=0403, idProduct=6001
    usb 1-1.1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
    usb 1-1.1.2: Product: TTL232R-3V3
    usb 1-1.1.2: Manufacturer: FTDI
    usb 1-1.1.2: SerialNumber: FTGNVZ04
    ftdi_sio 1-1.1.2:1.0: FTDI USB Serial Device converter detected
    usb 1-1.1.2: Detected FT232RL
    usb 1-1.1.2: Number of endpoints 2
    usb 1-1.1.2: Endpoint 1 MaxPacketSize 64
    usb 1-1.1.2: Endpoint 2 MaxPacketSize 64
    usb 1-1.1.2: Setting MaxPacketSize 64
    usb 1-1.1.2: FTDI USB Serial Device converter now attached to ttyUSB0
    A /dev/ttyUSB0 node has been created.
  • Now open your favorite terminal emulator with appropriate settings

Demo

Demo archives

Media typeBoardFeaturesBinaryDescription
Yocto Project / Poky based demo
NAND FlashSAMA7D65 CuriosityHeadlesslinux4sam-oecore-sama7d65_curiosity-headless-2025.04.zip (~ 129 MB)
md5: 4e7f25559508f1ae3d4bf1de1160ddc3
Linux4SAM Yocto Project / Poky based demo
compiled from tag linux4microchip-2025.04
Follow procedure: #Flash_the_demo
Graphicslinux4sam-oecore-sama7d65_curiosity-graphics-2025.04.zip (~ 249 MB)
md5: d7248ef82f80b3c4e037029edb3bf788
SD Card imageSAMA7D65 CuriosityHeadlesslinux4sam-oecore-sama7d65_curiosity-headless-2025.04.img.bz2 (~ 99 MB)
md5: da0f0e4e8a44c8037a5f9df94d294e3a
Linux4SAM Yocto Project / Poky based demo
compiled from tag linux4microchip-2025.04
Follow procedure: #Create_a_SD_card_with_the_demo
Graphicslinux4sam-oecore-sama7d65_curiosity-graphics-2025.04.img.bz2 (~ 203 MB)
md5: ad9bb1df938517f760e8c5dc20125c58
BuildRoot based demo
SD Card imageSAMA7D65 CuriosityHeadlesslinux4sam-buildroot-sama7d65_curiosity-headless-sama7d65-2025.04.img.bz2 (~ 75 MB)
md5: 9685f448108ae45d090a4541a0c47482
Linux4SAM BuildRoot based demo
compiled from tag linux4microchip-2025.04
Follow procedure: #Create_a_SD_card_with_the_demo
Graphicslinux4sam-buildroot-sama7d65_curiosity-graphics-sama7d65-2025.04.img.bz2 (~ 184 MB)
md5: fee1ab53f78e95024c2e4ec5c709f96b

Create a SD card with the demo

You need a 1 GB (or larger) SD card and to download the image of the demo. The image is compressed to reduce the amount of data to download. This image contains:

  • a FAT32 partition with the AT91Bootstrap, U-Boot and the Linux Kernel (zImage and dtb), and
  • an EXT4 partition for the rootfs.

Multi-Platform Procedure

To write the compressed image on the SD card, you will have to download and install balenaEtcher. This open-source software tool is useful for obtaining a compressed image as input. Additional information and support can be found on the  balenaEtcher website

Insert your SD card and launch Etcher:
Etcher launch window


Select the demo image. They are marked as "SD Card image" in the demo table above.

Information

Note: You can select a compressed image (like the demos available here). The tool is able to decompress files on the fly.

 


Select the device corresponding to your SD card (Etcher suggests the devices that are removable to avoid erasing your system disk).


Click on the Flash! button.


On Linux, Etcher finally asks you to enter your root password because it needs access to the hardware (your SD card reader or USB to SD card converter).


Then the flashing process begins followed by a verification phase (optional).

flashing process


Once writing is done, Etcher asks you if you want to burn another demo image:

Flash complete

Information

Your SD card is ready!

 

Flash the demo

Warning

use SAM-BA 3.9.y onwards. You can download it here: SAM-BA 3.91 release page.

Run script to flash the demo

  • download the demo package for the board. They are marked as "Media type: NAND Flash " in the table above
  • extract the demo package
  • run your usual terminal emulator and enter the demo directory
  • make sure that the sam-ba application is in your Operating System path so that you can reach it from your demo package directory
  • for Microsoft Windows users: Launch the demo_linux_nandflash.bat file
  • for Linux users: Launch the demo_linux_nandflash.sh file
  • this script runs SAM-BA 3 and the associated QML sam-ba script (demo_linux_nandflash_usb.qml) with proper parameters
  • when you reach the end of the flashing process (this will take a few minutes), the following line is written:
    -I- === Done. === 
  • connect a serial link on DBGU and open the terminal emulator program as explained just above
  • power cycle the board
  • monitor the system while it's booting on the LCD screen or through the serial line

Run script to boot in emulation mode

  • Make sure the sd card is removed.
  • Jumper J36 NAND_BOOT should be closed.
  • Run the folowing script to boot the board in emulation mode.
  • Microsoft users: Run demo_linux_nandflash_emul.bat file
  • Linux users: Run demo_linux_nandflash_emul.sh file
  • The script writes the boot configuration packet and the board should boot from NAND flash.

Build From source code

Setup ARM Cross Compiler

  • First step is to dowload the ARM GNU Toolchain:
    wget -c https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
  • Next step is to add the ARM GNU Toolchain into your system:
    tar -xf arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
    export CROSS_COMPILE=`pwd`/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf/bin/arm-none-linux-gnueabihf-

    or

    tar -xf arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz
    export CROSS_COMPILE=arm-none-linux-gnueabihf-
    export PATH=$PATH:/YOUR/PATH/TO/arm-gnu-toolchain-13.2.Rel1-x86_64-arm-none-linux-gnueabihf/bin/
  • If you already have an old ARM GNU Toolchain you need to clean up the PATH with:

    export PATH=${PATH/':/YOUR/PATH/TO/arm-gnu-toolchain-VERSION-x86_64-arm-none-linux-gnueabihf/bin/'/}

Build AT91Bootstrap from sources

This section describes how to get source code from the git repository, how to configure with the default configuration, how to customize AT91Bootstrap based on the default configuration and finally to build AT91Bootstrap to produce the binary. take the default configuration to download U-Boot from !NandFlash for example.

SAM-BA tool

SAM-BA tool is required to add a header in at91bootstrap image (for both manual compilation and
through build-systems like Buildroot or Yocto Project). Download SAM-BA software with the following link:
https://github.com/atmelcorp/sam-ba/releases/tag/v3

Uncompress the tgz file in your workspace with:

$ tar xvzf sam-ba_v3.9.1-linux_x86_64.tar.gz

Make sure to add the sam-ba application to your $PATH and verify that you have the correct
version:

$ sam-ba -v
SAM-BA Command Line Interface Tool v3.9.1 (linux - x86_64-little_endian-lp64)
Copyright 2025 Microchip Technology
Information

Note: this tool was tested with distribution Ubuntu 22.04 onward.
It is known to not work on Ubuntu 20.04 and previous ones, generating such kind of issues:

sam-ba: /lib64/libc.so.6: version `GLIBC_2.34' not found (required by sam-ba)

Get AT91Bootstrap Source Code

You can easily download AT91Bootstrap source code on the at91bootstrap git repository.

To get the source code, you should clone the repository by doing:

$ git clone https://github.com/linux4sam/at91bootstrap.git
Cloning into 'at91bootstrap'...
remote: Enumerating objects: 17621, done.
remote: Counting objects: 100% (3324/3324), done.
remote: Compressing objects: 100% (1029/1029), done.
remote: Total 17621 (delta 2465), reused 3102 (delta 2285), pack-reused 14297
Receiving objects: 100% (17621/17621), 5.65 MiB | 4.65 MiB/s, done.
Resolving deltas: 100% (13459/13459), done.
$ cd at91bootstrap/

Configure AT91Bootstrap

The source code has been taken from the master branch. You must switch to the specified tag by doing:

$ git checkout -b sama7d65 v4.0.9+sama7d65
Switched to a new branch 'sama7d65'

Assuming you are at the AT91Bootstrap root directory, you will find a configs folder which contains several default configuration files:

sama7d65_curiosity_bkptnone_defconfig
sama7d65_curiosity-bsrnf_uboot_defconfig
sama7d65_curiosity-bsrsd1_uboot_defconfig
sama7d65_curiositydf_qspi_uboot_defconfig
sama7d65_curiositynf_uboot_defconfig
sama7d65_curiositysd1_uboot_defconfig
Information

qspi means to read quad-SPI serial flash, sd means to read sd/mmc card, nf means to read nand flash

You can configure AT91Bootstrap to load U-Boot binary from SD Card by doing:

$ make mrproper
$ make sama7d65_curiosity-bsrsd1_uboot_defconfig

If the configuring process is successful, the .config file can be found at AT91Bootstrap root directory.

Customize AT91Bootstrap

If the default configuration doesn't meet your need, after configuring with the default configuration, you can customize it by doing:

$ make menuconfig

Now, in the menuconfig dialog,  you can easily add or remove some features to/from AT91Bootstrap as the same way as kernel configuration.
Move to <Exit> with arrows and press this button hitting the Enter key to exit from this screen.

Build AT91Bootstrap

Then you can build the AT91Bootstrap binary by doing:

$ make

If the building process is successful, the final .bin image is build/binaries/boot-plaintextimg.bin.
The boot-plaintextimg.bin, is the boot format to be used for booting the sama7d65 !SoC.

Warning

Warning:this boot-plaintextimg.bin file name is different from the preceding !SoC in the Microchip MPU family, pay attention to that while re-building AT91Bootstrap.

Build U-Boot from sources

Getting U-Boot sources

Dedicated page on U-Boot wiki: http://www.denx.de/wiki/U-Boot/SourceCode

You can easily download U-Boot source code from Linux4SAM GitHub U-Boot repository:

Clone the Linux4sam GitHub U-Boot repository:

$ git clone https://github.com/linux4sam/u-boot-at91.git
Cloning into 'u-boot-at91'...
remote: Enumerating objects: 1011450, done.
remote: Counting objects: 100% (111523/111523), done.
remote: Compressing objects: 100% (33355/33355), done.
remote: Total 1011450 (delta 77280), reused 111498 (delta 77272), pack-reused 899927 (from 1)
Receiving objects: 100% (1011450/1011450), 238.61 MiB | 24.92 MiB/s, done.
Resolving deltas: 100% (826270/826270), done.
Updating files: 100% (19925/19925), done.
$ cd u-boot-at91/

The source code has been taken from the master branch. You must switch to the specified tag by doing:

$ git checkout -b sama7d65 linux4microchip+sama7d65-2025.02
Switched to a new branch 'sama7d65'

Cross-compiling U-Boot

Before compiling the U-Boot, you need setup cross compile toolchain in the Setup ARM Cross Compiler above.

Warning

Latest versions of U-boot (2018.07 and newer) have a minimum requirement of 6.0 version of the GCC toolchain. We always recommend to use the latest versions.

Once the AT91 U-Boot sources available, cross-compile U-Boot is made in two steps: configuration and compiling. Check the Configuration chapter in U-Boot reference manual.

Information

Go to the configs/ to find the exact target when invoking make.

The U-Boot environment variables can be stored in different media, below config files can specify where to store the U-Boot environment.

   # To put environment variables in SD/MMC card:
  sama7d65_curiosity_mmc1_defconfig

Here are the building steps for the SAMA7D65-Curiosity board:

# You can change the config according to your needs.
make sama7d65_curiosity_mmc1_defconfig
make

The result of these operations is a fresh U-Boot binary called u-boot.bin corresponding to the binary ELF file u-boot.

  • u-boot.bin is the file you should store on the board
  • u-boot is the ELF format binary file you may use to debug U-Boot through a JTag link for instance.

Build Kernel from sources

At this step, you can modify default configuration using the menuconfig

  • $ make ARCH=arm menuconfig

    Now, in the menuconfig dialog, you can easily add or remove some features. Once done, Move to <Exit> with arrows and press this button hitting the Enter key to exit from this screen.

    Build the Linux kernel image, before you build you need set up the cross compile toolchain, check this section.

    $ make ARCH=arm

    [..]

      Kernel: arch/arm/boot/Image is ready
      Kernel: arch/arm/boot/zImage is ready

    Now you have an usable compressed kernel image zImage.

    If you need an uImage you can run this additional step:

    make ARCH=arm uImage LOADADDR=0x20008000

    [..]

    Kernel: arch/arm/boot/Image is ready
    Kernel: arch/arm/boot/zImage is ready
    UIMAGE  arch/arm/boot/uImage
    Image Name:   Linux-6.12.22-linux4microchip-20
    Created:      Thu May 22 18:05:21 2025
    Image Type:   ARM Linux Kernel Image (uncompressed)
    Data Size:    5688984 Bytes = 5555.65 KiB = 5.43 MiB
    Load Address: 20008000
    Entry Point:  20008000
    Kernel: arch/arm/boot/uImage is ready
    make ARCH=arm dtbs

    [..]

      DTC     arch/arm/boot/dts/microchip/at91-sama5d27_som1_ek.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama5d27_wlsom1_ek.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama5d29_curiosity.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama5d2_icp.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama5d3_eds.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama7d65_curiosity.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama7g54_curiosity.dtb
      DTC     arch/arm/boot/dts/microchip/at91-sama7g5ek.dtb

    [..]

    If the building process is successful, the final images can be found under arch/arm/boot/ directory.

Build Yocto Project rootfs from sources

Note that building an entire distribution is a long process. It also requires a big amount of free disk space.

The support for Microchip MPU SoC family is included in a particular Yocto Project layer: meta-mchp. The source for this layer are hosted on Linux4Microchip GitHub accounthttps://github.com/linux4microchip/meta-mchp

Building environment

A step-by-step comprehensive installation is explained in the Yocto Project Quick Build. The following lines have to be considered as an add-on that is MPU specific or that can facilitate your setup.

Step by step build procedure

Note here is the README procedure available directly in the meta-mchp-common layer. This file in the meta-mchp layer repository must be considered as the reference and the following copy can be out-of-sync.

Note starting with Linux4Microchip 2025.04 release, the meta-mchp layer supports Yocto Project templates, so make sure you create a new build environment using oe-init-build-env

OpenEmbedded/Yocto Project BSP layer for Microchip's SoCs

Description

The meta-mchp-common layer consolidates common Board Support Package (BSP) components and metadata for Microchip platforms, streamlining development across various Microchip devices for use with OpenEmbedded and/or Yocto Project.

Supported Machines

The meta-mchp-common layer provides support for various Microchip platforms. For detailed information about supported machines, please refer to the documentation in the relevant sub-layers:

Prerequisites

Before starting, please refer to the Required Packages for Build Host section in the Yocto Project Documentation to install required dependencies for the build environment:

Information

Note: Make sure to install git-lfs and repo in addition to the required packages for your Linux distribution.

For instance, on Ubuntu or Debian, these packages need to be installed on your development host:

sudo apt-get install gawk wget git-core git-lfs diffstat unzip texinfo gcc-multilib \
     build-essential chrpath socat cpio python3 python3-pip python3-pexpect \
     xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
     pylint3 xterm repo

Usage

To integrate this layer into your Yocto Project build environment:

Clone the necessary repositories:

Create an empty directory to hold the workspace:

mkdir yocto-dev
cd yocto-dev

Use the repo tool to fetch all the required repositories

Make sure to install the repo utility first.

repo init -u https://github.com/linux4microchip/meta-mchp-manifest.git -b <branch> -m <target>/default.xml

Replace and with the Yocto release branch and the manifest required. For example:

repo init -u https://github.com/linux4microchip/meta-mchp-manifest.git -b scarthgap -m mpu/default.xml

Fetch all the required repositories using the following repo command:

repo sync

Initialize the build environment:

The meta-mchp repository provides sample configuration templates that help set up BitBake layers and key configuration files in the Yocto build directory.

Set the TEMPLATECONF environment variable to point to the appropriate configuration template before initializing the build environment:

export TEMPLATECONF=${TEMPLATECONF:-../meta-mchp/<meta-layer>/conf/templates/default}

Replace meta-layer above with the desired layer based on your target platform. For example:

export TEMPLATECONF=${TEMPLATECONF:-../meta-mchp/meta-mchp-mpu/conf/templates/default}

Note: Setting TEMPLATECONF is only needed the first time you will run the source command.

Then initialize the Yocto build environment:

source openembedded-core/oe-init-build-env

 

Set the target machine and build the image:

MACHINE=<machine> bitbake core-image-minimal

Each sub-layer provides several images that include demos and applications tailored for its respective platform.

For more information on the supported images, please refer to the README:

MPU layer README

Layer Dependencies

This layer depends on the following layers:

- meta-openembedded
 - URI: git://git.openembedded.org/meta-openembedded
 - Layers: meta-oe, meta-networking, meta-python

- openembedded-core
 - URI: git://git.openembedded.org/openembedded-core
 - Layers: meta

For information on the specific revisions used, refer to the meta-mchp manifest repository.

Licensing

The contents of this layer are licensed under the MIT License. See COPYING.MIT for details.

Contributing

If you want to contribute changes, you can send Github pull requests at https://github.com/linux4microchip/meta-mchp/pulls.

See CONTRIBUTING.md for additional information about contribution guidelines.

Maintainers

  • Hari Prasath G E <hari.prasathge@microchip.com>
  • Valentina Fernandez Alanis <valentina.fernandezalanis@microchip.com>
  • Dharma Balasubiramani <dharma.b@microchip.com>

Using SAM-BA to flash components to board

NAND Flash demo - Memory map

demo_nandflash_map_lnx4sam6x.png

 

Install SAM-BA software in your PC

In addition to the official SAM-BA pages on http://www.microchip.com, we maintain information about SAM-BA in the SoftwareTools page.

Warning

use SAM-BA 3.9.y onwards. You can download it here: SAM-BA 3.9.1 release page.

 

Launch SAM-BA tools

In addition to the Qt5 QML language for scripting used for flashing the demos, most common SAM-BA action can be done using SAM-BA command line.

For browsing information on the SAM-BA command line usage, please see the Command Line Documentation that is available in the SAM-BA installation directory: doc/index.html or doc/cmdline.html .

SAM-BA includes command line interface that provides support for the most common actions:

  • reading / writing to arbitrary memory addresses and/or peripherals
  • uploading applets and using them to erase/read/write external memories

The command line interface is designed to be self-documenting.

The main commands can be listed using the "sam-ba --help" command:

SAM-BA Command Line Interface Tool v3.9.1 (linux - x86_64-little_endian-lp64)
Copyright 2025 Microchip Technology

Usage: sam-ba [options]

Options:
  -v, --version                             Displays version information.
  -h, --help                                Displays this help.
  -l, --loglevel <log_level[:options:...]>  Set verbose log level.
  -x, --execute <script.qml>                Execute script <script.qml>.
  -p, --port <port[:options:...]>           Communicate with device using
                                            <port>.
  -d, --device <device[:options:...]>       Connected device is <device>.
  -b, --board <board[:options:...]>         Connected board is <board>.
  -m, --monitor <command[:options:...]>     Run monitor command <command>.
  -a, --applet <applet[:options:...]>       Load and initialize applet
                                            <applet>.
  -c, --command <command[:args:...]>        Run command <command>.
  -t, --tracelevel <trace_level>            Set applet trace level to
                                            <trace_level>.
  -L, --applet-buffer-limit <SIZE>          Set applet buffer limit to <SIZE>
                                            bytes (default 131072).
  -w, --working-directory <DIR>             Set working directory to <DIR>.
  -u, --utils <tool[:args:...]>             Launch a tool <tool> .

If you get the following error, it indicates a symbol mismatch or unresolved symbol when the sam-ba executable is being loaded

$ sam-ba -v
sam-ba: symbol lookup error: sam-ba: undefined symbol: _ZdlPvm, version Qt_5

Check for Qt libraries inside the extracted SAM-BA directory.

$ cd path/to/sam-ba
$ export LD_LIBRARY_PATH=$(pwd)/lib:$LD_LIBRARY_PATH

Additional help can be obtained for most commands by supplying a "help" parameter that will display their usage.

For example "sam-ba --port help" will display:

Known ports: j-link, serial, secure

Command that take an argument with options (port, monitor, applet) will display even more documentation when called with "help" as option value.

For example "sam-ba --port serial:help" will display:

Syntax:
   serial:[<port>]:[<baudrate>]
Examples:
   serial                serial port (will use first AT91 USB if found otherwise first serial port)
   serial:COM80          serial port on COM80
   serial:ttyUSB0:57600  serial port on /dev/ttyUSB0, baudrate 57600

Configure NAND ECC

Using default PMECC parameters

Information

when choosing the board variant with the -b parameter of SAM-BA, the default PMECC configuration for the NAND populated on the board is valid. You can verify its value by running the command that reads one byte in a dummy file (named test.bin in the following command):

# sam-ba -p serial -b sama7d65-curiosity -a nandflash -c read:test.bin:0:1
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc1e04e07.
Supported erase block sizes: 256KB
Executing command 'read:test.bin:0:1'
Read 1 bytes at address 0x00000000 (100.00%)
Connection closed.

You can figure out that the default PMECC parameter for this sama7d65-curiosity board is 0xc1e04e07.

Information

Note that if you connect a serial console to the SoC RomCode default UART, you can see even more details about the NAND ECC parameters given by the SAM-BA Applet:

Applet 'NAND Flash' from softpack 3.8 (v3.8).
Initializing NAND ioSet1 Bus Width 8
PMECC configuration: 0xc1e04e07
Sector size: 512
Sectors per page: 8
Spare size: 224
ECC bits: 8
ECC offset: 120
ECC size: 104
PMECC enabled
Buffer Address: 0x0020a240
Buffer Size: 20480 bytes
NAND applet initialized successfully.

If you want to change the default PMECC parameters you can simply specify another value on the SAM-BA command line with the -a nandflash argument as shown below:

# sam-ba -p serial -b sama7d65-curiosity -a nandflash:help
Syntax: nandflash:[<ioset>]:[<bus_width>]:[<pmecc_cfg>]
Parameters:
   ioset      I/O set
   bus_width  NAND bus width (8/16)
   header     NAND header value
Examples:
   nandflash                 use default board settings
   nandflash:2:8:0xc0098da5  use fully custom settings (IOSET2, 8-bit bus, header is 0xc0098da5)
   nandflash:::0xc0098da5    use default board settings but force header to 0xc0098da5
For information on NAND header values, please refer to SAMA5D4 datasheet section "12.4.4 Detailed Memory Boot Procedures".

By reading this in-line documentation we can specify the NAND PMECC parameter with this command:

# sam-ba -p serial -b sama7d65-curiosity -a nandflash:::0xc1e04e07
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc1e04e07.
Supported erase block sizes: 256KB
Connection closed.

Programming components into NAND

Program AT91Bootstrap binary

Run SAM-BA with USB connection (equivalent to serial) and erase the beginning of the NAND flash and then write AT91Bootstrap binary:

# sam-ba -p serial -b sama7d65-curiosity -a nandflash -c erase::0x40000 -c writeboot:at91bootstrap-sama7d65_curiosity.bin
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc1e04e07.
Supported erase block sizes: 256KB
Executing command 'erase::0x40000'
Erased 262144 bytes at address 0x00000000 (100.00%)
Executing command 'writeboot:at91bootstrap-sama7d65_curiosity.bin'
Prepended NAND header prefix (0xc1e04e07)
Appending 4008 bytes of padding to fill the last written page
Wrote 20480 bytes at address 0x00000000 (83.33%)
Wrote 4096 bytes at address 0x00005000 (100.00%)
Connection closed.

Program U-Boot binary

Run SAM-BA with USB connection (equivalent to serial) and erase the U-Boot section in the NAND flash memory map and then write U-Boot binary:

# sam-ba -p serial -b sama7d65-curiosity -a nandflash -c erase:0x40000:0x80000 -c write:u-boot-sama7d65-curiosity.bin:0x40000
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 536870912 bytes.
Page size is 4096 bytes.
Buffer is 20480 bytes (5 pages) at address 0x0020a240.
NAND header value is 0xc1e04e07.
Supported erase block sizes: 256KB
Executing command 'erase:0x40000:0x80000'
Erased 262144 bytes at address 0x00040000 (50.00%)
Erased 262144 bytes at address 0x00080000 (100.00%)
Executing command 'write:u-boot-sama7d65-curiosity.bin:0x40000'
Appending 3137 bytes of padding to fill the last written page
Wrote 20480 bytes at address 0x00040000 (4.59%)
Wrote 20480 bytes at address 0x00045000 (9.17%)
Wrote 20480 bytes at address 0x0004a000 (13.76%)
[..]
Wrote 20480 bytes at address 0x00094000 (81.65%)
Wrote 20480 bytes at address 0x00099000 (86.24%)
Wrote 20480 bytes at address 0x0009e000 (90.83%)
Wrote 20480 bytes at address 0x000a3000 (95.41%)
Wrote 20480 bytes at address 0x000a8000 (100.00%)
Connection closed.

Recent FAQ