AT91Bootstrap for OP-TEE
Last modified by Microchip on 2025/03/03 06:22
Get Sources
You can easily download AT91Bootstrap source code on the at91bootstrap repository.
To get the source code, you should clone the repository by doing:
$ git clone https://github.com/linux4sam/at91bootstrap.git
Cloning into 'at91bootstrap'...
remote: Enumerating objects: 17621, done.
remote: Counting objects: 100% (3324/3324), done.
remote: Compressing objects: 100% (1029/1029), done.
remote: Total 17621 (delta 2465), reused 3102 (delta 2285), pack-reused 14297
Receiving objects: 100% (17621/17621), 5.65 MiB | 4.65 MiB/s, done.
Resolving deltas: 100% (13459/13459), done.
$ cd at91bootstrap/
Cloning into 'at91bootstrap'...
remote: Enumerating objects: 17621, done.
remote: Counting objects: 100% (3324/3324), done.
remote: Compressing objects: 100% (1029/1029), done.
remote: Total 17621 (delta 2465), reused 3102 (delta 2285), pack-reused 14297
Receiving objects: 100% (17621/17621), 5.65 MiB | 4.65 MiB/s, done.
Resolving deltas: 100% (13459/13459), done.
$ cd at91bootstrap/
Configure AT91Bootstrap
Inside the AT91Bootstrap root directory you will find a configs folder which contains several default configuration files only one file contains the correct configuration for OP-TEE:
sama5d27_som1_ek-opteesd_uboot_defconfig
You can configure AT91Bootstrap by doing:
$ make mrproper
$ make sama5d27_som1_ek-opteesd_uboot_defconfig
$ make sama5d27_som1_ek-opteesd_uboot_defconfig
If the configuring process is successful, the .config file can be found at AT91Bootstrap root directory.
Build AT91Bootstrap
Then you can build the AT91Bootstrap binary by doing:
$ make
If the building process is successful, the final .bin image is build/binaries/at91bootstrap.bin.