Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Get Memory Mapping Parameters With memmap Module
Last modified by Microchip on 2026/08/17 12:16
After booting the Linux® system, you can load the memmap module, which will output the memory mapping parameters to the console. This module is only used with the Manually Save and Load Snapshot Image mode.
Get mem_map information with the mem_map module.
Here are the steps to get runtime memory map information on the target board.
You can send modules via console input or from a USB flash drive.
First, send the mem_map_module.ko with ZMODEM. Type “lrz”.
# lrz lrz waiting to receive.**B0100000023be50
Next, select File > Transfer > ZMODEM > Send from the menu as shown in the accompanying image:
Then, select the mem_map_module.ko file under the mem_map folder. Run the module with the command as shown:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.