Get Memory Mapping Parameters in Pre-saved Mode

Last modified by Microchip on 2026/08/17 11:57

Prerequisites

To obtain memory mapping parameters in Load Pre-saved Snapshot Image mode, apply the Linux® kernel patch required to support this feature. See the "Apply Kernel Patch to Support Ultra-Fast Boot" page for more detailed information.

How to Get Memory Mapping Parameters

During the Linux kernel boot in Load Pre-saved Snapshot Image mode, the memory mapping parameters are printed to the console.

memory mapping parameters

Information

Note: These parameters will be required when generating snapshot images in the future.

See the "Create Snapshot Image With memmap Tools" page for details.