archive5_0
Last modified by Microchip on 2026/01/09 08:12
linux4sam_5.0 tag
Kernel
As a updated kernel revision this branch contains all the enhancements already found on the the Atmel linux-3.18-at91 branch.
Here is a little summary of the enhancements added on top of the official v4.1 Linux kernel tag:
- all Atmel material included in the following 4.2 kernel:
- addition of newer AT91 boards
- AT91SAM9x5: pwm0 pinctrl definition
- SAMA5D4: more peripherals: usarts, uarts, spi, pioD access
- SAMA5D3: phy address for gmac
- regulator additions for the SD/MMC
- rtc node for AT91SAM9RL/AT91SAM9RL-EK
- addition of the new SAMA5D2 SoC and associated SAMA5D2 Xplained board
- DMA: interleaved, memset and scatter-gathered memset offload operations
- flexcom: serial, I2C and SPI: new FIFO and DMA modes for SAMA5D2
- SDHCI driver (SD/MMC) for SAMA5D2
- ClassD audio output driver for SAMA5D2
- Image Sensor:
- ISC: support YUV sensor output ; support RGB output format
- ISI enhancement: add RGB565, GREY, SGRBG, SBGGR (Bayer) support
- new shutdown controller driver for SAMA5D2
- new I2S controller driver for audio on SAMA5D2
- CAN controller for SAMA5D2
- new watchdog driver for SAMA5D4 & SAMA5D2 SoCs
- generated and audio PLL clocks for SAMA5D2
- support for act8865 PMIC
- LCD specification to the at91sam9x5 series and associated boards
- fixes for USB, AES dma configuration
linux4sam_5.0-alpha7 tag
Kernel
- support for new SAMA5D2 SoC and the associated sama5d2 Xplained board
- QSPI with DMA (disabled in Device Tree by default)
- Flexcom with FIFO & DMA
- USART interface
- I2C interface
- SPI interface
- SD/MMC interface (SDHCI) + on-board eMMC
- Audio using Class D amplifier
- ISC
- support YUV sensor output
- support RGB output format
- Crypto engines
- AEAD support for IPSec
- fix residue computation for HDMA
- ISI: add RGB565, GREY, SGRBG, SBGGR (Bayer) support
- runtime PM: added the ISI driver, modifications to the HLCD DRM driver
And the enhancements from linux4sam_4.7 tag below
Pre-built Demo
| Board | Description | Binary | Sources location |
|---|---|---|---|
| SAMA5D2 Xplained | Linux4SAM Yocto Project / Poky based demo compiled from tag linux4sam_5.0 Follow procedure: #Flash_the_demo | linux4sam-poky-sama5d2_xplained-5.0.zip (~ 106 MB) md5: c6ed4d4dd987624d7aa9238f39d23cc3 | AT91Bootstrap U-Boot Linux Kernel Yocto |
| SD Card SAMA5D2 Xplained | Linux4SAM Yocto Project / Poky SD Card image compiled from tag linux4sam_5.0 Follow procedure: #Create_a_SD_card_with_the_demo | linux4sam-poky-sama5d2_xplained-5.0.img.bz2 (~ 98 MB) md5: 7a8ffcd8fca2c2c17a950200fffa25a | |
| SAMA5D4 Xplained | Linux4SAM Yocto Project / Poky based demo compiled from tag linux4sam_5.0 | linux4sam-poky-sama5d4_xplained-5.0.zip (~ 119 MB) md5: 8070d60387fd0462fe4cffa3a41c13e6 | AT91Bootstrap U-Boot Linux Kernel Yocto |
| SAMA5D3 Xplained | Linux4SAM Yocto Project / Poky based demo compiled from tag linux4sam_5.0 | linux4sam-poky-sama5d3_xplained-5.0.zip (~ 119 MB) md5: ff4bdca31793dccda32e52dca75e48db | AT91Bootstrap U-Boot Linux Kernel Yocto |