DT Overlays
You can easily download DT Overlay source code from Linux4Microchip GitHub DT Overlays repository
:
- clone the Linux4Microchip GitHub DT Overlay repository
$ git clone https://github.com/linux4microchip/dt-overlay-mchp.git
Cloning into 'dt-overlay-mchp'...
remote: Enumerating objects: 1585, done.
remote: Counting objects: 100% (465/465), done.
remote: Compressing objects: 100% (180/180), done.
remote: Total 1585 (delta 282), reused 441 (delta 274), pack-reused 1120
Receiving objects: 100% (1585/1585), 539.04 KiB | 4.08 MiB/s, done.
Resolving deltas: 100% (879/879), done.
$ cd dt-overlay-mchp/
- The source code has been taken from the master branch which is pointing to the latest branch we use.
To build the overlays for a board make sure the following steps are done:
- the environment variables ARCH and CROSS_COMPILE are set correctly
- (optional) the environment variable KERNEL_DIR points to Linux kernel and the kernel was already built for the board. This is needed because the DT Overlay repository uses the Device Tree Compiler (dtc) from the kernel source tree. By default, KERNEL_DIR is set to a linux directory that would be under the parent directory in the directory tree: ../linux
- (optional) the environment variable KERNEL_BUILD_DIR that points to where the Linux kernel binary and Device Tree blob, resulting of your compilation of the kernel, are located. By default, KERNEL_BUILD_DIR is set to the same directory as KERNEL_DIR. It shouldn't be changed if you have the habit of compiling your kernel within the Linux source tree
The following example shows how to build the overlays for sam9x75_curiosity_dtbos:
$ make sam9x75_curiosity_dtbos
To build the FIT image with overlays for a board make sure the following steps are done:
- the environment variables ARCH and CROSS_COMPILE are set correctly
- (optional) the environment variable KERNEL_DIR points to Linux kernel and the kernel was already built for the board. This is needed because the DT Overlay repository uses the Device Tree Compiler (dtc) from the kernel source tree. By default, KERNEL_DIR is set to a linux directory that would be under the parent directory in the directory tree: ../linux
- (optional) the environment variable KERNEL_BUILD_DIR that points to where the Linux kernel binary and Device Tree blob, resulting of your compilation of the kernel, are located. By default, KERNEL_BUILD_DIR is set to the same directory as KERNEL_DIR. It shouldn't be changed if you have the habit of compiling your kernel within the Linux source tree.
- mkimage is installed on the development machine
- the Device Tree Compiler from Linux kernel is in the PATH environment variable
The following example shows how to build the FIT image for sama5d27_wlsom1_ek:
$ make sam9x75_curiosity.itb
....
FIT description: Microchip SAM9X75-Curiosity FIT Image
Created: Thu May 16 15:14:43 2024
Image 0 (kernel)
Description: Linux4SAM Linux kernel
Created: Thu May 16 15:14:43 2024
Type: Kernel Image
Compression: uncompressed
Data Size: 5221704 Bytes = 5099.32 KiB = 4.98 MiB
Architecture: ARM
OS: Linux
Load Address: 0x22000000
Entry Point: 0x22000000
Hash algo: crc32
Hash value: 9778d68b
Hash algo: sha1
Hash value: 1c5dc50a13f1b6d18787ebdbbbcde67b069f10e3
Image 1 (base_fdt)
Description: SAM9X75-Curiosity Flattened Device Tree blob
Created: Thu May 16 15:14:43 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 28755 Bytes = 28.08 KiB = 0.03 MiB
Architecture: ARM
Load Address: 0x23000000
Hash algo: crc32
Hash value: d35678b4
Hash algo: sha1
Hash value: 2598efa5e36ccc3defdae2c0de86f416c9c088f7
Image 2 (fdt_isc_imx219)
Description: Device Tree blob ISC IMX219 overlay
Created: Thu May 16 15:14:43 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 4126 Bytes = 4.03 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23100000
Hash algo: crc32
Hash value: d8fd34cf
Hash algo: sha1
Hash value: 75ff92b00dc8d9466fe07789822127ee5d225640
Image 3 (fdt_lvds_panel)
Description: Device Tree blob for AC69T88A LVDS Display Panel
Created: Thu May 16 15:14:43 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 3946 Bytes = 3.85 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23110000
Hash algo: crc32
Hash value: f2aca13d
Hash algo: sha1
Hash value: cceb96efe1621f3ad6427d6cdf8f4e2702aacb00
Image 4 (fdt_gmac_lan8840)
Description: Device Tree blob for LAN8840 RGMII PHY overlay
Created: Thu May 16 15:14:43 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 2168 Bytes = 2.12 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23120000
Hash algo: crc32
Hash value: 44e2f96d
Hash algo: sha1
Hash value: 8879cb8f80cc87d5ed53af5bae11a4cc9f1ddc41
Image 5 (fdt_i2s_proto)
Description: Device Tree blob PROTO Audio board overlay
Created: Thu May 16 15:14:43 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 1666 Bytes = 1.63 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23130000
Hash algo: crc32
Hash value: df39dc8b
Hash algo: sha1
Hash value: 1c7c335aad79d82d3482b3d9da7fbbcd4bf98ee4
Default Configuration: 'kernel_dtb'
Configuration 0 (kernel_dtb)
Description: Linux kernel and base FDT blob for SAM9X75-Curiosity board
Kernel: kernel
FDT: base_fdt
Configuration 1 (base_dtb)
Description: Base FDT blob for SAM9X75-Curiosity board
Kernel: unavailable
FDT: base_fdt
Configuration 2 (imx219)
Description: FDT overlay blob for ISC IMX219 sensor
Kernel: unavailable
FDT: fdt_isc_imx219
Configuration 3 (lvds)
Description: FDT overlay blob for AC69T88A LVDS Display Panel
Kernel: unavailable
FDT: fdt_lvds_panel
Configuration 4 (lan8840)
Description: FDT overlay blob for LAN8840 RGMII PHY Daughter Card
Kernel: unavailable
FDT: fdt_gmac_lan8840
Configuration 5 (i2s_proto)
Description: FDT overlay blob for I2S PROTO audio board
Kernel: unavailable
FDT: fdt_i2s_proto
The following example shows how to build a FIT image for SAM9X60 Curiosity board using the KERNEL_DIR and KERNEL_BUILD_DIR environment variables that are handled by the dt-overlay-mchp Makefile. This allows you to precisely specify where the kernel source tree is and where the resulting of your compilation of this kernel is located. It allows the Makefile to find the Device Tree Compiler (dtc), the kernel image (zImage) and the device tree for the board (.dtb). This brings a lot of flexibility to the process of creating a FIT image.
Note that environment variables ARCH and CROSS_COMPILE are set to their adapted values on this example system. CROSS_COMPILE variable in particular must be adapted to your own development host.
$ KERNEL_DIR=/<path_to_kernel_sources> KERNEL_BUILD_DIR=/<path_to_kernel_build_dir> make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- sam9x60_curiosity.itb
....
mkimage -D "-i../linux/arch/arm/boot/ -i../linux/arch/arm/boot/dts -i../linux/arch/arm/boot/dts/microchip -p 1000 -@ -Wno-unit_address_vs_reg -Wno-graph_child_address -Wno-pwms_property" -f sam9x60_curiosity.its sam9x60_curiosity.itb
FIT description: Microchip SAM9X60-Curiosity FIT Image
Created: Thu May 16 15:16:13 2024
Image 0 (kernel)
Description: Linux4SAM Linux kernel
Created: Thu May 16 15:16:13 2024
Type: Kernel Image
Compression: uncompressed
Data Size: 5221704 Bytes = 5099.32 KiB = 4.98 MiB
Architecture: ARM
OS: Linux
Load Address: 0x22000000
Entry Point: 0x22000000
Hash algo: crc32
Hash value: 9778d68b
Hash algo: sha1
Hash value: 1c5dc50a13f1b6d18787ebdbbbcde67b069f10e3
Image 1 (base_fdt)
Description: SAM9X60-Curiosity Flattened Device Tree blob
Created: Thu May 16 15:16:13 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 36432 Bytes = 35.58 KiB = 0.03 MiB
Architecture: ARM
Load Address: 0x23000000
Hash algo: crc32
Hash value: a4558e6d
Hash algo: sha1
Hash value: b31d0eb8b22d9bc32c1751c8d9c01689d4ea0757
Image 2 (fdt_pda5)
Description: Device Tree blob pda5000 overlay
Created: Thu May 16 15:16:13 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 4772 Bytes = 4.66 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23100000
Hash algo: crc32
Hash value: 9b565bfe
Hash algo: sha1
Hash value: c425668b2bc897fa83e867a0dea13547bb393a96
Image 3 (fdt_wilc3000)
Description: Device Tree blob WILC3000 overlay
Created: Thu May 16 15:16:13 2024
Type: Flat Device Tree
Compression: uncompressed
Data Size: 1534 Bytes = 1.50 KiB = 0.00 MiB
Architecture: ARM
Load Address: 0x23110000
Hash algo: crc32
Hash value: 8294b75c
Hash algo: sha1
Hash value: 86494722c92f978610dbbc96cc5a07a3804cf6bf
Default Configuration: 'kernel_dtb'
Configuration 0 (kernel_dtb)
Description: Linux kernel and base FDT blob for SAM9X60-Curiosity board
Kernel: kernel
FDT: base_fdt
Configuration 1 (base_dtb)
Description: Base FDT blob for SAM9X60-Curiosity board
Kernel: unavailable
FDT: base_fdt
Configuration 2 (pda5)
Description: FDT overlay blob for PDA TM5000 screen
Kernel: unavailable
FDT: fdt_pda5
Configuration 3 (wilc)
Description: FDT overlay blob for WILC3000
Kernel: unavailable
FDT: fdt_wilc3000