OpenEmbedded / Yocto Project / Poky: build from sources
OpenEmbedded / Yocto Project / Poky: build from sources
How to build Poky for AT91
Note that building an entire distribution is a long process. It also requires a big amount of free disk space.
The support for Microchip AT91 SoC family is included in a particular Yocto Project layer: meta-atmel. The source for this layer are hosted on Linux4SAM GitHub account: https://github.com/linux4sam/meta-atmel
Building environment
A step-by-step comprehensive installation is explained in the Yocto Project Quick Build. The following lines have to be considered as an add-on that is AT91 specific or that can facilitate your setup.
Prerequisite
Here are the reference pages for setting up a Yocto Project building environment: What You Need and How You Get It.
For instance, on Ubuntu or debian, these packages need to be installed on your development host:
build-essential chrpath socat cpio python3 python3-pip python3-pexpect \
xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
pylint3 xterm
Step by step build procedure
====================================================================
For more information about the Microchip MPU product line see:
http://www.microchip.com/design-centers/32-bit-mpus
Linux & Open Source on Microchip microprocessors:
http://www.linux4sam.org
Supported SoCs / MACHINE names
==============================
Note that most of the machine names below, have a SD Card variant that can be
built by adding an "-sd" suffix to the machine name.
- SAMA5D2 product family / sama5d2-xplained, sama5d2-xplained-emmc, sama5d27-som1-ek-sd, sama5d27-som1-ek-optee-sd, sama5d2-ptc-ek, sama5d2-icp, sama5d27-wlsom1-ek-sd, sama5d29-curiosity-sd
- SAMA5D4 product family / sama5d4ek, sama5d4-xplained
- SAMA5D3 product family / sama5d3xek, sama5d3-xplained
- AT91SAM9x5 product family (AT91SAM9G15, AT91SAM9G25, AT91SAM9X25, AT91SAM9G35 and AT91SAM9X35) / at91sam9x5ek
- AT91SAM9RL / at91sam9rlek
- AT91SAM9G45 / at91sam9m10g45ek
- SAM9X60 / sam9x60ek, sam9x60-curiosity
- SAMA7G5 / sama7g5ek-sd, sama7g5ek-optee-sd, sama7g5ek-emmc, sama7g5ek-ospi
- SAM9X75 / sam9x75eb, sam9x75-curiosity
Sources
=======
- meta-atmel
URI: https://github.com/linux4sam/meta-atmel.git
Branch: scarthgap
Tag/commit:53c6bb2eddceb62ae5120c7c68174ce423d341e2
Dependencies
============
This Layer depends on :
- poky
URI: https://git.yoctoproject.org/poky
Branch: scarthgap
Tag:scarthgap-5.0.3
- meta-openembedded
URI: https://git.openembedded.org/meta-openembedded
Branch: scarthgap
Tag/commit:735ae0310870ffce07ce0c55c4f87c20ac161ff9
- meta-arm (for optee components)
URI: https://git.yoctoproject.org/meta-arm
Branch: scarthgap
Tag:yocto-5.0
Build procedure
===============
0/ Create a directory
mkdir my_dir
cd my_dir
1/ Clone yocto/poky git repository with the proper branch ready
git clone https://git.yoctoproject.org/poky && cd poky && \
git checkout -b scarthgap scarthgap-5.0.3 && cd -
2/ Clone meta-openembedded git repository with the proper branch ready
git clone git://git.openembedded.org/meta-openembedded && \
cd meta-openembedded && git checkout -b scarthgap 735ae0 && cd -
3/ Clone meta-atmel layer with the proper branch ready
git clone https://github.com/linux4sam/meta-atmel.git && cd meta-atmel && \
git checkout -b scarthgap 53c6bb && cd -
4/ Clone meta-arm layer with the proper branch ready
git clone https://git.yoctoproject.org/meta-arm && cd meta-arm && \
git checkout -b scarthgap yocto-5.0 && cd -
5/ Enter the poky directory to configure the build system and start the build process
cd poky
If not created yet, add a new "build-microchip" directory:
mkdir build-microchip
Else, if it's the first time you use Yocto Project templates, and if the
build-microchip directory remains from a previous use, we advise you to start
from a fresh directory. Keep your build-microchip/conf/local.conf file for
reference.
6/ Inside the .templateconf file, you will need to modify the TEMPLATECONF
variable to match the path to the meta-atmel layer "conf" directory:
export TEMPLATECONF=${TEMPLATECONF:-../meta-atmel/conf/templates/default}
7/ Initialize build directory
source oe-init-build-env build-microchip
8/ To build a small image provided by Yocto Project:
[MACHINE=] bitbake core-image-minimal
Example for sama5d2-xplained-sd SD card image:
MACHINE=sama5d2-xplained-sd bitbake core-image-minimal
9/ To build the microchip image with no graphics support:
[MACHINE=] bitbake microchip-headless-image
Example for sama5d2-xplained-sd SD card image:
MACHINE=sama5d2-xplained-sd bitbake microchip-headless-image
10/ To build the microchip image with graphics support (EGT):
[MACHINE=] bitbake microchip-graphics-image
Example for sama5d2-xplained-sd SD card image:
MACHINE=sama5d2-xplained-sd bitbake microchip-graphics-image
Typical bitbake output
======================
Build Configuration:
BB_VERSION = "2.8.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "sam9x75-curiosity-sd"
DISTRO = "poky-atmel"
DISTRO_VERSION = "5.0.3"
TUNE_FEATURES = "arm armv5 thumb dsp"
TARGET_FPU = "soft"
meta
meta-poky
meta-yocto-bsp = "heads/scarthgap-5.0.3:0b37512fb4b231cc106768e2a7328431009b3b70"
meta-oe
meta-networking
meta-webserver
meta-python
meta-initramfs = "735ae0310870ffce07ce0c55c4f87c20ac161ff9:735ae0310870ffce07ce0c55c4f87c20ac161ff9"
meta-atmel = "heads/linux4microchip-2024.10:53c6bb2eddceb62ae5120c7c68174ce423d341e2"
meta-multimedia = "735ae0310870ffce07ce0c55c4f87c20ac161ff9:735ae0310870ffce07ce0c55c4f87c20ac161ff9"
meta-arm
meta-arm-toolchain = "heads/yocto-5.0:8aa8a1f17f5b64bc691544f989f04fc83df98adb"
Contributing
============
To contribute to this layer you should submit the patches for review to:
the github pull-request facility directly or the forum. Anyway, don't forget to
Cc the maintainers.
Microchip Forum:
https://www.microchip.com/forums/f542.aspx
for some useful guidelines to be followed when submitting patches:
http://www.openembedded.org/wiki/How_to_submit_a_patch_to_OpenEmbedded
Maintainers:
Hari Prasath G E
Nicolas Ferre
When creating patches insert the [meta-atmel] tag in the subject, for example
use something like:
git format-patch -s --subject-prefix='meta-atmel][PATCH'
Poky SDK
The meta-toolchain recipes build tarballs which contain cross compilation toolchain, cross compiled libraries, includes and configuration tools suitable for application development outside Poky.
The cross-compilation toolchain and all coss-compiled libraries will be present in this SDK allowing the user to exactly match what is provided in the associated Linux4SAM demo image.
If a random cross-compilation toolchain was used, it would lead to undefined symbols and unmatched library calls. With this SDK matching what is present on the target, cross-development is enhanced with all possibilities offered by shared libraries that any embedded Linux developer could expect from such a system.
This cross-development cycle doesn't have to be integrated within an OpenEmbedded integration flow: usual Makefiles, cmake, IDE... in short: any developer-friendly environment could be used allowing the separation of the development phase from the integration phase.
Build Poky SDK
This SDK is generated using the bitbake handy target populate_sdk.
bitbake -c populate_sdk microchip-graphics-image
or
bitbake -c populate_sdk microchip-headless-image
It will produce a comprehensive SDK script (auto-extracting archive) available in the deployment directory: from the build directory it is usually located in tmp/deploy/sdk.
For instance, for the sama5d27-wlsom1-ek-sd graphic image type of SDK, you can find it available in: tmp/deploy/sdk/poky-atmel-glibc-x86_64-microchip-graphics-image-cortexa5t2hf-neon-vfpv4-sama5d27-wlsom1-ek-sd-toolchain-5.0.3.sh
Install Poky SDK
Once the SDK archive is generated, you can install it by running the script directly. Choose the appropriate script name according to your board.
Note that some of the SDK variants can apply on several boards or SoC (sama5d2 or sama5d4 SDK could match all boards equipped with these SoCs). You can check the Yocto Project SDK table for more information about the different SDK "flavors".
Some installation information will be asked to the user as well as the appropriate installation rights:
Hereunder is an example with a SDK from the Scarthgap branch of OpenEmbedded present in Linux4SAM 2024.10:
$./linux4sam-poky-Cortex-A5-sdk-2024.10.sh Poky (Yocto Project Reference Distro) SDK installer version 5.0.3 ================================================================= Enter target directory for SDK (default: /opt/poky-atmel/5.0.3): You are about to install the SDK to "/opt/poky-atmel/5.0.3". Proceed [Y/n]? y [sudo] password for administrator: Extracting SDK..................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /opt/poky-atmel/5.0.3/environment-setup-cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi
Use Poky SDK
The installation directory (/opt/poky-atmel/5.0.3) contains a setup script which can be sourced to initialize all required environment variables.
$ cd /opt/poky-atmel/5.0.3/ $ source environment-setup-cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi
You can check your new environment
export | less [...] declare -x AR="arm-poky-linux-gnueabi-ar" declare -x ARCH="arm" declare -x AS="arm-poky-linux-gnueabi-as " declare -x CC="arm-poky-linux-gnueabi-gcc -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a5 -fstack-protector-strong -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -D_TIME_BITS=64 -D_FILE_OFFSET_BITS=64 --sysroot=/opt/poky-atmel/5.0.3/sysroots/cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi" [...] declare -x CFLAGS=" -O2 -pipe -g -feliminate-unused-debug-types " declare -x CONFIG_SITE="/opt/poky-atmel/5.0.3/site-config-cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi" declare -x CPP="arm-poky-linux-gnueabi-gcc -E -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a5 -fstack-protector-strong -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -D_TIME_BITS=64 -D_FILE_OFFSET_BITS=64 --sysroot=/opt/poky-atmel/5.0.3/sysroots/cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi" declare -x CROSS_COMPILE="arm-poky-linux-gnueabi-" [...] declare -x CXX="arm-poky-linux-gnueabi-g++ -mthumb -mfpu=neon-vfpv4 -mfloat-abi=hard -mcpu=cortex-a5 -fstack-protector-strong -O2 -D_FORTIFY_SOURCE=2 -Wformat -Wformat-security -Werror=format-security -D_TIME_BITS=64 -D_FILE_OFFSET_BITS=64 --sysroot=/opt/poky-atmel/5.0.3/sysroots/cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi" declare -x CXXFLAGS=" -O2 -pipe -g -feliminate-unused-debug-types " declare -x LD="arm-poky-linux-gnueabi-ld --sysroot=/opt/poky-atmel/5.0.3/sysroots/cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi" declare -x LDFLAGS="-Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -Wl,-z,relro,-z,now" [...] declare -x OECORE_DISTRO_VERSION="5.0.3" [...]
To be able to compile the EGT demo applications provided in the Linux4SAM release, SDK needs to be generated using a clone of meta-atmel
.
EGT demo applications can be compiled using the poky SDK by following the below steps
$ source /opt/poky-atmel/5.0.3/environment-setup-cortexa5t2hf-neon-vfpv4-poky-linux-gnueabi $ git clone --recursive https://github.com/linux4sam/egt.git $ cd egt/ $ ./autogen.sh $ ./configure --host="arm" $ make
To use the SDK toolchain directly one can refer to the Yocto Project documentation
.
Tips & tricks
BitBake
- BitBake User Manual

- BitBake Cheat Sheet

- List tasks provided by a package:
bitbake -c listtasks <package_name>You can use one of those tasks to have a fine grained control over the package building.
Hello World example
Reference to the "Hello World" example
.
Recent FAQ
• Using Systemd: Basic systemd user guide.
• Sam 9 x 60 Ek Attaching Tm 5000 Display: Addition to the other generic FAQ about LCD displays: ConnectModuleFromPDA.
• Audio FAQ: Audio with ALSA. ()
• Gui Solutions: Presentation of some GUI solutions.
• Yocto Project FAQ: Some Yocto Project FAQ entries.