Interfacing SAMA7G5 With Parallel OMNIVISION® OV7740 Sensor

Last modified by Microchip on 2026/01/09 08:12

This page describes the possibility of connecting a parallel sensor (example given is OMNIVISION® OV7740) to the SAMA7G5 microprocessor (MPU).

Warning

Warning: The SAMA7G5-EK board does not have a parallel sensor connector. This tutorial applies to custom boards that use this type of interface.

Introduction

OMNIVISION OV7740 is a parallel sensor , 8-bit raw Bayer, that can also stream directly in YUYV format.

Warning

Warning: Being a parallel sensor, all sensor data lines must be connected to the Image Sensor Controller (ISC) I/O lines.

Warning

Warning: SAMA7G5 uses the media controller paradigm to configure the pipeline. Please refer to the "Media Controller Pipeline for Image Acquisition and SAM MPU Products" page for more information.

Device Tree Configuration

This is an example device tree configuration. It uses a specific ISC I/O IOSET. One has to adapt this to its own board. The example shows how to connect endpoints between the different nodes in the device tree, to have everything in place for a parallel capture.

The snippet below assumes that all nodes in sama7g5.dtsi are available as in the Linux® mainline tree. The properties that are already in Linux mainline are not duplicated here. The following snippet can be added as an overlay or directly to your board dts file because it uses references to already existing nodes from sama7g5.dtsi.

&csi2dc {
      /* this clock is requested by the csi2dc from the xisc,
        * and then it's passed to the sensor. It is mandatory to
        * request the same frequency, otherwise the clock subsystem
        * will change the frequency to the last one requested */
    
        assigned-clock-rates = <24000000>;                                                 
        status = "okay";                                                         
                                                                                
        ports {                                                                  
                port@0 {                                                         
                       csi2dc_in: endpoint {
                               /* csi2dc will automatically understand from the endpoint if this is a Parallel or CSI2 endpoint connection */                                    
                                remote-endpoint = <&ov7740_0>;                   
                        };                                                       
                };                                                               
        };                                                                       
};      

&flx1 {
      /* make sure flexcom1 is in TWI mode for the i2c1 subnode below... */
       atmel,flexcom-mode = <ATMEL_FLEXCOM_MODE_TWI>;
};
                                                                                
&i2c1 {                                                                          
      #address-cells = <1>;                                                     
      #size-cells = <0>;                                                        
                                                                                
      ov7740: camera@21 {                                                       
               compatible = "ovti,ov7740";                                       
               reg = <0x21>;                                                     
               pinctrl-names = "default";                                        
               pinctrl-0 = <&pinctrl_sensor_power &pinctrl_sensor_reset>;        
               reset-gpios = <&pioA PIN_PA13 GPIO_ACTIVE_LOW>;                   
               powerdown-gpios = <&pioA PIN_PA12 GPIO_ACTIVE_HIGH>;              
               clocks = <&xisc>;                                                 
               clock-names = "xvclk";     /* be careful at the clock name, to be the one expected by the driver */                                       
               assigned-clocks = <&xisc>;                                        
               assigned-clock-rates = <24000000>;  /* also requested by csi2dc above */                              
               status = "okay";                                                  
                                                                                
               port {                                                            
                      ov7740_0: endpoint {                                      
                               remote-endpoint = <&csi2dc_in>;                   
                               hsync-active = <1>;                               
                               vsync-active = <0>;                               
                               pclk-sample = <1>;                                
                       };                                                        
               };                                                                
       };                                                                        
};             

                                                                                
&pioA {                                                                          
      pinctrl_sensor_power: sensor_power {                                      
               pinmux = <PIN_PA12__GPIO>;                                        
               bias-disable;                                                     
       };                                                                        
                                                                                
      pinctrl_sensor_reset: sensor_reset {                                      
               pinmux = <PIN_PA13__GPIO>;                                        
               bias-disable;                                                     
       };                                                                        
};                                                                               
                                                                                
&xisc {                                                                          
       pinctrl-names = "default";                                                
       pinctrl-0 = <&pinctrl_isc_base &pinctrl_isc_data_8bit>;                   
       status = "okay";                                                          
                                                                                
       port {                                                                    
              xisc_in: endpoint {                                               
                       hsync-active = <1>;                                       
                       vsync-active = <0>;                                       
                       pclk-sample = <1>;                                        
               };                                                                
       };                                                                        
};                                                                               
                                                                                    
&pioA {                                                                          
      pinctrl_isc_base: isc_base {                                              
               pinmux = <PIN_PA27__ISC_PCK>,                                     
                       <PIN_PA25__ISC_VSYNC>,                                   
                       <PIN_PA24__ISC_HSYNC>,                                   
                       <PIN_PA15__ISC_MCK>;                                     
               bias-disable;                                                     
       };                                                                        
       
      /* ISC uses the top data bits always, if your sensor outputs 10 bits e.g., you need to use D2-D11 */                                                                         
      pinctrl_isc_data_8bit: isc_data_8bit {                                    
               pinmux = <PIN_PA31__ISC_D11>,                                     
                       <PIN_PA30__ISC_D10>,                                     
                       <PIN_PA29__ISC_D9>,                                      
                       <PIN_PA28__ISC_D8>,                                      
                       <PIN_PA23__ISC_D7>,                                      
                       <PIN_PA22__ISC_D6>,                                      
                       <PIN_PA21__ISC_D5>,                                      
                       <PIN_PA20__ISC_D4>;                                      
               bias-disable;                                                     
       };                                                                        
};                                                                               
     

Back to Top

Media Controller Pipeline

If probed correctly, the media controller pipeline looks like this: 

# media-ctl -p
Media controller API version 5.16.0

Media device information
------------------------
driver          atmel_isc_commo
model           microchip,sama7g5-isc
serial
bus info        platform:microchip-sama7g5-xisc
hw revision     0x220
driver version  5.16.0

Device topology
- entity 1: atmel_isc_scaler (2 pads, 2 links)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev0
       pad0: Sink
                [fmt:SBGGR8_1X8/3264x2464 field:none colorspace:srgb
                 crop.bounds:(0,0)/3264x2464
                crop:(0,0)/3264x2464]
               <- "csi2dc":1 [ENABLED,IMMUTABLE]
       pad1: Source
                [fmt:SBGGR8_1X8/3264x2464 field:none colorspace:srgb]
               -> "atmel_isc_common":0 [ENABLED,IMMUTABLE]

- entity 4: csi2dc (2 pads, 2 links)
            type V4L2 subdev subtype Unknown flags 0
            device node name /dev/v4l-subdev1
       pad0: Sink
                [fmt:SRGGB8_1X8/640x480 field:none colorspace:srgb]
               <- "ov7740 0-0021":0 [ENABLED]
       pad1: Source
                [fmt:SRGGB8_1X8/640x480 field:none colorspace:srgb]
               -> "atmel_isc_scaler":0 [ENABLED,IMMUTABLE]

- entity 7: ov7740 0-0021 (1 pad, 1 link)
            type V4L2 subdev subtype Sensor flags 0
            device node name /dev/v4l-subdev2
       pad0: Source
                [fmt:YUYV8_2X8/640x480@1/60 field:none colorspace:srgb]
               -> "csi2dc":0 [ENABLED]

- entity 17: atmel_isc_common (1 pad, 1 link)
             type Node subtype V4L flags 1
             device node name /dev/video0
       pad0: Sink
               <- "atmel_isc_scaler":1 [ENABLED,IMMUTABLE]

#

The pipeline can be also represented as a graph, as in the accompanying image:

pipeline graph

Back to Top

Capturing

Capturing YUYV Directly From the Sensor

v4l2-ctl -v pixelformat=YUYV,height=480,width=640   # configure video format to YUYV packed 16 bits per pixel                             
media-ctl --set-v4l2 '"ov7740 0-0021":0[fmt:YUYV8_2X8/640x480@1/60 field:none colorspace:srgb]' # configure sensor to stream YUYV directly in 2 bytes per pixel 2x8
media-ctl --set-v4l2 '"csi2dc":0[fmt:YUYV8_2X8/640x480 field:none colorspace:srgb]' # configure csi2dc accordingly
media-ctl --set-v4l2 '"atmel_isc_scaler":0[fmt:YUYV8_2X8/640x480 field:none colorspace:srgb]' # configure scaler accordingly
fswebcam -r 640x480 -p YUYV -S 20 test.jpg        # capture YUYV packed 2 bytes per pixel at 640x480                               

Capturing RAW From Sensor and Converting in the ISC

v4l2-ctl -v pixelformat=YU12,height=480,width=640    # configure video format to YUV planar 4:2:0                             
media-ctl --set-v4l2 '"ov7740 0-0021":0[fmt:SBGGR8_1X8/640x480@1/60 field:none colorspace:srgb]' # configure sensor to stream raw bayer BGGR 8 bits
media-ctl --set-v4l2 '"csi2dc":0[fmt:SBGGR8_1X8/640x480 field:none colorspace:srgb]' #configure csi2dc accordingly
media-ctl --set-v4l2 '"atmel_isc_scaler":0[fmt:SBGGR8_1X8/640x480 field:none colorspace:srgb]' #  configure scaler accordingly
fswebcam -r 640x480 -p YUV420P -S 20 testplanar.jpg    # simple capture at 640x480 in YUV4:2:0 planar                          

Supported Sensor Formats

We can always query the sensor for which formats it supports:

# v4l2-ctl -d /dev/v4l-subdev2 --list-subdev-mbus-codes
ioctl: VIDIOC_SUBDEV_ENUM_MBUS_CODE (pad=0)
       0x2008: MEDIA_BUS_FMT_YUYV8_2X8
       0x3001: MEDIA_BUS_FMT_SBGGR8_1X8
#

Back to Top

Related Topics

Boards

Components

Back to Top

Summary

This article explained how to interface the OMNIVISION OV7740 parallel image sensor with the SAMA7G5 microprocessor, focusing on custom board implementations since the SAMA7G5-EK does not include a parallel sensor connector. It detailed the necessary device tree configuration, media controller pipeline setup, and commands for capturing both YUYV and raw Bayer formats from the sensor. Supported sensor formats and provides example commands for configuring and capturing images using Linux media tools were highlighted.

Back to Top