customize-at91-bootstrap
Last modified by Microchip on 2025/07/17 06:40
Customize AT91Bootstrap
If the default configuration doesn't meet your need, after configuring with the default configuration, you can customize it by doing:
$ make menuconfig
Now, in the menuconfig dialog, you can easily add or remove some features to/from AT91Bootstrap as the same way as kernel configuration.
Move to <Exit> with arrows and press this button hitting the Enter key to exit from this screen.
Build AT91Bootstrap
Then you can build the AT91Bootstrap binary by doing:
$ make
If the building process is successful, the final .bin image is build/binaries/at91bootstrap.bin.