dsPIC® ADC Applications
Contents
Some of the dsPIC® digital power conversion applications, such as Power Factor Correction (PFC), and Full-Bridge Zero Voltage Transition (ZVT) Converter are covered on the Power Operations page. The following section covers a digital power conversion application, specifically on the Boost Converter, in relation to using dsPIC DSC ADC.
dsPIC DSC Boost Converter Application
A Boost Converter is one of the most popular DC/DC Converter topologies. A boost converter steps up the voltage from a lower rectified input voltage to a higher regulated output voltage. The accompanying figure illustrates the concept of the boost converter using an inductor (L), switch, diode (D), and output capacitor (Co).

In the accompanying image, we see a practical example of using a dsPIC33FJ32GS406 in a boosted Power Factor Correction (PFC) converter application.

Just like the boost converter, the boost PFC converter produces a voltage higher than the input rectified voltage. Therefore, the switch (MOSFET) should be rated higher than the output voltage. The accompanying figure shows the Boost PFC input current shape.

PFC Theory
Most of the power conversion applications consist of an AC-to-DC conversion stage immediately following the AC source. The accompanying figure shows a high-level block diagram of the Switched-Mode Power Supply (SMPS) AC-to-DC conversion design.

Since many applications demand a DC voltage source, a rectifier with a capacitive filter is necessary. Current pulses with high peak amplitude are drawn from this rectified voltage source. Please refer to the input current waveform of the PFC boost converter above. The current drawn is of short duration regardless of the load connected to the system and discontinuous. When this type of current is drawn from the mains supply, the resulting network losses, the total harmonic content, and the radiated emissions become significantly higher. At power levels of more than 500 watts (W), these problems become more pronounced. This leads to the implementation of the Power Factor Correction (PFC) using dsPIC DSC. Because Power Factor (PF) is a parameter that gives the amount of working power used by any system in terms of the total apparent power.
Power Factor = Real Power / (Voltage * Ampere)
Power Factor becomes an important measurable quantity because it often results in significant economic savings. The waveforms of the current with and without PFC are shown in the accompanying image. These waveforms show that the PFC can improve the input current drawn from the main supply and reduce the DC voltage ripple. The results of these are energy consumption reduction and an increase in power efficiency. Without PFC, the ratio of the power factor deviates from a constant, the input contains phase displacement, harmonic distortion, or both, which ultimately degrades the Power Factor.

In a DSC-based application, the relevant analog parameters and the control loops need to be redefined. By doing this, change-over from existing analog hardware to its digital counterpart is easier and more logical. The basic function of PFC is to make the input current drawn from the system sinusoidal and in-phase with the input voltage. The accompanying figure shows the component blocks required for PFC and the PFC stage interfaced to a dsPIC DSC device. This is an AC-to-DC converter stage, which converts the AC input voltage to a DC voltage and maintains sinusoidal input current at a high input Power Factor. As indicated in the block diagram, three input signals are required to implement the control algorithm.

The high-speed 10-bit ADC module converts the analog inputs in pairs. This module supports up to 24 external analog inputs and two internal analog inputs. To monitor the reference voltages, two internal inputs: AN24 and AN25, are connected to the external reference source (EXTREF) and internal band gap voltages (1.2V), respectively. The 26 analog inputs available on the ADC module are grouped into thirteen analog input pairs. Each analog input pair is a combination of an even and odd numbered analog input, such as AN0 and AN1, AN2 and AN3, and so on. The technique of using pairs is particularly useful in power conversion applications that require voltage and current measurements for each PWM control loop.
The first four even numbered analog inputs in both single and dual SAR devices have a dedicated Sample & Hold (S&H) circuit. For example, the dedicated S&H circuit (SH0) samples AN0 (see accompanying figure). On a conversion request, the dedicated S&H circuit allows the corresponding analog input to be sampled without any latency (zero latency).

In the boost circuit (see the accompanying figure), the dedicated S&H circuit samples the peak inductor current measurement with zero latency. Any latency in sampling would lead to an incorrect result.
ADC Interrupt Service Routine
The ADC Interrupt Service Routine (ISR) is the heart of the control algorithm. All control loops are executed in the ISR. Since faster control loop execution is desired for the best system performance, functions executed in this routine, as well as other time-critical functions are usually written in Assembly language. On the other hand, the main loop, peripheral setup routines, and initialization routines are written using C.
In terms of execution priority, the ADC ISR has the highest priority for execution. The ADC module is configured to generate interleaved interrupt requests in order to execute multiple control loops within the same ISR. The accompanying flowchart shows the SMPS AC-to-DC reference design following a single basic structure.

ADC Module Registers
The following lists the specific functions of the high-speed 10-bit ADC module registers:
| Register Name | Descriptions |
| ADCON: ADC Control Register | This register configures the sample conversion sequence, enables the ADC module, and is used to set up the clock divider for the ADC clock. |
| ADSTAT: ADC Status Register | This register contains the Pair Data Ready (PxRDY) flag to indicate the analog input pair that caused the common ADC interrupt. The Pair Data Ready flag is cleared in the specific pair handler. |
| ADBASE: ADC Base Register(1,2) | This register contains a unique offset value based on the analog input pair that caused the common ADC interrupt. It is read in the common ADC interrupt to branch to the specific analog pair handler. |
| ADPCFG: ADC Port Configuration Register | This register configures the analog input pins as analog inputs or digital I/O. |
| ADPCFG2: ADC Port Configuration Register 2 | This register configures the analog input pins as analog inputs or digital I/O. |
| ADCPC0: ADC Convert Pair Control Register 0 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 0 and Pair 1. |
| ADCPC1: ADC Convert Pair Control Register 1 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 2 and Pair 3. |
| ADCPC2: ADC Convert Pair Control Register 2 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 4 and Pair 5. |
| ADCPC3: ADC Convert Pair Control Register 3 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 6 and Pair 7. |
| ADCPC4: ADC Convert Pair Control Register 4 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 8 and Pair 9. |
| ADCPC5: ADC Convert Pair Control Register 5 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 10 and Pair 11. |
| ADCPC6: ADC Convert Pair Control Register 6 | This register selects the trigger source, enables the common ADC interrupt, and allows software trigger generation for Analog Input Pair 12. |