Transition to Digital ADC
Each Pulse Width Modulation (PWM) in the dsPIC33E/33F device can generate a trigger to the Analog-to-Digital (ADC) module to sample the analog signal at a specific instance during the PWM period. In addition, the High-Speed PWM module generates a Special Event Trigger for the ADC module based on the master time base. The table in Figure 1 shows the dsPIC33F device names, pin counts, memory sizes, and peripheral availability of each device. Please note the ADC module in the red box.

Figure 1
Figure 2 shows the interconnection between various registers in the High-Speed PWM module. Note the ADC module in the bottom left showing the triggering interface from the PWM generator.

Figure 2
PWM Triggers
In digital power supplies, the ADC is used for the measurement of feedback signals. This means that a trigger signal is required by the ADC peripheral to start the conversion operation. This allows the user to select the correct instant in time when the voltage or current should be acquired. Because these feedback signals can have complex waveforms or high noise content, precise triggering of the ADC is important.
For the ADC module, the TRIGx and STRIGx registers specify the triggering point for the PWMxH and PWMxL outputs, respectively. An ADC trigger signal is generated when the Independent Time Base Counter (PTMRx or STMRx) register value matches with the specified TRIGx or STRIGx register value. The PWM triggers (TRIGx/STRIGx) have a resolution of 8.32 ns (for a PWM resolution of 1.04 ns). In addition to the triggers generated by the TRIGx and STRIGx settings, the ADC pairs can also be triggered by the current-limit sources of individual PWM generators and the Special Event Trigger (SEVTCMP). The Trigger Output Divider bits (TRGDIV<3:0>) in the PWMx Trigger Control register (TRGCONx<15:12>) act as a postscaler for the TRIGx register to generate ADC triggers. This allows the trigger signal to the ADC to be generated once for every one, two, three… and 16 trigger events. These bits specify how frequently the ADC trigger is generated.

Figure 4
Figure 5 introduces the available options to generate the trigger signal.

Figure 5
The first set of triggers can be generated by the PWM peripheral's Period register, with an approach that is very similar to the one used to generate the PWM period and duty cycle.
On the top right, the ADC Trigger register and a comparator are added. Please note that this diagram does not exactly replicate the true hardware, but it is provided to show the operation. The comparator continuously compares the value of the ADC Trigger register with the value of the counter, which is counting up or down. When the two values match, the trigger signal is generated and the ADC starts the sampling operation.
Each PWM generator consists of the Trigger Postscaler Start Enable Select bits, TRGSTRT<5:0> (TRGCONx<5:0>), that specify how many PWM cycles to wait before generating the first ADC trigger. The logic for ADC triggering by the High-Speed PWM module is shown in Figure 6.

Figure 6
Dual Trigger to Analog-to-Digital Converter (ADC) per PWM Period
One of the high-speed PWM module features is the Dual Trigger from PWM to ADC per PWM period. The trigger is controlled by the TRGCONx.

Figure 7
Dual Trigger Mode Bit (DTM)
- 1 = Secondary trigger event is combined with the primary trigger event to create the PWM trigger
- 0 = Secondary trigger event is not combined with the DTM: Dual Trigger Mode bit
- 1 = Secondary trigger event is combined with the primary trigger event to create the PWM trigger
- 0 = Secondary trigger event is not combined with the primary trigger event to create the PWM trigger; two separate PWM triggers are generated
Incorrect triggering of the ADC may have a major impact on the operation of the power converter. Figure 8 demonstrates the need for precise ADC triggering. The converter example is a DC-DC boost converter with the current sensor located in series with the source pin of the power MOSFET. This configuration eliminates the need for a differential amplifier with a high common-mode voltage capability, providing a low-cost sensing solution. The trade-off is that the ADC only sees the MOSFET current. If the digital control system is configured to measure the peak current, a small delay in triggering the ADC will yield a result of 0x0000. This delay may be caused by software overhead or if the ADC is busy at the sampling instant.

Figure 8
We can see from the PWM, inductor, and resistor current waveforms in Figure 9 that the late sample of the peak inductor current causes zero ADC sampled data, which alters the boost converter's transfer function. By using the flexible ADC triggering features of the High-Speed PWM module, this guarantees that the ADC conversion is triggered exactly when needed by the circuitry.

Figure 9
Special Event Trigger
The Special Event Trigger is commonly used when all the PWM signals have the same frequency. A single trigger can be used to start the ADC operation. The High-Speed PWM module consists of a master Special Event Trigger that can be used as a CPU interrupt source and for synchronization of Analog-to-Digital conversions with the PWM time base. The Analog-to-Digital sampling time can be programmed to occur at any time within the PWM period. The Special Event Trigger allows the user-assigned application to minimize the delay between the time the Analog-to-Digital conversion results are acquired and the time the duty cycle value is updated. The Special Event Trigger is based on the Master Time Base. Figure 10 shows the Master Time Base block diagram.

Figure 10
The master Special Event Trigger value is loaded into the PWMx Special Event Compare register (SEVTCMP/SSEVTCMP). In addition, the PWM Special Event Trigger Output Postscaler Select bits (SEVTPS<3:0>) in the PWMx Time Base Control register (PTCON<3:0>) or the PWMx Secondary Master Time Base Control register (STCON<3:0>) control the Special Event Trigger operation. To generate a trigger to the ADC module, the value in the PWM Master Time Base Counter (PMTMR/SMTMR) is compared to the value in the SEVTCMP/SSEVTCMP register. The Special Event Trigger consists of a postscaler that allows 1:1 to 1:16 postscaler ratio. The postscaler is configured by writing to the SEVTPS<3:0> control bits (PTCON<3:0>). Special Event Trigger pulses are generated if the following conditions are satisfied:
- On a match condition, regardless of the status of the Special Event Trigger Interrupt Enable bit, SEIEN bit (PTCON<11>)
- If the compare value in the SEVTCMP/SSEVTCMP register is a value from zero to a maximum value of the PTPER/STPER register
The Special Event Trigger output postscaler is cleared on these events:
- Any device Reset
- When PTEN = 0 (PTCON<15>)
The configuration of the ADC Special Event Trigger is shown in the following code box.
2 SEVTCMP = 1248; /* Special Event Trigger value set at ~25%
3 of period value (4999)*/
4 PTCONbits.SEVTPS = 0; /* Special Event Trigger output postscaler
5 set to 1:1 selection (trigger generated
6 every PWM cycle */
7 PTCONbits.SEIEN = 0; /* Special event interrupt is disabled */
8 while (PTCONbits.SESTAT == 0); /* Wait for special event status change */
ADC Triggers: Current Limit
The PWM active interval can be stopped by an external signal, e.g. current limit. At the same time, the trigger signal can be generated enabling the ADC to measure the current at that specific instant in time. Figure 11 shows the PWM signal stops upon the current limit event.

Figure 11
In the Figure 11 example, the current-limit input signal is used as a trigger signal to the ADC, which initiates an ADC conversion process. The ADC trigger signals are always active, regardless of the state of the High-Speed PWM module, the FLTMOD<1:0> bits (FCLCONx<1:0>) or the
FLTIEN bit (PWMCONx<12>).
In addition to generating ADC triggers, the Special Event Trigger can also be used to generate the primary and secondary Special Event Trigger interrupts on a compare match event.
ADC Sampling and Conversion
After the trigger signal is generated and the converted value is available in the ADC buffer, the sampling and conversion process begins. Figures 12 through 15 show a dual Successive Approximation (SAR) ADCs, using synchronous sampling and parallel conversion.

Figure 12

Figure 13

Figure 14

Figure 15