Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Key Power Stage Parameters: Vin, Vout and Iout
Last modified by Microchip on 2025/01/09 09:52
Understanding the fundamental parameters of a buck (step-down) converter is crucial for designing and evaluating power efficiency and performance. Here, we'll explore the roles of Input Voltage (Vin), Output Voltage (Vout), and Output Current (Iout) in the operation of these converters.
Vin (Input Voltage): This is the source voltage supplied to the buck converter. It's typically higher than the desired output voltage, allowing for the step-down conversion.
Vout (Output Voltage): The regulated voltage provided by the converter to the load. In a buck converter, Vout is always less than or equal to Vin, controlled by the duty cycle of the switch.
Iout (Output Current): Represents the current drawn by the load from the converter. The inductor in the circuit smoothens this current, maintaining a steady supply to the load, with Iout being proportional to the load demand and inversely related to the output voltage set by the converter's control.
Menu
Microchip Support
Query Microchip Forums and get your questions answered by our community:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.