Import Existing Project
                  Last modified by Microchip on 2023/11/09 08:54
              
      The Import Existing Project option will copy all the settings from a previously created DCDT project into a new folder and allow the user to give a new name to the project.
New Project
When creating a new project, you will define the project name and folder. The DCDT GUI will use this folder as the active project path and all the generated GUI files will be saved in this location.
It is not possible to create two projects using the same folder path (Project Location). You must create an individual folder for each project.