Symmetric Authentication with a Non-Secure MCU – Use Case Example
- Authentication
- to authenticate; to prove that something is real, true, or genuine.
In terms of system security, authentication is a process where a device provides information to the other to authenticate its identity. Depending on the use-case, there can be one-way authentication as well as two-way (mutual) authentication.
In this use case example, we will authenticate an object using one-way symmetric authentication. One-way symmetric authentication avoids the need for an Internet connection and white (or black) list. A white list is a lookup table for identifying approved units. A black list is a lookup table for identifying non-approved units.
The object can be any accessory—peripheral, battery, cartridge, etc. The purpose of authenticating an object is to ensure that it is genuine and it is authorized to connect to a product. Another purpose is to prevent cloning and counterfeiting.
Why you may want to use this method?
The Host Microcontroller does not contain a Secret key. Thus, compromise of the Secret Key is minimized. The Peripheral device does contain a hardware CryptoAuthentication™ device to store the Secret Key. This is an example of one-sided hardware protection using symmetric keys.
This method limits the target population and any hack to the one device, not the entire cryptosystem.
Implementation
Method A – If the Host Microcontroller has sufficient memory, the best solution is to calculate unique challenge-and-response sets for each device. These sets should be calculated in a secure production line. The challenge-and-response sets are compiled into the host microcontroller source code.
Method B – If the Host Microcontroller does not have sufficient memory, divide the production in some manner such as by work day, week, or month. This method has the advantages of (1) limiting any compromise to that subset of challenge-and-response sets, and (2) adding more variance and therefore making the ecosystem stronger.
Authentication Steps
The Host Microcontroller sends one of its precompiled challenges to the Peripheral device. The peripheral performs a Hash Function on the challenge and its securely stored Secret Key. This re-creates one of the Intermediate Keys precompiled in Flash.
The Host Microcontroller sends a random challenge to the Peripheral device. The Peripheral device performs a hash function with the random challenge and Intermediate Key.
The Host Microcontroller performs a hash function of the same random challenge and the associated precompiled Intermediate Key.
The result from the Peripheral device and the Host Microcontroller are compared. If the results are equal, the Peripheral device has been authenticated.

You can make the hacking of the devices even more difficult by:
- Obfuscate the challenge/response. The longer the code, the stronger the defense.
- Hash state variables with stored challenge set. Use state variables with known values at certain points in the algorithm. Authenticate at these points.
- Perform the challenge-and-response in multiple areas of the source code. Code them differently to make them more difficult to find. Use different challenge-and-response pairs.
- Do not return an error message immediately after an authentication failure. Do housekeeping tasks and other non-essential functions before faulting.
- If possible, randomly challenge. Avoid periodic challenges which can be anticipated.