MCC Classic mTouch® Capacitive Sensing Library Installation

Last modified by Microchip on 2026/03/10 12:58

The mTouch® Capacitive Sensing Library is a software library that can be loaded by the MPLAB® Code Configurator (MCC) Classic version. Please refer to the MCC installation instructions.

The mTouch library is included in the MCC Classic installation, but it is always a good idea to check the latest version of the library in the Current Download section of the MCC Classic website, because the mTouch library may be released independently of the MCC release. The release note associated with the library provides part support list, change log, etc.

mTouch Library in the list of libraries for MCC Classic latest download

If a newer version is found on the website, download the library file and unzip the .jar file, and then open up the Options windows of MPLAB X IDE, as shown in the figure.

Updating the mTouch Library in MCC Classic in the Options window

Click the Install Library button, and select the unzipped .jar file.
After adding the library file, restart the MPLAB X IDE.