Sensor Pin Manager
Last modified by Microchip on 2026/03/10 12:59
After the mTouch® Capacitive Sensing Solution Library is loaded, the 'CS' and 'Driven Shield' rows are populated in the Pin Manager Grid View.

You can select the pins that connect to the sensors and the 'Driven Shield' if needed. Once a 'CS' pin is chosen, the corresponding pin is populated into the Hardware Sensors panel.