Introduction to MPLAB® Data Visualizer Touch Plugin

Last modified by Microchip on 2026/03/10 12:59

Overview

This page provides information on using the Touch plugin for MPLAB® Data Visualizer.

Installation

Go to Menu > Tools > Plugins.


Select the MPLAB Touch plugin from the Available Plugins tab and click on Install.

MPLAB Touch plugin from the Available Plugins tab


Configuration

Touch Plug In Configuration View

Back to Top

Section I: Connection

Select the COM port in the Connections tab.

COM port view in the Connections tab


Update the Baud Rate in COM Settings.

Baud Rate setting in COM Settings


Start COM port streaming.

COM port serial streaming


Select Touch in the Connections tab.

Touch session indicator in the Connections tab


Choose the COM port as the data source.

Select COM port as the data source.


Start Touch streaming.

Start Touch streaming

Back to Top


Section II: Configuration

Select any one of the listed options other than Output Data. In this case, we selected Sensor Key Parameters.

Sensor Key Parameters Selected


Under the Configuration tab, select and modify any one of the parameters in the table.

Configuration tab view


Once the required parameters are changed, the Write to kit button changes its color to yellow. Then click on the Write to kit button. If the write is successful, the button will change to green indicating success; else, it will change to red, indicating an error with the kit.

Write to kit button and then click on the Write to kit button


Click on Read from Kit to retrieve the configuration from the kit.

Read from Kit view

Back to Top


Section III: Graph

For CVD Devices:

The Graph is automatically populated for Deviation and Pressed parameters for the sensors.

For PTC Devices:

The Graph is automatically populated for State and Delta parameters for the sensors.

Back to Top