QTouch® and mTouch® Solution Terminology
Last modified by Microchip on 2026/03/10 12:59
This table is based on QTouch® library v5.0 and mTouch® library v2.5.
| Parameter Categories | Parameter Description | Parameter Name in QTouch | Configurable in Atmel START | Parameter Name in mTouch | Configurable in MCC | Additional Details |
|---|---|---|---|---|---|---|
Touch Basic Terms | Sensor acquisition value | Signal | No | Reading | No | |
| Reference value used for touch detection | Reference | No | Baseline | No | ||
| Difference between acquisition and reference | Delta | No | Deviation | No | ||
| State of touch detection | Detect | No | Pressed | No | ||
| Measurement technique | Dual-slope measurement | No | Differential CVD | No | ||
| Sensor Definitions | Key sensor which reports ON/OFF status | Button | Yes | Button | Yes | |
| Linear touch sensor | Slider | Yes | Slider | Yes | ||
| Angular touch sensor | Wheel | Yes | Wheel | Yes | ||
| Proximity sensor | Button with high gain | Yes | Proximity | Yes | Proximity could be created by configuring a button with high gain and driven shield in QTouch. No specific configuration settings are available. | |
| Sensor Technology | Self-capacitance sensor | Selfcap | Yes | sensor | Yes | Requires one Y-line sense pin per button. |
| Mutual capacitance sensor | Mutualcap | Yes | Not Available | No | Requires one X-line drive pin and one Y-line sense pin per button. | |
| Sensor Acquisition Parameters | Touch measurement periodicity | Scan rate | Yes | Scan Rate | Yes | MCC mTouch configurator has options to control the scan rate using TMR1 and scan the sensor in free running mode. |
| Touch measurement frequency | Acquisition frequency | Yes | Not Available | No | ||
| Sensor acquisition interrupt priority | PTC interrupt priority | Yes | Not Available | No | PTC interrupt priority only applicable on SAM devices. | |
| Button Configuration Parameters | Sensor's detect threshold | Sensor detect threshold | Yes | Threshold | Yes | |
| Sensor's out-of-detect threshold | Sensor detect hysteresis | Yes | Sensor detect hysteresis | Yes | ||
| Group selection for adjacent key suppression | AKS group | Yes | AKS group | Yes | AKS can be used when touching multiple sensors is not allowed in a system. | |
| Method selection for button status update | Not Available | No | Interface method | Yes | Callback or polling needs to be used to notify/update the application. | |
| Slider/Wheel Configuration Parameters | No. of segments in a slider/wheel | No. of buttons | Yes | No. of Segments | Yes | |
| No. of unique positions reported by the slider/wheel | Resolution | Yes | Resolution | Yes | ||
| Inactive area on both ends of the slider | Dead band Percentage | Yes | Dead band Percentage | Yes | ||
| No. of positions you have to move before the touch position is reported | Position hysterisis | Yes | Position hysterisis | Yes | ||
| Slider/wheel detect threshold | Threshold | Yes | Threshold | Yes | ||
| Proximity Configuration Parameters | Gain for deviation integration filter | Not Applicable | No | Deviation integration filter: gain | Yes | |
| Enable median filter | Not Applicable | No | Median filter | Yes | ||
| Window for median filter | Not Applicable | No | Median filter: window | Yes | ||
| Sensor Node Parameters | Pin selection | Y-line, X-line | Yes | Pin | Yes | Mutual capacitance sensor requires one X-line drive pin and one Y-line sense pin per button. |
| Acquisition clock prescaler | Prescaler for PTC | Yes | Not Available | No | MCC mTouch configurator will calculate the prescaler for ADC based on Fosc automatically. | |
| Internal series resistor selection | Series resistor | Yes | Not Available | No | ||
| Gain setting for touch signal/reading | Digital/analog gain | Yes | Not Available | No | ||
| IIR filter for touch signal/reading | Not Available | No | Reading filtering: level | No | In mTouch, new reading is updated as ((oldreading-(oldreading»filter level))+(rawsample»filter level)). | |
| Gain setting for touch reference/baseline | Not Available | Yes | Baseline filtering: gain | Yes | In mTouch, new baseline is updated as ((oldbaseline-(oldbaseline»gain))+reading). | |
| Scaling for deviation | Not Available | No | Deviation scaling | Yes | In mTouch, the deviation value is calculated as ((reading - baseline)»scaling). | |
| Number of samples taken for each measurement | Filter level | Yes | Oversample | Yes | ||
| Sensor charging time | Charge share delay (CSD) | Yes | Precharge time | Yes | CSD indicates the number of additional cycles that are inserted within a touch measurement cycle. Precharge time is the amount of time spent charging the internal and external capacitors. | |
| Settling time delay | Not Applicable | No | Acquisition time | Yes | Acquisition time is the amount of time spent allowing the capacitors to equalize to a median voltage after being precharged to opposite states. | |
| Additional internal capacitance to the sensor nodes | Not Available | No | Additional sample capacitance | Yes | This is used to improve the match between internal and external capacitance for a better sensing performance. | |
| Sensor Configuration Parameters | Enable auto-calibration | Sensor charge time auto-tune | Yes | Auto-calibration | Yes | For AVR devices, enabling this setting will automatically set the number of additional charge cycles needed to ensure full charging of the touch sensor. For SAM devices, enabling this setting will automatically set the pre-scaler setting needed to ensure full charging of the touch sensor. For PIC devices with HCVD, enabling this setting will automatically set acquisition time and additional internal capacitor. When the option is disabled, you need to manually set these parameters and ensure full charge transfer of the touch sensor. |
| Enable noise performance improvement and water tolerance | Enable driven shield | Yes | Driven shield | Yes | Both QTouch and mTouch can assign a dedicated driven shield pin. Having a dedicated shield improves both noise performance and water tolerance. PTC devices, PIC16LF156x and ADCC devices can drive non-scanning sensors as the shield, which improves water tolerance. | |
| Sensor Touch Parameters | No. of additional touch measurements to confirm touch | Detect integration (DI) | Yes | Debounce | Yes | |
| No. of additional touch measurements to confirm an out-of-touch detection | Away from touch detect integration | Yes | Debounce | Yes | ||
| Threshold for out-of-touch recalibration | Away from touch recalibration threshold | Yes | Negative threshold | No | Negative threshold is configurable in mTouch code and not in MCC. | |
| No. of additional touch measurements to confirm out-of-touch recalibration | Not Available | No | Consecutive decodes | Yes | ||
| Rate of change of reference (baseline) for positive delta (deviation) | Towards touch drift rate | Yes | Baseline filtering: update | Yes | For QTouch, value is scaled by 200 ms. In mTouch, a baseline update is done after this number of sensing cycles. | |
| Rate of change of reference (baseline) for negative delta (deviation) | Away from touch drift rate | Yes | Baseline filtering: update | Yes | Common value for towards touch and away from touch in mTouch. For QTouch, the value is scaled by 200 ms. | |
| Amount of time the change of reference needs to be paused after removing the finger | Drift hold time | Yes | Baseline Hold | No | Value is scaled by 200 ms for QTouch. This is configurable in the firmware for mTouch. | |
| Re-bursting mode | Re-burst mode | Yes | Re-burst mode | Yes | ||
| Enable sensor ON timeout | Max-ON duration (MOD) | Yes | Press timeout | Yes | Set the value of MOD as zero in Atmel START to disable sensor ON timeout in QTouch. | |
| Sensor ON timeout unit | Not Available | No | Press timeout unit | Yes | In QTouch, unit is time in ms. In mTouch, the unit is main loop task calls by default. | |
| Set maximum sensor ON time/counts | Max-ON duration (MOD) | Yes | Press timeout counts | Yes | In QTouch, value is scaled by 200 ms. | |
| Frequency Hop Parameters | Enable multiple burst frequencies | Enable frequency hop | Yes | Enable AFA | Yes | Frequency hopping is enabled by default in mTouch. |
| Enable auto changing of burst frequency | Enable frequency auto tuning | Yes | Automatic frequency adaptation | Yes | Intelligently choose scan frequency at run-time to avoid noise frequency and its harmonics. | |
| Timer selection for frequency hop | Not Available | No | AFA filter timer | Yes | The PIC with ADCC doesn't need a timer to implement the frequency hopping. | |
| Number of frequencies used in touch measurement | Frequency steps | Yes | Max/Min Frequency | No | The mTouch will pick the frequencies in a range, which is configurable in the firmware. | |
| Threshold for noise frequency replacement | Maximum variance | Yes | Noise Threshold | No | This can be configured in the firmware for mTouch. | |
| Count for noise frequency replacement | Tune in count | Yes | Over Limit Threshold | No | This can be configured in the firmware for mTouch. | |
| Clock Configuration Settings | Oscillator selection | Oscillators | Yes | Oscillator select | Yes | Select the oscillator from the list. |
| External clock selection | Oscillators | No | External clock select | Yes | Select the external clock source from the list if an external oscillator is selected. | |
| Internal clock frequency selection | Clock settings: prescaler | Yes | HF internal clock | Yes | Set the internal clock frequency by selecting the prescaler value. | |
| External clock frequency selection | Frequency | Yes | External clock | Yes | Enter the external clock frequency if an external oscillator is selected. | |
| Clock source prescaler | Generic clock generator division | Yes | Clock divider | Yes | The internal/external clock selected is divided by this prescaler. | |
| Enable low voltage programming | Not Available | No | Low voltage programming enable | Yes | ||
| CPU and peripheral clock selection | Clock source | Yes | Not Available | No | Select the clock generator source for CPU and components from the list in QTouch. | |
| CPU clock divider | CPU clock prescaler | Yes | Not Available | No | The CPU frequency will be the generic clock selected for the CPU divided by the prescaler. | |
| Enable watchdog timer | Not Available | No | Watchdog timer enable | Yes |