Guide for Slider Sensor Design When Using Modular QTouch® Library

Last modified by Microchip on 2026/03/10 13:00

This article provides guidelines for designing a self-capacitance slider. A suitable design should be chosen based on the width requirements of the slider. This slider design should be used when using Atmel START-based QTouch® Modular Library.

When using the Microchip Studio-based QTouch library, the slider design guidelines provided in "Section 5" of the " Capacitive Touch Sensor Design Guide" should be used. For mutual capacitance slider design, refer to "Section 6" of the " Capacitive Touch Sensor Design Guide".

Note: The Y line numbers indicated in the images represent the order only and NOT the actual PTC Y lines. The PTC Y line can be connected in any order.

Back to top

Small Width Slider

Example of small width slider sensor layout

Back to top

Medium Width Slider

Example of medium width slider sensor layout

Back to top

Large/Wide Width Slider

Example of large width slider sensor layout