Step by Step Examples of Using the MCC Melody mTouch® Capacitive Sensing Library Module
Last modified by Microchip on 2026/02/26 08:50
The following tutorials demonstrate how to use the MPLAB® Code Configurator (MCC) Melody mTouch® Capacitive Sensing Library Module to implement and debug various touch sensing elements in an MPLAB X IDE project.
The "Generate a Generic Touch Sensing Project with MCC Melody" page demonstrates how to create a generic project and add touch elements like buttons, sliders, and touch surfaces. It also demonstrates the windows for adjusting the settings of the sensors once they have been added to the project.