Guide to Interpreting CC Calibration Value for Atmel START QTouch Library

Last modified by Microchip on 2026/02/26 08:50

This page provides information on computing sensor capacitance values using the Compensation Capacitor (CC) value. The CC value is also called the CC calibration value as it is computed during the calibration phase. The CC value of each touch button can be obtained as follows:

uint16_t cc_value = ptc_qtlib_node_stat1[SENSOR_NUMBER].node_comp_caps;

The unsigned 16-bit CC values are stored as node_comp_caps in Peripheral Touch Controller (PTC) CC register format.

PTC CC Register Format

Depending on the device, the CC register format changes.

CC register for SAM and ATmega devices

CC register for ATtiny devices using self-capacitance

CC register for ATtiny devices using mutual-capacitance

Back to Top


CC Register Bit Values

CC register Course/Fine/Accurate bit values

CC register Rough bit values

CC register Rough Additional bit values

Back to Top


Computing Sensor Capacitance

SAMD20/SAMD21/SAMDA1/SAMD10/SAMD11, ATmega328PB/ATmega324PB, SAML21/SAML22/SAMC20/SAMC21/SAMHA1 Devices

  • Read CC value in decimal: 11639
  • Read CC value in hexadecimal: 0x2D77
  • Substitute the rough, coarse, fine and accurate values from the table
    • Rough: 2*6.75 = 13.5
    • Coarse: 13*0.675 = 8.775
    • Fine: 7*0.0675 = 0.4725
    • Accurate: 7*0.01 = 0.07

Sensor Capacitance (pF) = Rough + Coarse + Fine + Accurate = 22.82 pF (maximum 31 pF)

ATtiny81x/ATtiny161x/ATtiny321x - Self-Capacitance

  • Read CC value in decimal: 46967
  • Read CC value in hexadecimal: 0xB777
  • Substitute the rough, coarse, fine and accurate values from the table
    • Rough Addition: 2*6.2 = 12.4
    • Rough: 3*6.75 = 20.25
    • Coarse: 7*0.675 = 4.725
    • Fine: 7*0.0675 = 0.4725
    • Accurate: 7*0.01 = 0.07

Sensor Capacitance (pF) = Rough Addition + Rough + Coarse + Fine + Accurate = 37.92 pF (maximum 51 pF)

Back to Top


AVRDA

Self-Capacitance
Sensor Capacitance value = (CC value + 1) * 0.03125 * 2
Mutual Capacitance
Sensor Capacitance value = (CC value + 1) * 0.03125

Back to Top


SAME54/SAME53/SAME51/SAMD51/SAML10/SAML11 - Maximum Sensor Capacitance

Self-Capacitance
Here, the internal compensation capacitance can compensate twice the sensor capacitance.
The maximum supported sensor capacitance is twice the maximum compensation capacitance value (2 * 32 pF).
So, if computed capacitance from CC is 10 pF, then actual sensor capacitance is 20 pF.

Mutual Capacitance
The maximum sensor capacitance is the same as the maximum compensation capacitance value, which is 32 pF.

Back to Top


PIC32CZCA

The compensation capacitance values for PIC32CZCA are calculated as "(((X & 0x1F)+1)*0.075)+(((X » 8) & 0x1F)*1.5)" for mutual capacitance technology and for self-capacitance, the value is multiplied by 2.

Mutual Capacitance

  • Read CC value in decimal: 2568
  • Read CC value in hexadecimal: 0x0A08
  • Calculate the coarse and fine values
    • Coarse: A*1.5pF = 15pF
    • Fine: (8+1)*75fF = 0.675pF
  • Sensor Capacitance (pF) = Coarse + Fine = 15.675 pF (maximum 48.9pF )

Self-Capacitance

  • Sensor Capacitance (pF) = (Coarse + Fine) * 2= 31.35 pF (maximum 97.8pF )

Back to Top