Guide for Slider Sensor Design When Using Modular QTouch® Library
Last modified by Microchip on 2026/02/26 08:50
This article provides guidelines for designing a self-capacitance slider. A suitable design should be chosen based on the width requirements of the slider. This slider design should be used when using Atmel START-based QTouch® Modular Library.
When using the Microchip Studio-based QTouch library, the slider design guidelines provided in "Section 5" of the "" should be used. For mutual capacitance slider design, refer to "Section 6" of the "".
Note: The Y line numbers indicated in the images represent the order only and NOT the actual PTC Y lines. The PTC Y line can be connected in any order.
Small Width Slider

Medium Width Slider

Large/Wide Width Slider