Visualize Touch Debug Data using Data Visualizer

Last modified by Microchip on 2026/02/26 08:51

Objective

This page provides information on using the Data Visualizer tool to view and debug QTouch® technology data.

Materials

Procedure

Enable Debug

Ensure that the Enable Data Streamer option is selected while generating the QTouch project from Atmel START.

Screenshot of enabling Data Streamer in Atmel START

Detailed information on how to generate a QTouch project in Atmel START can be read from the "Generate User Board Touch Project".

Back to top.


Import Project

After downloading the package from Atmel START, generate the project using Atmel Studio 7 or IAR.

  • Procedure to generate project using Atmel Studio 7
  • Procedure to generate project using IAR

Program the generated .hex file to the device.

Back to top.


Open Data Visualizer

Back to top.


Serial Port Control Panel

The Xplained Pro Kits support Data Gateway Interface (DGI) and virtual COM Port Interface in order to transmit data from kits to Data Visualizer. In QTouch projects, debug data is sent through the serial interface (COM Port).

Expand the Serial Port Control Panel by doing a double-click on the 'Serial Port Control Panel' title bar.

Back to top.


Select COM Port

In the Serial Port Control Panel:

  • Select the 'EDBG Virtual COM Port (COMxx)' (If multiple Xplained Pro kits are connected, disconnect other Xplained Pro kits to identify correct COM Port).
  • Uncheck the 'Open Terminal' check-box and select 'Autodetect Protocol'.
  • Click Connect

The Data Visualizer tool automatically checks for data on 9600, 19200, 38400, 57600, 115200, 230400, 500000, 1000000 and 2000000 baud rates.

Selecting the COM port in the 'Serial Port Control Panel' of Data Visualizer

Back to top.


Configuration Files

Verify whether .ds.db.sc files are present in the ../qtouch/datastreamer/ folder. The Data Visualizer configuration files will be present in the ../qtouch/datastreamer/ folder ONLY if the Atmel START extension version is 1.0.105.0 or above is used in Atmel Studio. If these files are not present, update the Atmel START extension as follows:

  • Open Atmel Studio 7.
  • Select Tools > Extension Manager.
  • In Extension Manager window, click Installed > All.
  • Select 'Atmel START' extension from the list and click Update.

After Updating the extension create the project again using the .atzip package, program, and continue.

Data Visualizer will prompt you to select the folder containing the configuration information if there was no folder selected before. Configuration files are stored as part of the project source files. Browse the ../qtouch/datastreamer/ project folder and select 'Select Folder'. The selected folder will be saved by Data Visualizer. It may be necessary to change this folder location when you want to view data of another/updated project. If you would like to change the path, you can click on Autodetect Protocol.

Back to top.


Dashboard

The dashboard will display basic and advanced information in tabular/graphical form:
Basic Information

Screenshot of Basic Information displayed in Data Visualizer

Advanced Information

Screenshot of Advanced Information displayed in Data Visualizer

Back to top.


Graphical View

The graphical view provides a graphical representation of signal, reference and touch delta.

Screenshot of Data Visualizer Graphical View of data

Back to top.


Legends

Lastly, you can select the desired signals to plot by clicking the legends.

Screenshot of Legends at the bottom of Data Visualizer display window

Back to top.