CAP1xxx Library User's Guide for MCC Turnkey Touch Library from Microchip

Last modified by Microchip on 2026/02/26 08:51

Introduction

The CAP1xxx library module will generate the low-level driver code to access the CAP1xxx register. The example code is also provided, showing you how to use the driver in application code.

The CAP1xxx library module is found under the Turnkey Touch library inside the Device Resources window in MPLAB® Code Configurator (MCC). Select the CAP1xxx library module and the I2C module will be added automatically.

Showing the CAP1xxx Library in the Device Resources tab in MPLAB X


Driver Configuration

There are several configuration options for the CAP1xxx driver code, as shown below.

The CAP1xx driver configuration window

Select Device

Choose the device that the host controller is communicating with.

Device Address

By default, all the CAP1xxx devices use 0x28 as the 7-bit I2C address. Some devices allow assigning different I2C addresses.

Generate Example

You have the option to generate an example code file that shows how to use the CAP1xxx driver in the application code.

I2C

This enables the MCC I2C driver for the device.

ALERT

The CAP1xxx has an ALERT pin to notify the host if an event happened, for example, touch, release, noise, etc.
If the ALERT pin is enabled, you will need to assign a pin on the host to read the ALERT state.

RESET

Some of the CAP1xxx devices feature a RESET pin which is active low.

WAKE

Some of the CAP1xxx devices feature a WAKE pin to wake up the device from Sleep mode. More information can be found on the CAP1xxx datasheet.

Select I2C Master

If the host has multiple I2C peripherals, you can choose the one to talk to the CAP1xxx device.

The I2C Master will need to be configured to support clock stretching in order to communicate with the CAP1xxx device, some of the devices have to do it manually in the I2C module configuration.


Generated Files

The module will generate the CAP1xxx driver and application example code (optional).

  • cap1xxx_app.ccap1xxx_app.h: low-level driver that accesses the register.
  • cap11xx.h/cap12xx.h: full register description of the CAP1xxx device.
  • cap1xxx_example.ccap1xxx_example.h: example of how to use the driver in application code.

Code Example

Here are some examples using the driver code (PIC32MM as the host):

Use the example code directly

The example function provides a quick start to verify if the hardware is functional.

1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
#include "mcc_generated_files/system.h"
#include
"mcc_generated_files/mcc.h"
#include
"mcc_generated_files/cap1xxx_example.h"
int main(void)
{
   // initialize the device
   SYSTEM_Initialize();

   // the CAP1xxx device needs at least 200ms at power up to respond the I2C command
   // this is a user-defined function to delay at least 200ms before excute CAP1xxx initialization.
   my_delay_function();

    CAP1xxx_initializationExample();

   while (1)
    {
        CAP1xxx_handleGeneralStatusExample();
        CAP1xxx_readSensorStatusExample();
    }
   return 1;
}

Use the driver code

Once the design is functional, you can use the driver code to integrate with your application.

1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
#include "mcc_generated_files/system.h"
#include
"mcc_generated_files/mcc.h"

// sensor initial configuration
const uint8_t myCAP1xxxConfig[][2] =   
{   //  Address     Value
   {   0x00,       0x00    },      // Main Control
   {   0x1F,       0x2F    },      // Sensitivity Control
   {   0x20,       0x20    },      // General Configuration
   {   0x21,       0xFF    },      // Sensor Input Enable
   {   0x22,       0xA4    },      // Sensor Input Configuration
   {   0x23,       0x07    },      // Sensor Input Configuration 2
   {   0x24,       0x39    },      // Averaging and Sampling Config
   {   0x26,       0x00    },      // Calibration Activate
   {   0x27,       0xFF    },      // Interrupt Enable
   {   0x28,       0xFF    },      // Repeat Rate Enable
};

int main(void)
{
   // initialize the device
   SYSTEM_Initialize();

   // the CAP1xxx device needs at least 200ms at power up to respond the I2C command
   // this is a user-defined function to delay at least 200ms before excute CAP1xxx initialization
   my_delay_function();

   // initialize the CAP1xxx device
   CAP_init(myCAP1xxxConfig,sizeof(myCAP1xxxConfig)/2);

   // wait until all the sensor is calibrated.
   while(!CAP_isCalibrated());

   while (1)
    {
        CAP_GENERAL_STATUSbits_t CAP_current_status;

       // read out the general status of the CAP1xxx device
       CAP_current_status.value = CAP_getGeneralStatus();

       if(CAP_current_status.TOUCH)
        {
           // Touch Event
           CAP_SENSOR_INPUT_STATUSbits_t CAP_sensor_input_status;
           // Read out sensor status to check which sensor is pressed
           CAP_sensor_input_status.value = CAP_getSensorStatus();

            printf("Sensor Status = %d \r\n",CAP_sensor_input_status.value);

           if (CAP_sensor_input_status.CS1)
            {
               // application process if CS1 is pressed
               LED_SetHigh();
            }
           else
            {
               // application process if CS1 is released
               LED_SetLow();

            }

        }
    }
   return 1;
}
}

Touch Tuning

Microchip recommends using the CAP1xxx GUI for intuitive and efficient tuning.
Application note AN2034 provides guidelines on touch performance tuning.

Screenshot of the CAP1xxx GUI for tuning

Back to Top