Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Helper APIs
Last modified by Microchip on 2026/02/10 14:29
DO_NOT_REMOVE
The Application Programming Interfaces (APIs) defined in this sections are not mandatory to use. These APIs can be used to get or set touch library specific state or data.
Description: Returns the surface's vertical or horizontal position based on input value. The value contact determines whether it is first position or second position.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.