How to Create a Lump Sensor

Last modified by Microchip on 2026/03/27 13:06

Overview

This section provides a step-by-step guide for generating a lump sensor using Touch Configurator in MPLAB® Code Configurator (MCC).

Procedure

Open Touch Configurator

Select MCC and open Touch Configurator in the Resource Management (MCC) tab.

Plugins dropdown

Back to Top


Create Buttons, Slider, and Wheel

Add the required number of buttons, sliders, and wheels.

Create tab

Back to Top


Create Lump Button

Press the Control key and click the sensors (buttons, sliders, and wheels) to be configured as a lump sensor. (A lump can also be created by mouse movement.) Now, click Create Lump Sensor.

Create Lump Sensor button

Information

Note: Multiple lump sensors can be created.

Back to Top


Visualize Lump Sensor

The hexagon graphic represents lump sensors. The lumped individual sensors will be displayed in yellow when the mouse cursor is placed over the lump sensor.

Hexagon Graphic

Back to Top


Generate Lump Sensor Code

Click Generate in the MCC (Resource Management) tab.

Generate button

The following animation shows the process of creating a lump sensor in Touch Configurator.

Creating a lump sensor

Back to Top