USB Type-C® Alternate Mode
Last modified by Microchip on 2023/11/09 08:55
A central feature of USB Type-C® Power Delivery (PD) protocol is the ability to activate Alternate mode.
Alternate mode allows some of the pins on a Type-C connector to be reconfigured to support other protocols.


Using the PD protocol, the Downstream Facing Port (DFP) begins the negotiation with the Upstream Facing Port (UFP) to enter Alternate mode.
- The DFP queries the UFP for a list of supported modes.
- The UFP responds with a report of the available modes the UFP can support.
- The DFP selects a mode, then directs the UFP to reconfigure the pins and enter Alternate mode.
- Both the UFP and DFP enter Alternate mode.
Alternate Mode Example
A user-designed or industry-standard protocol can be run using Alternate mode. A common use of Alternate mode is a video monitor.
- The UFP (Monitor) and the DFP (Portable Workstation) are connected with a Type-C cable
- The DFP enumerates
- Using the Power Delivery Protocol, both the UFP and DFP enter Alternate mode and set the interface to a graphics interface
Active Signals During Enumeration

Active Signals for Alternate Mode Graphics Client

Active Signals for Vendor Specific Device