Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Network Configurations
Last modified by Microchip on 2023/11/09 08:55
Infrastructure Mode
This is the standard network configuration mode utilized for Wi-Fi® networks.
Uses Access Points (AP).
Nodes can only transmit to other nodes through the AP.
AP fully supports all 802.11 network management functions and operations.
Basic Service Set (BSS), AKA cell in the Infrastructure mode contains:
Access points
Wireless hosts
LAN connection (second PHY)
In a typical home access network, the AP function is combined with switch and router functionality in a single device, such as the Linksys E1200.
Ad-Hoc Mode
No Access Points.
Nodes can only transmit to other nodes within the link coverage.
Nodes organize themselves into a network of peer-to-peer connections.
Independent Basic Service Set (IBSS) aka cell in the Ad-Hoc mode contains:
Wireless hosts only
Distributed management
Each station searches for an IBSS before starting its own (best practice – not mandated by 802.11).
Each station takes turns transmitting the beacon for the IBSS.
Each station applies security to communications.
Due to the computational/protocol overhead of current Wi-Fi security frameworks (i.e. WPA/2), most stations only implement WEP (the original 802.11 security framework) in Ad-Hoc mode. The WEP is known to be easily broken.
For this reason, 802.11 Ad-Hoc mode is not supported in some systems (for example, Android). This has led to the development of alternative configurations for implementing point-point Wi-Fi communications, such as Wi-Fi Direct or SoftAP.
Menu
Microchip Support
Query Microchip Forums and get your questions answered by our community:
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.