Introduction to Operational Amplifiers

Op Amp Common Mode Rejection Ratio (CMRR)

Last modified by Microchip on 2026/01/09 08:12

   Input Bias and Offset Current  Power Supply Rejection Ratio   

Common Mode Rejection Ratio (CMRR) is a measure of the capability of an Operational Amplifier (op amp) to reject a signal that is common to both inputs. Ideally, CMRR is infinite. If both inputs fluctuate by the same amount (while remaining constant relative to each other), this change will have no bearing on the output.

Common mode rejection is a feature of differential amplifiers. Op amps are amplifiers with differential input, so common mode rejection applies to operational amplifiers. Common mode signal is when both of the inputs of the amplifier have the same voltage or they have a common voltage across them. Under this condition the output of the amplifier should be zero or the amplifier should reject the signal and not amplify it.

Figure 1 shows an op amp in a comparator configuration where the output should be zero because the inputs are the same.

CMRR

Figure 1

Figure 2 shows the MCP601 common mode rejection specification.

CMRR Specs

Figure 2