PIC32MX Instruction Pipeline
Introduction
The control unit in all Central Processing Units (CPUs) follows the same basic instruction processing sequence:
- Fetch the instruction
- Decode the instruction
- Execute the instruction
On traditional CPUs, these phases are typically executed sequentially as shown in the accompanying image:

Modern, high-performance CPUs (like MIPS®) use a technique called pipelining, whereby these phases of instruction processing are executed in independent overlapping stages, as shown in the accompanying image:

N-stage pipelines, therefore, have n-instructions at different stages of execution moving through the pipeline, similar to an automotive assembly line.
PIC32MX Pipeline
The MIPS® M4K® CPU core implements a five-stage pipeline as shown in the accompanying image:

- I-STAGE: INSTRUCTION FETCH
- Fetch the instruction from cache/instruction SRAM. Increment the PC by four.
- E-STAGE: EXECUTION
- Fetch operands from the register file. Begin Arithmetical Logical Unit (ALU) Operation. Calculate the branch target address. Begin MDU operation.
- M-STAGE: MEMORY FETCH
- ALU Op Completes. Data cache/SRAM access is performed for load/store operations. MDU operations proceed.
- A-STAGE: ALIGN
- Align loaded data with its word boundary. Load data or MDU result to E-STAGE for bypassing.
- W-STAGE: WRITEBACK
- For register-to-register or load instructions, the result is written back to register file.
Data Hazards
The term data hazard refers to the situation where results from prior ALU operations are required before they have been written back to the register file.
In the following example, the result of the first operation (in register t3) is required as input for execution of the second operation:
2
sub t4, t3, t7 /* t4 = t3 - t7 (HAZARD: t3 not written yet!) */
The M4K microprocessor cores implement a bypass mechanism that allows the result of an operation to be sent directly to the instruction that needs it without having to write the result to the register and then read it back.
The following diagram depicts the PIC32MX datapath, showing the A » E and M » E stage bypass connections:

The following pipeline diagram depicts how the result (t3) can be made available after the M-STAGE to the following instruction without stalling the pipeline:

Control Hazards
Control hazards arise in pipelined CPU architectures whereby instructions that follow branch instructions are fetched by the control hardware, and (traditionally) are flushed if the branch is taken, reducing instruction throughput.
M4K CPU cores implement a delay slot in the pipeline and include branch target address calculation hardware in the E-stage of the pipeline.
For branch operations, these result in:
- Having an instruction slot available after all branch instructions to do useful work
- Guaranteeing that the pipeline fetches either the branch taken instruction or fall-through instruction in the cycle immediately following the delay slot
Since the branch cannot take effect until the second stage of the pipeline, we say that it is a delayed branch (i.e., the branch/jump will take place after the instruction following the branch is in the pipeline).
The following pipeline diagram demonstrates how either the branch taken instruction (label L2) or the fall-through instruction (label L1) is executed immediately after the delay slot instruction (sw t0, 0(sp)):

Summary
The PIC32MX pipeline begins the fetch of either the branch path or the fall-through path in the cycle following the delay slot. The MIPS programmer (or compiler!) must organize their code to perform some useful work during this delay slot, or simply insert a nop instruction.