Enable Cache and Manage Cache Coherency
Manage Stale Cache:
If Direct Memory Access (DMA) changes main memory, there is no hardware mechanism to automatically update associated cache. Your software will have to ensure the cache is coherent (is not stale) when the core reads data from it. You can force the cache to reload specific lines (CACHE and PREF instructions), or force the core to read directly from main memory (KSEG1).
The following code example demonstrates how to read a variable defined in cached memory (KSEG0) from uncached memory (KSEG1). This uses the KVA0_TO_KVA1 macro (Kernel Virtual Address Segment 0 to Segment 1 XC32 C compiler macro) to translate a variable's cached address to its uncached address.
int Var1InKseg0 = 5;
// Declare a pointer and use the KVA0_TO_KVA1 macro to assign it the uncached address of Var1InKesg0
int *pVar1InKseg1 = KVA0_TO_KVA1(&Var1InKseg0);
y = *pVar1InKseg1; // Assign y the uncached value of Var1InKseg0
Manage Dirty Cache:
Hardware will automatically update main memory if the core writes to cache. You can configure the hardware with one of the following options:
Write-back with write allocation
(default configuration)
If the core writes to cache, the hardware will allow cache to remain dirty until data is evicted from the cache. The hardware keeps track of the dirty cache lines, and will write-back these lines to main memory when or if the data is evicted from the cache.
When the core reads from cached memory (KSEG0), it will first search cache, reading main memory only if the desired data does not reside in cache. The hardware automatically fills cache on a cache miss. This is called read allocation.
The core also has the ability to allocate cache lines for writes to cached memory even if the data isn't already in cache. This is called write allocation.
This policy is the easiest for the hardware to implement and consumes the least system bus resources and power. It is also the least useful for keeping shared data coherent. Combining this cache policy with using uncached (KSEG1) memory for shared data is the simplest cache management approach, and is recommended for getting your project up and running.

Write-through with write allocation
If the core writes to cache, the hardware will also automatically update main memory. This write-through configuration ensures data in the cache is never dirty.
When the core reads from cached memory (KSEG0), it will first search cache, reading main memory only if the desired data does not reside in cache. The hardware automatically fills cache on a cache miss.
The core also has the ability to allocate cache lines for writes to cached memory even if the data isn't already in cache. This is called write allocation.
This policy ensures shared data is never dirty, but you will still need to ensure shared data is not stale.

Write-through with no write allocation
If the core writes to cache, the hardware will also automatically update main memory. This write-through configuration ensures data in the cache is never dirty.
When the core reads from cached memory (KSEG0), it will first search cache, reading main memory only if the desired data does not reside in cache. The hardware automatically fills cache on a cache miss.
The core does not have the ability to write to cache unless the data to be modified is already in cache. This is called no write allocation.
- If the core writes to cacheable memory, and the data is not in the cache, it will write to main memory only.
- If the core writes to cacheable memory, and the data is in the cache, it will write to cache and also update main memory.
This policy ensures shared data is never dirty, but you will still need to ensure shared data is not stale.

Cache Policy Recommendations
The recommended approach is to start with a writeback write-allocate (default) cache policy and use KSEG1 when accessing any memory used by a DMA peripheral. This is the simplest approach and in most cases it will provide acceptable performance.
Once the project is running and debugged, performance can be improved by changing the access of DMA memory to KSEG0 and employing the CACHE and PREF instructions to manage coherency. In systems employing multiple DMA bus masters, software management of the cache can be used only where necessary and implemented on one DMA peripheral at a time simplifying the debug process.
The following table summarizes some of the pros and cons of each cache policy. The default cache policy for the PIC32MZ family, as is present in the start-up code supplied in the development tools, is write-back with write allocation.
| Policy | Pros | Cons |
|---|---|---|
| Uncached | No cache coherency issues. | Greatly impaired performance since every memory access must account for bus transfer time and memory wait states. |
| Write-back with Write Allocation | Best performance is achieved with this policy. All transactions are done using the cache with memory accesses performed only when needed. | Application must address coherency on both reads and writes to memory. |
| Write-through with no Write Allocation | Cache coherency issues are eliminated for writes as memory is always updated. | Results in the CPU taking a larger percentage of the memory bus bandwidth since every CPU write results in a bus transaction. Even back-to-back writes are written to memory. Cache coherency for CPU reads must still be addressed. |
| Write-through with Write Allocation | Cache coherency issues are eliminated for writes as memory is always updated. Writes to memory and also fills cache so the data written is immediately available for a CPU read. | Results in the CPU taking a larger percentage of the memory bus bandwidth since every CPU write results in a bus transaction. Even back-to-back writes are written to memory. Cache coherency for CPU reads must still be addressed. Writes to memory also fill the cache which can result in needed data being evicted from cache. |
Changing cache policy

The MPLAB® XC32 C compiler provides an easy-to-use cache configuration file: pic32_init_cache.S. If you copy this file into your local project directory it will override the default runtime setup code used to initialize the cache. The default runtime setup code initializes the cache policy to write-back with write allocation.
You can find this file in the following XC32 install directory:
…xc32/vx.xx/pic32-libs/libpic32/stubs
File: pic32_init_cache.
#define _CACHE_WRITEBACK_WRITEALLOCATE 3
#define _CACHE_WRITETHROUGH_WRITEALLOCATE 1
#define _CACHE_WRITETHROUGH_NOWRITEALLOCATE 0
#define _CACHE_DISABLE 2
/* Set __PIC32_CACHE_MODE to the desired coherency attribute */
#define __PIC32_CACHE_MODE _CACHE_WRITEBACK_WRITEALLOCATE //default runtime setup policy
Changing cache policy during code development and debug
Microchip recommends the cache policy be configured by the run time start-up code, and should not be changed on the fly. For code development and debug, you may want to use the example code shown below to see how a given cache policy affects your code's performance. It should be placed at the top of the Main () function.
#define UNCACHED 0x02 // uncached
#define WB_WA 0x03 // write-back, write allocate
#define WT_WA 0x01 // write-through, write allocate
#define WT_NWA 0x00 // write-through, no write allocate
void set_cache_policy(int cc)
{
unsigned int cp0;
cp0 = _mfc0(16, 0); // read the cp0 config register
cp0 &= ~0x03; // clear the K0 field
cp0 |= cc; // update K0 with the new value
_mtc0(16, 0, cp0); // write the cp0 config register
}
int main(void)
{
set_cache_policy(UNCACHED); // set_cache_policy(UNCACHED);
.....
.....
}