PIC32MZ Shadow Register Sets
The PIC32 processor implements one or more copies of the General Purpose Registers (GPR) for use by high-priority interrupts. The extra banks of registers are known as shadow register sets. When a high-priority interrupt occurs, the processor automatically switches to a shadow register set without software intervention. This reduces overhead in the interrupt handler and reduces effective latency.

The shadow register sets are controlled by registers located in the System Coprocessor (CP0) as well as the interrupt controller hardware located outside of the CPU core.
Basic Operation
An interrupt exception request is decoded by the interrupt controller. The vector number, requested priority level and shadow register set numbers are provided to the CPU core as shown:

The shadow register set number is then written to the SRSCtlEICSS bit-field, which is used to select the "current shadow set" for the interrupt.
The microAptivTM/M5150 core then uses this information to perform the following:
- The current GPR Bank ID is copied into the SRSCtlPSS field of the SRSCtl register. This is the Previous Shadow Set (PSS) ID to be recovered later when the interrupt exception request is completed.
- The GPR set ID pulled from SRSCtlEICSS is copied into the SRSCtlCSS field of the SRSCtl register. This now specifies the Current Shadow Set (CSS).
- Execution of the interrupt exception handler proceeds to completion, and an IRET instruction is executed.
- The core then copies the values from the SRSCtlPSS bit field into the SRSCtlCSS bit field and execution resumes from the point at which the interrupt exception was issued.