SAMA7D6 Series Microprocessor Collaterals and Solutions

Last modified by Microchip on 2026/03/27 13:10

SAMA7D6 series microprocessors (MPUs) offer a rich and balanced set of peripherals and user interfaces that deliver high performance, market-leading low power, and advanced security for cost-sensitive industrial and consumer applications. Microchip MPUs are supported by a wide range of software and development tools, including Linux®, bare metal, MPLAB® Harmony, third-party tools, and software.

To reduce the learning curve and help in developing applications on SAMA7D6 series MPUs, a wide range of supporting collateral is available, including training modules, application notes, technical briefs, demos, reference guides, and videos. This document provides references to such technical material.

Microchip University Courses

The following Microchip University courses are available:

Microchip Graphics Suite (MGS)

 The following MGS user guides are available:

MPU Brochure

The following MPU brochure is available:

SAMA7D6 Series Collaterals

NoTitle/LinkHardware Board/KitDescription
1SAMA7D6 SeriesStep-by-step guide explaining:
  • MPLAB Harmony v3 Software Framework
  • How to install MPLAB X IDE
  • How to install MPLAB XC32 Compiler

2

SAMA7D6 SeriesApplication note explaining the boot process of the SAMA7D6 series microprocessors
3MPLAB Discover Code ExamplesSAMA7D6 SeriesMPLAB Discover code examples
4MPLAB Harmony GitHub ExamplesSAMA7D6 SeriesMPLAB Harmony v3 application examples (CSP, graphics, Ethernet, etc.)
5SAMA7D65 Curiosity Board (EV63J76A) (Quick Start Demo)SAMA7D65 Curiosity KitA specific demonstration application that comes with the SAMA7D65 Curiosity Kit
6SAMA7D65-Curiosity – Getting Started with MPLAB® Harmony v3 Development: RTC ApplicationSAMA7D65 Curiosity KitProvides a step-by-step instruction on how to create an MPLAB Harmony-based RTC application and debug it
7Linux SolutionSAMA7D65 Curiosity KitGetting started on Linux OS development
8SAMA7D65-Curiosity – Booting Demo Linux ImageSAMA7D65 Curiosity KitHow to boot a demo Linux image on a microSD™ card
9SAMA7D65 Curiosity Development Board – IntroductionSAMA7D65 Curiosity KitIntroduction to the SAMA7D65 Curiosity Kit
10 SAMA7D65-Curiosity – FeaturesSAMA7D65 Curiosity KitFeatures of the SAMA7D65 Curiosity Kit
11SAMA7D65-Curiosity – Console Serial CommunicationsSAMA7D65 Curiosity KitHow to connect a host computer running a terminal emulation program to the SAMA7D65-Curiosity Kit serial debug port to access the console
12SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from NOR Flash (QSPI) MemorySAMA7D65 Curiosity KitHow to configure and build the second-stage bootloader to boot an MPLAB Harmony application from Quad Serial Peripheral Interface (QSPI) (Octal SPI)
13SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from NAND Flash MemorySAMA7D65 Curiosity KitHow to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an NAND Flash memory
14SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from SD Memory CardSAMA7D65 Curiosity KitHow to configure and build at91bootstrap to load an MPLAB Harmony v3 application from SD™ card memory
15SAMA7D65-Curiosity – Configure and Build at91bootstrap for an MPLAB® Harmony v3 Project with MPLAB X IDESAMA7D65 Curiosity KitHow to configure and build at91bootstrap to debug an MPLAB Harmony v3 project with MPLAB X IDE
16SAMA7D65-Curiosity – Writing MPLAB® Harmony v3 Application and at91bootstrap to NAND Flash Memory Using SAM-BA® ISPSAMA7D65 Curiosity KitHow to write an MPLAB Harmony v3 application and at91bootstrap to an NAND Flash memory using SAM-BA In-System Programmer (ISP)
17SAMA7D65-Curiosity – Writing MPLAB® Harmony v3 Application and at91bootstrap to NOR Flash (QSPI) Memory Using SAM-BA® ISPSAMA7D65 Curiosity KitHow to write an MPLAB Harmony v3 application and at91bootstrap to a QSPI NOR Flash memory using SAM-BA In-System Programmer (ISP)
18SAMA7D65-Curiosity – Copy MPLAB® Harmony v3 Application and at91bootstrap to SD Memory CardSAMA7D65 Curiosity KitHow to write an MPLAB Harmony v3 application and at91bootstrap to an SD card

19

SAMA7D65 Curiosity KitVideo on the process and logic used to compute the Programmable Multi-bit Error Correction Code (PMECC) header required for NAND flash memory interfacing on the SAMA7D65 Curiosity Kit
20SAMA7D65 Curiosity KitVideo on how to use the SAM-BA In-System Programmer (ISP) to provision the SAMA7D65 MPU to boot from NAND.
21SAMA7D65 Curiosity KitTraining on how to display the Microchip Graphics Quick Start project template on the AC69T88A - 5" WVGA LVDS Display using the Microchip Graphics Suite (MGS) on the SAMA7D65 Curiosity Kit
22

SAMA7D65 Curiosity Kit

Training on how to download, configure, and build an MPLAB Harmony v3 Software Framework application to run on the SAMA7D65 Curiosity Kit using MPLAB X IDE
23SAMA7D65 Curiosity KitStep-by-step instruction on how to connect the 5.5" MIPI® 720p LCD Display Module to the SAMA7D65 Curiosity Kit
24SAMA7D65 Curiosity KitStep-by-step instructions on how to connect the NewVision 1280x800 10" LVDS LCD Module to the SAMA7D65 Curiosity Kit
25SAMA7D65 Curiosity KitStep-by-step instructions on how to connect the Waveshare® Capacitive Touch Displays for Raspberry Pi, DSI Interface module to the SAMA7D65 Curiosity Kit
26eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony v3 (AN5218) SAMA7D65 Curiosity KitApplication note describing how to execute an MPLAB Harmony application from QSPI Flash on board
27SAMA7D65 Curiosity KitThis document lists some memory references(QSPI, NAND, SD/e.MMC) that have been tested successfully on SAMA7D65 as boot memories
28Power Monitoring (PAC1934) on SAMA7D65 Curiosity Development Board Using an MPLAB® Harmony ApplicationSAMA7D65 Curiosity KitLearn how to measure power consumption on the SAMA7D65 Curiosity Development Board using the PAC1934 power monitoring IC
29SAM-BA In-System Programmer (ISP)N/ASAM-BA ISP and command line interface

Back to Top