Introduction to PIC64GX Development: Setup, Tools, and First Project on Windows®

Last modified by Microchip on 2026/01/09 08:12

Introduction

PIC64GX Curiosity Board

In this guide, you will learn how to prepare your PIC64GX Curiosity Board, install the necessary software tools, and navigate the development workflow using Visual Studio Code (VS Code®) and Microchip’s Software Development Kit (SDK) extensions. By following the step-by-step instructions, you will gain hands-on experience with the platform and establish a solid foundation for further exploration and application development on PIC64GX devices.

This starting guide is designed to be accessible for beginners while providing enough detail for experienced developers to quickly get up and running with the PIC64GX series.

Useful References

This application is developed for the CURIOSITY-PIC64GX1000-KIT-ES development platform. For platform-related documentation, see the following pages:

Environment Setup

Hardware Setup

Warning

For optimal performance and to avoid compatibility issues, power the board directly from a laptop or the USB port of the PC. The kit has not been tested with USB ports from the docking stations, so using a USB port on a laptop or PC is the most reliable option.

You could also power the board via the OTP-5V power jack. Before connecting the power jack, ensure that J47 jumper is removed.

Software Setup

Back to Top

Development Environment Configuration

This section describes the driver installation process, the VS Code extension installation process, and the workspace initializing process.

PIC64GX Extension Setup on VS Code

Open VS Code.

Back to Top


Now we need to install MPLAB PIC64GX SDK Extension on VS Code.

Open the extensions installer.

Search for "PIC64".

Select MPLAB PIC... extension.

Click on the Install button to install the extension.

install MPLAB PIC64GX SDK Extension

You will see the following on your screen:

MPLAB PIC64GX SDK Extension installed

Back to Top

Install PIC64GX Drivers

Install the PIC64GX drivers.

To open the Windows Device Manager, right-click the Start button (or press Windows key + X), and then click Device Manager.

Confirm the Device Manager warning.

In the Device Manager window, click Other devices to expand the section.

Device Manager window

Back to Top


Find and click on Other Devices, and double-click one of the devices named MCHP-Debug. The MCHP-Debug Properties window opens.

Click Change settings.

Warning

Administrator privileges are required.

Back to Top


Click on Change settings.

MCHP-Debug Properties window

Back to Top


On the Driver tab, click Update Driver. The Update Drivers - MCHP-Debug window opens.

MCHP-Debug Properties window Driver tab

Back to Top


Click Browse my computer for drivers.

Update Drivers - MCHP-Debug

Back to Top


Drivers are in the MPLAB® PIC64GX SDK Extension.

You will find the drivers under the extension folder. Example: 

C:/Users/{USER}/.vscode/exenstions/microchip.pic64gx-sdk-extension-{VERSION}/PIC64GX_drivers

Information

{USER}must be replaced with your user name

{VERSION}must be replaced with the version of the extension that was installed

You can find the version of the extension that was installed in VS Code. Open the extension menu and look for the version.

MPLAB PIC64GX SDK Extension version

Back to Top


Choose your drivers path and click Next.

update drivers MCHP Debug window

Confirm the installation by clicking the Install button.

Windows security window

Information

You will be prompted with a message stating, “Windows has successfully updated your drivers”; you can close this window.

Back to Top


Confirm the driver update.

Update Drivers - USB MCHP-Debug Serial Converter B

Back to Top


Repeat Steps 2 through 7 for each MCHP-Debug device in the Other devices section.

The Other devices section must now contain three USB Serial Port devices. Repeat Steps 2 through 6 for each USB Serial Port device.

Device Manager window - Other devices

Back to Top


To verify that the drivers have been installed, check for this view:

Device Manager window - Ports

Back to Top

Initialize SDK

Open VS Code.

Back to Top


 Press Ctrl + Shift + P to open the command menu, then type "PIC64" and find:

PIC64GX SDK: Initialize SDK

PIC64 search

Back to Top


Specify the Python executable path to extension.

Python executable path to extension

Information

Python is in the AppData folder of your user.

Example: C:\Users\{USER}\AppData\Local\Programs\Python\Python{VERSION}\python.exe

{USER}must be replaced with your user name.

{VERSION}must be replaced with the version of Python that was installed.

A path can be an alias call to a Python executable that is registered in the environment's PATH variable, which can be either an absolute or a relative path.

⚠️ We recommend using the absolute path.

Back to Top


Choose a workspace where you would like to create the SDK.

Information

A workspace is a folder where the workspace repo will be downloaded and initialized.

Choose a workspace

Information

If you don't have workspaces, click on the add (+) button in the top right corner.

Back to Top


Now we should wait for the SDK to be generated.

After a generation, you should see the following output:

Oputput

Warning

If you get a "Python not found" error, you need to change the Python path because it is not specified correctly.

  1. Press Ctrl + ,  to open settings.
  2. Search for the python.
  3. Change pic64gx-sdk-extension.pythonPath parameter to your Python path.

⚠️ We recommend using the absolute path.

Back to Top

Creating and Editing a Basic Project

Creating Project

Now, to continue, we need to create a project. To create the project, click on Extension on the left dock.

Create a project pane
​​​​​

Back to Top


Click on the Create New SDK Project.

Back to Top


Put the name of your project into the Enter project name field.

Back to Top


The next step is to create a project folder in the SDK.

This is a path example for your project:

C:\Developers\{YOUR_PROJECT_NAME}
Warning

Your project should be in the SDK folder.

 Then we should add the project's absolute path into the Enter project directory field.

Back to Top


Then click on Create Project and wait until the project is created. You will see the following output:

Information
 *  Terminal will be reused by tasks, press any key to close it.
Warning

If you see:

Error

AttributeError: module 'os' has no attribute 'unsetenv'

Open the c:\...\{SDK_WORKSPACE}\config.py and change line 63 to os.environ.pop("srctree", None).

Back to Top


To understand if the project was generated successfully, we need to check:

C:\...\{SDK_WORKSPACE}\{YOUR_PROJECT_NAME}\src\application

Press Ctrl + Shift + E and expand your project folder; now you should have the hierarchy shown in the accompanying image:

project folder hierarchy

Back to Top

Bare Metal Application Development

Now we can begin customizing u54_1.c.

Open the u54_1.c file located in:

C:\...\{SDK_WORKSPACE}\{YOUR_PROJECT_NAME}\src\application\hart1\u54_1.c

Start modifying it.

This bare metal program runs on the PIC64GX platform and blinks a General Purpose Input/Output (GPIO) pin using direct hardware access:

  1. It enables the clock for the GPIO1 peripheral.
  2. Initializes GPIO1_LO and configures pin 2 as an output.
  3. In an infinite loop, it toggles the pin high and low every second using a delay loop.
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
#include <stdint.h>
#include
"pic64gx_hal/mss_hal.h"
#include
"mss_gpio/mss_gpio.h"

void delay(uint8_t seconds){
   for (uint64_t i = 0; i < (seconds * 11000000U); ++i) {
        __asm__("sll x0, x0, x0"); // Dummy instruction for delay
   }
}

void u54_1(void)
{
   // Enable clock for GPIO1 peripheral
   (void)mss_config_clk_rst(MSS_PERIPH_GPIO1, (uint8_t) 1, PERIPHERAL_ON);

   // Initialize GPIO1 lower half
   MSS_GPIO_init(GPIO1_LO);

   // Configure pin 2 as output
   MSS_GPIO_config(GPIO1_LO, MSS_GPIO_2, MSS_GPIO_OUTPUT_MODE);

   // Blink loop
   while (1u)
    {
        delay(1);
        MSS_GPIO_set_output(GPIO1_LO, MSS_GPIO_2, 1u); // LED ON
       delay(1);
        MSS_GPIO_set_output(GPIO1_LO, MSS_GPIO_2, 0u); // LED OFF
   }
}
Line 1Includes standard integer types like uint8_t, uint64_t
Line 2-3Includes Microchip’s hardware abstraction layer (HAL) and GPIO driver headers
Line 5-9

Defines a crude delay loop using a dummy RISC-V instruction (sll x0, x0, x0) to waste CPU cycles

Multiplies seconds by a constant to approximate timing

Line 11Entry point for core U54_1 (one of the RISC-V application cores on PIC64GX)
Line 14Enables the clock and resets the GPIO1 peripheral
Line 17Initializes the lower half of GPIO1 (pins 0–15)
Line 20Configures pin 2 on GPIO1_LO as an output
Line 23Infinite loop to keep blinking
Line 25-26Waits 1 second, then sets pin 2 high (LED ON)
Line 27-28Waits another second, then sets pin 2 low (LED OFF)

Back to Top


Now we need to add GPIO drivers to our project.

Open the:
C:\...\{SDK_WORKSPACE}\{YOUR_PROJECT_NAME}\src\application\proj.conf file and append CONFIG_MSS_GPIO=y.

 

Back to Top

Building Project

To build the project, open the Extension menu.

Extension menu

Back to Top


Click on Build SDK Project.

Back to Top


In the Choose a board field, add your board directory.

Information

Your board path is C:\...\{SDK_WORKSPACE}\boards\pic64gx-curiosity-kit.

Back to Top


Pass your project directory to Project directory:

Information

Your project directory will be similar to:
C:\...\{SDK_WORKSPACE}\{YOUR_PROJECT_NAME}

Back to Top


Click on the Build button.

Wait until the project builds. You should see this message:

Terminal will be reused by tasks, press any key to close it.

Terminal

Back to Top

Running Project

Open Run and Debug (Ctrl + Shift + D).

Run and Debug

Back to Top


Open the drop-down menu and select debug-PIC64GX configuration.

debug-PIC64GX

Back to Top


Click on the green start button.

You will see this pop-up. Add your .elf file path (typically, it is build\{YOUR_PROJECT_NAME}.elf) and press Enter. .elf file path

Back to Top


Select the microchip_pic64gx_curiosity option.

microchip_pic64gx_curiosity option

 

Back to Top


When debugging has started, you should see these buttons:
debugging buttons
They allow you to continue,  step into or over that line, and restart and end the debug. From left to right:

  1. Continue execution and stop on the next breakpoint.
  2. Step over the current point.
  3. Step into the current point.
  4. Step out current point.
  5. Restart the debug session and reset the device.
  6. Stop debug session.

Back to Top


Now the debug is running. To add a breakpoint, open your source files (e.g., C:\...\{SDK_WORKSPACE}\{YOUR_PROJECT_NAME}\src\application\hart1\u54_1.c).

add a breakpoint

Click to add a breakpoint. You'll see this once the code is paused at your breakpoint.

code is paused at breakpoint

Back to Top

Debugging Tools

Variables View

In the Debug view, we have a control panel that allows us to view and modify defined variables. At first, we need to define some variables. Copy this code into BlinkExample\src\application\hart1\u54_1.c.

1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
#include <stdint.h>
#include
"pic64gx_hal/mss_hal.h"

void delay(uint8_t seconds){
   for (uint64_t i = 0; i < (seconds * 11000000U); ++i) {
        __asm__("sll x0, x0, x0"); // Dummy instruction for delay
   }
}

void u54_1(void)
{
   uint8_t status = 0;
   long a[10];

   while (1u)
    {
        status++;
    }
}

Now you need to run the code with a breakpoint on the 17th line.

Information

To create a breakpoint, click on the red circle to the left of the line number.

Back to Top


Build and run the application referring to the section Running Project (Debug Mode).

Back to Top


Wait for the debug process to start, and code execution stops at breakpoint.
code execution stops at breakpoint

Back to Top


Now you have stopped execution on line 17, so in the left part of the window, you have a debug panel where you can see the variables that are defined in that scope and global variables.

Back to Top


Search for the Variables menu and you'll see all variables.

Variables menu 

Here you see a status variable and a array values. To change the variable value, double-click on the value of the variable. You'll see this:

LocalsYou can set any value that is allowed by the variable type.

Back to Top


Add a watchpoint.

Watchpoint is a statement, an expression written in the C language. You could create a watchpoint by clicking + in the Watch tab.

Watch tab

Write your expression.

Watch status

Press Enter. Now you will see your expression and its value.

Watch status

Continue execution until the status is equal to 11 and check your watchpoint again.

Watch status

Now our expression is equal to 1 (true).

Back to Top

Summary

This guide introduced the PIC64GX platform, covering hardware and software set up, development environment configuration, and project creation. You also built and debugged a simple GPIO project to gain hands-on experience with basic hardware interaction. These steps provided a solid foundation for further development and exploration with PIC64GX devices.

Back to Top