Demonstrating 8-bit PIC® MCU Direct Memory Access (DMA)

Last modified by Microchip on 2025/08/26 05:29

Objective

This tutorial shows how to configure the PIC18F57Q43 Direct Memory Access (DMA) feature using Microchip’s MPLAB® Code Configurator (MCC). MCC is used to configure Core Independent Peripherals (CIPs) such as the DMA, Universal Asynchronous Receiver Transmitter (UART), Analog-to-Digital Converter (ADC), Timer, and Pulse Width Modulator (PWM).

A video version of this training is available on Microchip Technology's YouTube™ Channel "How to use DMA on 8 bit PIC® MCUs".

Overview

This tutorial makes use of Microchip’s Curiosity Nano Evaluation Boards and Microchip’s Curiosity Nano Adapter Boards to simplify hardware integration.

It showcases the capability of the PIC18F57Q43 DMA to transfer data between CIPs without using any CPU bandwidth.

The PIC18F57Q43 DMA is designed to service data transfers between different memory regions directly, without intervention from the CPU. By eliminating the need for CPU-intensive management of handling interrupts intended for data transfers, the CPU now can spend more time on other tasks.

The DMA modules can be independently programmed to transfer data between different memory locations, move different data sizes and use a wide range of hardware triggers to initiate transfers. The DMA modules can even be programmed to work together to carry out more complex data transfers without CPU overhead.

For more details about the features of the PIC1827/47/57Q43 device family, refer to the PIC18F27/47/57Q43 Datasheet.

MCC is a free graphical programming environment that generates seamless, easy-to-understand C code that is inserted into your project. It enables and configures a rich set of CIPs and functions using an intuitive interface. It is integrated into MPLAB X IDE to provide a powerful and easy-to-use development platform.

This training uses two PIC18F57Q43 Curiosity Nano Evaluation Kits (DM164150) and two Curiosity Nano Adapter Boards (AC164162), which are available from Microchip Purchasing and Client Services.

The application is based on two sets of software. The first performs regular ADC conversions on the potentiometer every 50 ms. When the DMA determines the UART transmit buffer is empty, it loads the ADC result to send the information via the UART. The second set of software moves the data from its UART receiver buffer, when it is full, to the PWM duty cycle register to modify the LED brightness.

DMA Example Project Flowchart​​​​

The potentiometer varies the input voltage to MCU1’s ADC input. The LED connected to MCU2’s digital output changes according to the potentiometer position.

This application utilizes:

  • Timer0 to regularly trigger ADC conversions
  • ADC to read the potentiometer voltage
  • UART to send/receive data between MCUs
  • PWM to control LED brightness
  • DMA to transfer data between CIPs
  • General Purpose I/O (GPIO) to drive the LED

Two Ways to Use This Tutorial

  • Create the project from scratch:
    • Follow the step-by-step instructions to create the required software
  • Use the solution project as an example:
    • Build the solution projects and program them to the PIC18F57Q43 Curiosity Boards to observe the expected behavior

Back to Top

Lab Objectives

  • Create an MPLAB X IDE MCC project for a PIC18F57Q43 microcontroller from scratch
  • Use MCC to configure and generate peripheral libraries (PLIB) code for the following CIPs:
    • Timer0
    • ADC
    • UART
    • PWM
    • DMA
    • GPIO

Reference Materials

Apart from the hardware tools listed above, the following items are required:

  • 2 USB Type-A male to Micro-B male cable for programming and debugging
  • Potentiometer
  • 3 jumper wires to connect the potentiometer
  • 1 jumper wire for UART communication
  • 4 28-pin 100 mil male header strips
  • Breadboard
Information

Note: The Curiosity series evaluation boards include an on-board, embedded debugger. No external tools are necessary to program or debug the PIC18F57Q43. For programming/debugging, the debugger connects to the host PC through the USB Micro-B connector on the PIC18F57Q43 Curiosity Board.

Hardware Connection Setup

DMA Project HW Setup​​​​

Back to Top

Connection Diagram

The application has the potentiometer connected to the ADC, LED connected to GPIO, and the host UART connected to the client UART.

Hardware Setup for DMA Lab​​​​

Information

Note:
This project has been verified to work with the following versions of software tools:

Because we regularly update our tools, occasionally you may discover an issue while using the newer versions. If you suspect that to be the case, we recommend that you double-check and use the same versions that the project was tested with.

Back to Top

Lab Solutions

This ZIP file contains the completed solution projects for this lab. The contents of this ZIP file contains two files and they can be placed in a folder of your choice. Both files are stored in a single GitHub repository. You will need to create a free account to download the files.

Information

Note: Because MCC generates source and header files and libraries under the project folder, the contents of this ZIP file can be placed in any folder of your choice.

GitHub Download​​​​


PIC18F57Q43 Curiosity Nano Evaluation Board Connections

Connect PIC18F57Q43 Curiosity Nano Board and Curiosity Nano Adapter Board using 100 mil header strip.

Note: Soldering is not required. The adapter and evaluation boards have offset vias to provide press-fit to secure headers without soldering.

Connect Potentiometer using three jumper wires to connect the potentiometer to Vdd, Vss and RA0 of MCU1 Curiosity Nano Adapter Board.

Attach a Jumper Wire from MCU1 UART TX to MCU2 UART RX.

Here’s how the setup should look after all connections have been made:

DMA Project Setup​​​​

Back to Top


Create and Set Up an MPLAB® X IDE Project for MCU1

Connect the USB Micro-B cable from the PIC18F57Q43 Curiosity Nano Board to the computer. MPLAB® X Integrated Development Environment (IDE) will use this connection to program and debug the microcontroller (MCU).

Create an MPLAB X IDE project for the PIC18F57Q43 using the MPLAB XC8 compiler.

Note: Note: We’ll refer to your chosen project location as <your MPLAB X IDE project folder>.

If needed, install MPLAB Code Configurator (MCC). We will use it to graphically create peripheral drivers for this tutorial (if you didn't download the whole project).

Note: You can refer to the "Install MPLAB® Code Configurator (MCC)" page if you would like detailed steps on how to do this.

Back to Top


Configure MCU1 Resources with MCC

Note: If you downloaded the completed project files, you can skip this step.

Launch MCC - Open MPLAB® Code Configurator (MCC) by clicking the MCC logo in the MPLAB X Integrated Development Environment (IDE) toolbar.

MCC Logo​​​​

Note: MCC may take a while to load the first time it is launched.

Configure System Module - Click on System Module in the Project Resources window.

System Module Setup​​​​

  • For System Module, we will use the HFINTOSC Oscillator for the clock source.

System Clock Selection​​​​

Timer0 will be configured to create a periodic interrupt to trigger the Analog-to-Digital Converter (ADC) conversions.

Configure TImer 0 - Add Timer0 by opening the Timer folder under Device Resources window and clicking the + icon for TMR0.

Timer 0​​​​

  • Select the TMR0 CIP in the Project Resources window to configure its settings:

Timer 0 Project Resources​​​​

  • In the TMR0 configuration window, select FOSC/4 for the Clock Source and 1:64 for the Clock prescaler. This will configure Timer0 for a 50 ms rollover.

PIC DMA Clock Settings​​​​

The ADC is used to read the potentiometer voltage.

Configure ADC - Add ADC by opening the ADCC folder in the Device Resources window and clicking the + icon for ADCC.

ADCC Settings​​​​

  • Now select the ADCC CIP in the Project Resources window.

ADCC in Project Resources​​​​

  • Update the ADCC configuration window to match the following:

ADCC Configuration Settings​​​​

The UART for MCU1 is used to transmit the ADC results.

Configure UART - Add UART3 by opening the UART folder in the Device Resources window and clicking the + icon for UART3.

UART Selection​​​​

  • Select UART3 in the Project Resources window.

UART Configuration Settings​​​​

  • Update the UART3 configuration window to match the following:

UART Configuration Settings​​​​

General Purpose Input/Output (GPIO) is configured to read the analog potentiometer input and output the UART data.

Configure GPIO - Select Pin Manager: Grid View in the bottom right window. Click each pin with a green lock as either an input or output as shown in the accompanying figure:

GPIO Selection​​​​

The DMA for MCU1 is used to transfer the ADC result to the UART transmit buffer.

Configure DMA - Select DMA Manager from the Project Resources window

Project Resources Update​​​​

Update the DMA configuration window as follows:

  • Check the DMA Channel 1 box
  • Set Source Module to ADCC
  • Set Source Region to SFR
  • Set Source SFR to ADRESL
  • Set Source Mode to Incremented
  • Set Source Message Size to 2

Note: Since the ADC result is 12 bits, the value is spread across two 8-bit registers. Both registers are automatically read by the DMA by setting Source Mode to Incremented and Source Message Size to 2.

DMA Manager​​​​

Continue to update the DMA configuration window as follows:

  • Set the Destination Module to UART3
  • Set the Destination Region to SFR
  • Set the Destination SFR to U3TXB
  • Set the Destination Mode to Unchanged
  • Set the Destination Message Size to 1
  • Set the Start Trigger to U3TX

Note: Destination Message Size is 1 because the UART transmit buffer is one byte wide. Both ADC result buffer values will be transmitted by the DMA.

Setup DMA in MCC​​​​

Note: If the DMA Start Trigger was set to occur after every ADC conversion, the DMA might write the UART transmit buffer before all the bits are shifted out, corrupting the transfer. Triggering the DMA after the UART transmit buffer is empty avoids this issue.

Generate MCC Code - Press the Generate button.

Generate Button​​​​

  • Verify the MCC code generation is successful.

Results​​​​

Back to Top


Build Application for MCU1

Build Application - Right-click on the project and select Build.

Build Selection​​​​

  • The project will successfully build.

Build Results​​​​

Program MCU1 - Click the Make and Program Device icon to program the MCU.

Build Icon​​​​

  • On the PIC18F57Q43 Curiosity Nano tab, you will be able to see a “Programming complete” message.

Programming Successful Results​​​​

Back to Top


Create and Set Up MPLAB® X IDE Project for MCU2

Disconnect the MCU1 Demonstration Board and connect the MPU2 USB Micro-B cable from the PIC18F57Q43 Curiosity Nano Board to the computer. MPLAB® X Integrated Development Environment (IDE) will use this connection to program and debug the MCU.

Create an MPLAB X IDE project for the PIC18F57Q43 using the MPLAB XC8 compiler.

Note: We’ll refer to your chosen project location as <your MPLAB X IDE project folder>.

Back to Top


Configure MCU2 Resources with MCC

Launch MCC - Open MPLAB® Code Configurator (MCC) by clicking the MCC logo in the MPLAB X Integrated Development Environment (IDE) toolbar.

MCC Logo​​​​

Configure System Module - Now you can start configuring the settings for MCU2.

Click on System Module in the Project Resources window.

System Module​​​​

As before, we will use the HFINTOSC Oscillator for the clock source.

System Module Clock​​​​

Configure PWM - Now we will add the Core Independent Peripherals (CIPs) needed to the project and configure them. The PWM is used to control the LED brightness with its duty cycle value.

Add PWM by opening the PWM folder under Device Resources window and clicking the + icon for PWM1_16BIT.

MCC DMA PWM Selection​​​​

Select the PWM1_16BIT CIP in the Project Resources window to configure its settings:

DMA PWM 2​​​​

Make necessary changes to the PWM configuration window to match the following settings:

  • Enable PWM: Check
  • Clock Selection: FOSC
  • Clock Prescaler: 0
  • Mode: Left aligned mode
  • Requested Frequency: 1 kHz
  • Output1 Duty Cycle (%): 50
  • Output2 Duty Cycle (%): 50

PWM Setup​​​​

Configure UART - The UART is used to receive the ADC results.

Open the UART folder in the Device Resources window and click on the + icon for UART3.

UART 3 Selection​​​​

Open the UART3 setting by clicking UART3 in the Project Resources window.

Select UART3 in MCC​​​​

Configure UART3 for the following settings:

  • Mode: Asynchronous 8-bit mode
  • Enable UART: Check
  • Enable Transmit: Check
  • Enable Receive: Check
  • Baud Rate: 9600
  • Transmit Polarity: not inverted
  • Receive Polarity: not inverted

UART 3 Setup​​​​

Configure GPIO - GPIO will be configured to output the PWM waveform and to receive UART data.

Select Pin Manager: Grid View in the bottom right window. Click each pin with a green lock as either an input or output as shown in the accompanying figure:

GPIO Selection​​​​

Configure DMA - The DMA is used to transfer the UART receive buffer contents to the PWM duty cycle register

Select DMA Manager from the Project Resources window.

Project Resources​​​​

Update the DMA configuration window as follows:

  • DMA Channel 1 Box: Check
  • Source Module: UART3
  • Source Region: SFR
  • Source SFR: U3RXB
  • Source Mode: unchanged
  • Source Message Size: 1

DMA Setup​​​​

Continue to update the DMA configuration window as follows:

  • Destination Module: PWM1_16BIT
  • Destination Region: SFR
  • Destination SFR: PWM1S1P1L
  • Destination Mode: incremented
  • Destination Message Size: 2
  • Start Trigger: U3RX

Configure DMA in MCC​​​​

Update PWM Settings - The PWM needs to be assigned to DMA Channel 1.

Select the PWM1_16BIT CIP from the Project Resources window again.

Select PWM1 in MCC Project Resources​​​​

Open the UART3 setting by clicking UART3 in the Project Resources window.

Select LDS for DMA1​​​​

Generate MCC Code - Press the Generate button.

MCC Generator Button​​​​

Verify the MCC code generation is successful.

MCC code generation success​​​​

Back to Top


Build Application for MCU2

Right-click on the project and select Build.

Select Build for DMA Project

The project will successfully build.

Build Results from DMA Project

Program MCU2 - Click the Make and Program Device icon to program the MCU.

Program Icon

On the PIC18F57Q43 Curiosity Nano tab, you will be able to see a "Programming complete" message.

Program complete message

Back to Top


Verify Correct Operation

With the USB cables still connected supplying power, both MCUs will run. When the potentiometer is turned, the LED on the MCU2 demonstration board will adjust its brightness accordingly.

Final Project Testing

Results

The application reads the potentiometer voltage and adjusts the LED brightness in relation to its position.

Analysis

You have successfully demonstrated DMA functionality using the MPLAB® Code Configurator (MCC). Your project used fundamental DMA elements to move data between peripherals that can benefit almost any application. This demonstration continuously reads the potentiometer voltage, moves data to the UART peripheral for transmission, moves data from another UART after reception, and updates the PWM duty cycle without using a single line of code in the execution loop.

You used MCC to configure the system clock, Timer0 to create a continuous 50 ms trigger, ADC to read the potentiometer voltage, UART to send and transmit data, GPIO for analog and digital modes and input and output operations, PWM to control LED brightness and DMA to move data between peripherals.

Conclusion

This tutorial provided you with training for configuring the PIC18F57Q43 DMA using MPLAB X IDE and MCC. As a next step, you can create your own application to suit your needs. Ultimately, if you use another MCU with a DMA, you can explore a similar solution. Note that the configuration would change since the MCU resources will be different.

Back to Top