Lab 2. Using Peripheral Pin Select (PPS)

Last modified by Microchip on 2026/04/09 14:36

Purpose

This lab uses the MPLAB® X Integrated Development Environment (IDE) tools through their integration with Microsoft® VS Code®. In this lab exercise, you will create and build a new standalone dsPIC33A MPLAB X IDE project through its integration with Microsoft VS Code that demonstrates the Peripheral Pin Select (PPS) functionality of the dsPIC33A IO port. PPS lets you map digital peripheral functions to almost any remappable pin. This makes it easy to assign functions like Universal Asynchronous Receiver/Transmitter (UART) or interrupts to the pins that best fit your design.

To learn more about the dsPIC33A IO port, please visit the dsPIC33A I/O Ports Peripheral page, or refer to the dsPIC33AK512MPS512 Family Data Sheet.

Overview

After creating a new MPLAB X IDE project in VS Code, you will modify main.c with a code example that assigns the UART1 TX function to pin RH0/RP113, and the UART1 RX function to pin RD10/RP59. The code example also enables the use of the printf() function using UART1. The main loop simply echoes characters typed in the serial terminal application. 

Here is a simplified connection diagram for this lab exercise:

connection diagram

This lab exercise is divided into the following sections:

Procedure

Part A. Create a New dsPIC33A Project in VS Code®

In this exercise, you will create a new project and verify that it builds successfully.

Follow the procedures covered in Lab 0 and Lab 1 to create a new MPLAB X IDE project called lab2 in the C:\projects\dspic33a folder.

Ensure you are running the VS Code profile created in Lab 0 (MCHP Dev).

Create a basic empty project having a default main.c file.

Create Program Project and Debug Project launch configurations in launch.json.

Perform a build of this project (Ctrl + Shift + B), and verify a successful build.

 

Part B. Update main.c With a Code Example

The following code example demonstrates simple PPS initialization and usage on a dsPIC33A device. The code assigns the UART1 TX function to pin RH0/RP113, and the UART1 RX function to pin RD10/RP59. The code example also enables the use of the printf() function using UART1. The main loop simply echoes characters typed in the serial terminal application. 

Replace the default application with the provided example code.

Open main.c and replace the default application code with the contents below (copy/paste).

Note: In lines 76, 79 that PPS registers are initialized to connect pin RH0/RP113 to U1TX and connect U1RX to pin RD10/RP59.

  

1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
/*
 * File:        main.c
 * Project:     lab2
 *
 * Description:
 *
 * Configures UART1 and PPS to map RH0/RP113 and RD10/RP59 to U1TX/U1RX functions
 * Enables printf() use with UART1 (9600, 8N1)
 *
 * Main loop echoes characters entered from a serial terminal
 *
 */


#include <xc.h>
#include
<stdio.h>

#define FCPU        8000000U
#define FPB_FAST    FCPU
#define FPB_STD     FCPU/2
#define FPB_SLO     FCPU/4
#define UART_BAUD   9600    
// Options: 9600, 19200, 38400

#pragma config FWDT_WDTEN = SW

void clocksInit(void);
void pinsInit(void);
void uartInit(void);
void uartWrite(unsigned char txData);
unsigned char uartRead(void);

int main(void)
{
    INTCON1bits.GIE = 0;        // prevents interrupt flooding since reset state is a '1'
   clocksInit();               // initialize all clocks
   pinsInit();                 // initialize all pins
   uartInit();                 // initialize uart peripheral for printf()
   INTCON1bits.GIE = 1;        // enable global interrupts
    
    printf("\r\ndsPIC33A Hands On Labs - Lab 2\r\n\r\n");
    printf("Enter some text: ");
   
   while(1)
    {
        uartWrite(uartRead());
    }
   
}

void clocksInit(void)
{
   /*** System Clocks Initialization ***/

   // The FRC provides the source clock
   // Instruction Clock, Fcpu = 8 MHz
   // Peripheral Bus Clocks: Fpb_fast = 8 MHz, Fpb_std = 4 MHz, Fpb_slow = 2 MHz

   // Clock settings left at defaults listed above

}

void pinsInit(void)
{
   /*** Digital I/O Initialization ***/
   
   // Initialize RGB Red LED pin
   LATDbits.LATD9 = 0;
    TRISDbits.TRISD9 = 0;

   // Initialize Switch S2 input
   ANSELFbits.ANSELF0 = 0;         // disable analog function
   TRISFbits.TRISF0 = 1;           // make pin digital input

   /*** PPS Initialization ***/
   
   // UART1 TX Assigned to RH0/RP113 (P102_UART_PKOB_TX)
   RPOR28bits.RP113R = 19;
   
   // UART1 RX Assigned to RD10/RP59 (P100_UART_PKOB_RX)
   RPINR13bits.U1RXR = 59;
   
}

void uartInit(void)
{
   unsigned long brg;
    brg = (FCPU/UART_BAUD/4-1)/2;
    U1BRG = (unsigned short)brg;    
    U1CON = 0;
    U1STAT = 0;
    U1CONbits.BRGS = 1;   
    U1CONbits.TXEN = 1;
    U1CONbits.RXEN = 1;
    U1CONbits.ON = 1;
}

void uartWrite(unsigned char txData){
   while(U1STATbits.TXBE == 0);
    U1TXB = (unsigned long)txData;
}

unsigned char uartRead(){
while(U1STATbits.RXBE != 0);
   return U1RXB;
}

// support for printf()

int __attribute__((__section__(".libc.write"))) write(int handle, void *buffer, unsigned int len){
   unsigned char *pData = (unsigned char*)buffer;
   unsigned short count;
   for(count=0; count<len; count++)
    {
        uartWrite(*pData++);
    }
   
   return count;
}

int __attribute__((__section__(".libc.read"))) read(int handle, void *buffer, unsigned int len){
   unsigned char *pData = (unsigned char*)buffer;
   unsigned short count;

   for(count=0; count<len; count++)
    {        
       *pData++ = uartRead();
    }
   
   return count;
}

 

Press Ctrl + Shift + B to build the project. Fix any syntax errors, ensuring that the project builds successfully:

Build project

 

Part C. Run the Application

Next, we'll program the project into the board and test it using the Microsoft Serial Monitor extension, which you installed in Lab 0.

Program the application into the target.

Launch the program configuration by navigating to Run and Debug and selecting Program Project:

selecting Program Project

Verify that the program operation was successful:

Debug Console tab

 

Back to Top


Test the application using the Serial Monitor.

Click on the Serial Monitor tab in the output window:

Serial Monitor tab

 

Set the COM port to the one enumerated by the on-board PICKit 4 Virtual COM Port.

Information

Note: The dsPIC33A Curiosity Board enumerates 2 Virtual COM ports on your PC. Some experimentation may be required to locate the one from the PICKit™ 4 PKOB Device.

Set Baud rate to 9600. Toggle Terminal Mode. Press Start Monitoring:

Start Monitoring

 

Press the MCLR button on the development board to reset the application. You should see the following welcome message:

welcome message

 

Begin typing at the keyboard. The characters should be echoed back to the Serial Monitor window as shown:

Serial Monitor window

 

Back to Top

Results

Re: Using Peripheral Pin Select (PPS) on dsPIC33A Devices

Digital-only peripherals, such as UART, Serial Peripheral Interface (SPI), Timer Clock Input, Input Capture, Output Compare (OC), etc., are not connected to any GPIO pins by default. Several PPS registers need to be correctly initialized to map pins to peripheral functions.

Input Mapping Registers (RPINRx)

PPS inputs are mapped based on the basis of the peripheral. Each peripheral input function is associated with an RPINRx register, containing an 8-bit field that maps a re-programmable IO pin (RPx) to the input function.

From the dsPIC33AK512MPS512 data sheet, the UART1 RX input function mapping is controlled by the U1RXR bitfield in the RPINR13 register. To map reprogrammable pin RD10/RP59 to this input function, either of the following statements may be executed:

  • RPINR13bits.U1RXR = 59;
  • _U1RXR = 59;
Output Mapping Registers (RPORx)

PPS outputs are mapped on the basis of the pin. Each reprogrammable pin (RPx) is associated with an RPORx control register, containing a 6-bit field that maps a specific peripheral output to that pin.

From the dsPIC33AK512MPS512 data sheet, the UART1 TX output function ID number is 19, and the reprogrammable pin RP113 output mapping is controlled by RPOR28.RP113R. Therefore, to map UART1 TX output function to pin RH0/RP113, either of the following statements may be executed:

  • RPOR28bits.RP113R = 19;
  • _RP113R = 19;

Back to Top

Next Project

  • Start Lab 3 to learn how to set up Timer1 interrupts on dsPIC33A to create a simple Tick interface that helps create non-blocking delays.