Smartphone Basic Demo (Transparent UART)
Objective
This tutorial takes you through the steps needed to establish a transparent UART connection using the Bluetooth Smart Data (SmartData) app.
Reference Materials
- RN4870 PICtail™ Board
- Bluetooth SmartData (iOS app)
- Terminal Emulator
- Windows®/Mac®/Linux®: CoolTerm from Roger Meier's Freeware
Procedure
Jumpers
Make sure the following connections on the RN4870 PICtail are enabled.
J3: USB-UART Interface Connection
This jumper bank connects the RX, TX, RTS, and CTS signals from the module to the USB. Put the jumpers on the bottom two (TX and RX). The top two can be added based on your flow control preferences.

JP8: P0_2 LED Display
Connect this one if you want to see the LED indication from the module, it is connected by default.

J1: Power Source Connector
This lab uses CoolTerm, so make sure to connect the middle jumper labeled USB.

Connect RN4870 PICtail Board to PC
Connect the RN4870 PICtail to the PC via supplied USB cable.

Verify COM Port
Open the Device Manager window by going to Start Menu > Control Panel > Hardware and Sound > Device Manager. Once open, check which COM port has been assigned to the RN4870 PICtail board.

Start a CoolTerm Connection
Launch CoolTerm and establish a connection with the following settings (your COM port might be different).

Enable Transparent Service
Enter the following commands into your CoolTerm window:
$ // Enter Command Mode + // Turn Local Echo on SS,C0 // Support Device Info and UART Transparent services R,1 // Reboot device for configuration to take effect
SmartData App
On your Apple® device, go to the App Store®, and install the SmartData app by Microchip Technology Inc.

Launch the SmartData App
After you open the SmartData app on your smartphone, it will immediately scan for Bluetooth devices nearby. The default name for the RN4870 module, RN_BLE, should show up. Tap on it to connect to your RN4870 module.

On the CoolTerm window, you will see the status message %CONNECT,1,<MAC>% returned by the RN4870 UART, indicating a connection has been established. The <MAC> address is the address of the remote device that initiated the connection. Next to it, you will also see the %STREAM_OPEN% message, indicating that the UART Transparent data pipe has been established. Once connected to another device, the RN4870/71 automatically enters Data mode if the UART Transparent feature is enabled.

Another message you might see is the %CONN_PARAM,<Interval>,<Latency>,<Timeout>% status message. This shows the connection interval, slave latency, and supervision timeout parameters for the existing connection.
Send Data
You can now start exchanging data. Once you have typed your message, (Hello World!), on the app, press the Send button to transfer data from SmartData app to the RN4870 module. The message is received and printed on the serial terminal of the RN4870 UART (CoolTerm window).

Type another message, (How are you?), into the serial terminal of the RN4870 and you will see it is received and printed on the Receive view of the SmartData app.
Conclusions
In this lab, you:
- Added the Transparent UART Service to your RN4870 module.
- Sent and received data using Microchip's Transparent UART Service.