RN4020 Device Firmware Update Over-The-Air (OTA)
Objective
This page shows you how to upgrade RN4020 firmware to the latest version via the Over-The-Air (OTA) process using Microchip's "Bluetooth Smart Data" app running on an iOS device. The following conditions must be met when the RN4020 performs a Device Firmware Update (DFU) through OTA:
- Only a one-to-one connection is allowed between the device whose firmware is to be updated and the device that provides the update image
- Avoid RF interference whenever possible
- The module that is streaming the image to the remote device must have UART hardware flow control enabled
Reference Materials
- RN-4020-PICtail RN4020 Bluetooth Low Energy PICtail™ and PICtail Plus
- Terminal Emulator:
- Smart Data App (iOS)
Connection Diagram
A host is required to enter commands that place the RN4020 into OTA DFU mode with Microchip Low-energy Data Profile (MLDP) enabled and advertising enabled. The following connections are required at a minimum:

Procedure
Detailed Steps – RN4020 Device Under Test (DUT) – RN-4020-PICtail Daughter Board
Ensure that the minimum signal connections as shown in the diagram above are connected. If you are using the RN4020 PICtail, they are already connected.
Connect the RN-4020-PICtail to the PC via the supplied USB cable (make sure jumper JP1 is in the OFF position).

Determine which COM port number has been assigned.

Start Tera Term (115200, 8, n, 1, none)

and enter the following:
+ // echo on
SF,2 // perform complete factory reset
SR,10008000 // support MLDP, enable OTA
// (peripheral mode is enabled by default)
R,1 // reboot to apply settings
// wait for "CMD"
A // start advertising
Detailed Steps – iOS Device
On your iOS device, go to the Apple® App Store®, search for "Bluetooth Smart Data" and install the app.

Launch the app and enable your Bluetooth interface (if required). The app will then begin scanning for devices. Once finished, select your device from the list shown.

The accompanying screen capture shows BTLE v1.10.09. Depending on which version your RN4020 contains will be shown on the screen.

On the Status activity window, select the DFU-OTA option at the bottom of the screen.

Select Download RN4020 DFU File to pull the image from iTunes®.

Once the file is downloaded to your device, click the Browse button to browse to the DFU file.

Select the DFU file.

On the Status activity window, move the Module to DFU mode slider switch to the ON position.

Select Upgrade.

You will see a download status bar displaying the status of the download.

Upon successful completion, you will see the following dialog on success. Click OK.

The module will reboot and output CMD:
The accompanying screen capture shows BTLE v1.10.09. Depending on which version your RN4020 contains will be shown on the screen.

Results
Type "V" in Tera Term to verify the new firmware version: