BM70 Stopwatch Demo (Private Service)
Objective
This lab exercise will have you configure/deploy a custom (private) Generic Attribute Profile (GATT) service (Stopwatch Service) on a BM70, then interface it with a PIC24 MCU (running demo code) and test it using a dedicated Android® stopwatch app.
You will:
- Configure a custom GATT Stopwatch Service attribute table on a BM70 using the User Interface (UI) Configuration Tool.
- Create a BM70 Configuration EEPROM table for inclusion into the PIC24 project.
- Prepare the BM70 PICtail™ board for use on the Explorer 16 board.
- Program the PIC24 MCU Stopwatch Demo Project.
- Interact with the Service using the Stopwatch app.
Reference Materials
- BM70 PICtail™ Board
- Explorer 16 Development Board
- MPLAB ICD3
- Android Smartphone (Lab tested with BLU Advance 5.0).
- OS version 4.4 or higher
- BT 4.0 or higher hardware
- MPLAB X IDE
- MPLAB XC16 Compiler
- MCP2200 USB Driver
- UI Configuration Tool
- Manual Pattern Test Tool
Before You Begin
- Install MPLAB X IDE and XC16 Compiler.
- Install the MCP2200 USB driver.
- Download the BM7x EEPROM Table Utility using the link above.
- Download/extract the UI Configuration Tool as well as the Manual Pattern Test Tool to your PC using the links above.
- Download/extract the Explorer 16 BM7x PICtail Stopwatch Project to your C:\ folder.
Connection Diagram

Generic Access Profile (GAP) Peripheral Device (GATT Server)
The Explorer 16 Board with the BM70 advertises a Stopwatch Service, which provides stopwatch data to a smartphone, as well as providing a control point to remotely trigger the stopwatch to start counting.
GAP Central Device (GATT Client)
An Android smartphone running the Stopwatch demo app, scans, filters, and connects to a specific stopwatch. It also can trigger the stopwatch to begin counting.
MCU Interface

Demo Flowcharts

Procedure
GATT Server Configuration
In this sequence, you will configure the BM70 static parameters for this application, including creating the GATT Table for the Stopwatch Service.
Verify Module Firmware Version
This demo requires BM70 module firmware version 1.06. Verify the firmware version, and if necessary, program v1.06 firmware into the module.
Load UI Configuration
Launch the UI Configuration Tool (found in the "Software Tools" section above) and load in the Default BM70 UI Config File (IS1870SF_102_BLEDK3_UI v100.132(BM70) default.txt), which you obtained from the "Reference Materials" section of this page.

Edit UI Configuration
Select Edit and ensure the BLEDK3 radio button is checked with the BM70 device under Main Feature. Then press OK.

Change the Device Name, Universal Asynchronous Receiver Transmitter (UART) Setting, Operation Mode
In the System Setup tab, under the Device Information pane, set the Name Fragment to a unique value. This identifier will become the GAP Service Device Name characteristic.
Recommend a maximum length of eight characters.
If your name is longer than eight characters, you will see an error message when filling in the balance of your ADV_IND payload. (Remember, we only have 31 bytes of payload!)
In the System Setup tab, under the Uart Setting pane, enable the UART RX_IND pin function.
In the System Setup tab, under the Operation Mode Setting pane, set the Operation Pattern to Manual Pattern as shown:

Click Next to proceed to the System Setup2 tab.
GPIO Configuration
In the System Setup2 tab, under the GPIO Configuration pane, select NO_USE for all pin functions EXCEPT P33, which should be assigned to the UART_RX_IND function as shown:

Click Next to proceed to the LE Mode Setup tab.
Advertising Interval (ADV_IND Packets)
In the LE Mode Setup tab, under the LE Advertising Setting pane, change the default LE Fast Advertising Interval to 100 mS (0x00A0) as shown:

LE Reduced Power Advertising Interval parameter (not shown above) is only used in Auto Pattern (Transparent UART) mode operation. You do not need to modify this.
BLE ADV_IND type advertising packet is a generic advertisement, meaning that it is undirected and is connectable. This would be the initial default advertising type for a new product before it has paired with a smartphone.
Advertising Payload (ADV_IND Packets)
In the LE Mode Setup tab, under the Advertising Data Setting pane, add the Stopwatch Service Universally Unique Identifier (UUID) (0x8E9598AC066211E6B5123E1D05DEFE78) to the ADV_IND payload as shown:

The Stopwatch app uses the Service UUID from the ADV_IND packets to filter out other devices, only displaying Stopwatch Devices on a scan.
Click Next to proceed to the GATT Service Table tab.
GATT Stopwatch Service
You will now create the Stopwatch Service attribute table having the following characteristics and features:
Stopwatch Service
UUID: 0x8E9598AC066211E6B5123E1D05DEFE78
Stopwatch Control Point” Characteristic
UUID: 0x8E959DE8066211E6B5123E1D05DEFE78
Value:0x00 (1 byte)
Value Permissions: Write/Write without response
Stopwatch Status” Characteristic
UUID: 0x8E959FE6066211E6B5123E1D05DEFE78
Value:0x0000000000 (5 bytes)
Value Permissions: Read/Notify
Requires Client Characteristic Configuration Descriptor (CCCD) (UUID: 0x2902) with value 0x0000
Notes:
- These UUIDs are version 1 types and were generated using UUID generator.
- Attribute handle values will be automatically assigned by the UI Configuration Tool, starting at 0x8000.
- The characteristics need to be added to the service table in the order shown below, so the handle values match those embedded in the PIC24 demo code.
Create Custom GATT Service Table
Scroll down to the Add-on Service pane, and from the Service List, drag/drop Others into the Add-on Service Table view as shown:

You should see a dialog box prompting you to define a new private service. Type or copy and paste the Stopwatch Service UUID value (0x8E9598AC066211E6B5123E1D05DEFE78) into the UUID field as shown:

Click Next to enter the first characteristic.
Add Stopwatch Control Point Characteristic
Enter the Hex UUID value (0x8E959DE8066211E6B5123E1D05DEFE78), Permissions (Properties), and initial Characteristic Value for the Stopwatch Control Point characteristic (defined above), as shown:

Click OK.
Add Stopwatch Status Characteristic
In the Add-On Service Table window, add the next characteristic by right-clicking on the Service UUID and selecting Add Characteristic as shown:

Enter the Hex UUID value (0x8E959FE6066211E6B5123E1D05DEFE78), Permissions (Properties), and Characteristic Value (0x0000000000) for the Stopwatch Status characteristic (defined above), as shown:

Click OK.
Add CCCD Descriptor Attribute to Stopwatch Status Characteristic
In the Add-On Service Table pane, expand all the + tabs to see the completed GATT service table. Right-click on the characteristic handle 0x8003. We need to add a descriptor attribute (CCCD, type 0x2902) to this characteristic:

Define a CCCD by entering its Hex UUID value (0x2902) and initial value of 0x0000 as shown:

Click OK.
Review GATT Service Table
In the Add-On Service Table pane, expand all the + tabs to see the completed GATT service Table. It should match as shown:

Click Next to proceed to the LED Setup Tab.
LED0 Setup
In the LED Setup pane, configure P0_2/LED0 output to flash two times per second during advertising (Standby mode), and then turn fully on when a connection is established, as shown:

Click Finish.
Save BM70 Configuration Settings to a File
Press Save to save your settings to a BM70 configuration file (for example C:\Masters\20055\Lab4\bm70-config\bm70-config.txt) as shown :

Click OK to close the final dialog box.
Close UI Config Tool
Close the UI Configuration Tool as shown:

Create BM70 Config EEPROM Table Array
The PIC24 demonstration code simplifies the deployment of BM70 configuration settings by in-circuit-programming the module's configuration EEPROM memory. In this sequence, you will convert your BM70 configuration file into a Flash Configuration Table that can be included in the MPLAB project.
If you have not done so already, download and extract the to your C:\ folder.
Start the BM7x EEPROM Utility, Load the BM70 Configuration File
Launch the BM7x EEPROM Table Utility (found in the "Reference Materials" section above). When prompted, navigate to your saved configuration file from Step 14 above:

Create the BM70 Configuration EEPROM Table in the MPLAB Project Folder
When prompted, save the output file to the PIC24 demo project folder C:\host-firmware\Explorer16 BM70 Pictail Stopwatch.X.

Prepare the BM70 PICtail for use on the Explorer 16 Board
Prepare BM70 PICtail Jumpers
Disconnect the USB cable from the PICtail board. Configure the module for Application mode by moving the dip-switch SW7 to the OFF position. Prepare for connection to Explorer 16 by disconnecting the BM70 UART pins from the MCP2200 (remove J3 jumpers), and finally, set the power source to PIC® (jumper J1) as shown:

Install BM70 PICtail
Install the BM70 PICtail board into the Explorer 16 board as shown (ensure PIC24FJ128GA010 PIM is installed):

Program/Run the PIC24 MCU Stopwatch Demo Project
If not done so already, download and extract the to your C:\ folder
Open the Project
Start MPLAB X and open the project C:\host-firmware\Explorer16 BM70 Pictail Stopwatch.X.
Select the BM70 Project Configuration
Select the BM70 project configuration as shown:

#include the BM70 Configuration EEPROM Table
With your editor, open the bm70_configure.c file. Go to line 57 and change the name of the included BM70 EEPROM Table file to the name you chose in Step 17:

Build/Run the Project
Build/run the project by pressing the Make and Program Device button.
You will first see “Initializing…” text on the LCD display, indicating the initialization of the BM70 parameters, as well as verification of the correct BM70 firmware version (1.06).
On success, the LCD should display the device name, the last four bytes of the MAC address, as well as a stopwatch display.

LED_D3 should also blip two times per second indicating an advertising state.

PIC24 Demo Startup Troubleshooting
The LCD reads “Initialize Error."
This results in the host MCU not receiving any response to the Read Information command or an invalid BM70 fw version being read (not v1.06)
Possible Causes:
- Incorrect PICtail jumper settings: review Step 18.
- Incorrect BM70 firmware: reprogram with v1.06.
- Incorrect BM70 configuration: re-load your saved BM70 UI configuration file and verify the correct settings as described in steps 1 through 15. Re-create the BM70 EEPROM Configuration Table.
- Alternatively, create/deploy the BM70 EEPROM Configuration Table using the provided.
Sanity Check:
To verify the basic functionality of the module, you can revert the PICtail jumpers J3 and J1 for standalone operation (as shown) and use the Manual PatternTest Tool. Note, you may need to jumper UART_RX_IND to GND before the tool will be able to communicate as shown:

Interact With The Service using the Stopwatch App
You will need to research the specific details for the installation of APK application files on your Android device.
Generally, you connect your phone to the PC using the USB cable that came with it, then transfer the APK file over to the device. Next, go to the security settings and enable the installation of apps from "sources other than the Play Store". Finally, simply locate and tap on the APK file to install it.
After installing the app, go to security settings and disable the installation of apps from sources other than the Play Store.
Start The App, Scan for Stopwatch Devices, and Select Device
Start the stopwatch app on your smartphone:

Tap on SCAN to begin scanning for devices as shown:

Locate and tap on your device to establish a connection to it. The Explorer 16 LCD should indicate the connected status. In addition, you should see Explorer 16 LED_D3 latch to an ON state indicating a connected state:

Interact With The Service
Once connected, you will be taken to the main activity page of the app.
Press Start to start the stopwatch from the app.
Press Explorer 16 and switch S3 to Start or Stop the display. Press S6 to reset.
The History pane will show track these events as shown:

Demo Not Working?
Symptoms
The device is connected, however, you cannot start the stopwatch from the app, or you do not receive any updates from the Explorer 16 when pressing S3/S6 buttons.
Causes
The most likely cause is a mismatch between handle values in the BM70 GATT Service Table, vs what is encoded in the PIC24 firmware.
In MPLAB X IDE, open the definitions.h file, and scroll to line 106. Here is where we define the Handle IDs for each characteristic we want to update in our application:

In particular, note the two handles circled. The first is the writable characteristic Stopwatch Control Point (0x8002), and the second is the notify characteristic Stopwatch Status (0x8004).
The handle values for these two characteristics need to match those generated by the UI Configuration tool (see Step 12):

Conclusions
- Private GATT Services are easily created on the BM70 using the UI Configuration tool.
- The BM70 EEPROM Table Utility is used to convert a UI Configuration file to an EEPROM Table that can be embedded into your project, simplifying production deployment.
- The MCU host must capture BLE connection parameters (including Connection Handle) to be able to modify characteristic values in the BM70.
- Care must be taken to embed the correct characteristic handles generated by the tool into the embedded host code.