BM70 Security Features
This page covers Bluetooth® Low Energy security features offered in the BM70 module. You should have a working knowledge of BLE security to gain a complete understanding of the way the BM7x operates and provides security.
Overview
The GAP Layer defines modes and procedures which relate to the security of a connection. The BM70 supports LE Security Mode 1 with four security levels as specified by the definitions in the GAP layer. In general, LE Security Mode 1 gains security by using encryption, and this will only be done after the connection has been established.
To keep it simple, when two connected devices that initially do not have security wish to do something that requires security, the devices must first pair. Pairing involves authenticating the identity of two devices, encrypting the link, and then distributing keys used for encryption (bonding). The diagram below tries to capture what pairing involves. The level of security gained from all this is determined from the pairing method used and this is selected based on the I/O capabilities of each device.

Pairing Methods Supported
BM70 supports the following pairing methods:
- Just Works (unauthenticated)
- Passkey Display (authenticated)
- Numeric Comparison (authenticated)
These methods are supported via the following I/O capability settings, which are available on BM70:
- No Input No Output
- Display Only
- Display Yes/No
- Keyboard Only
- Keyboard Display
The following table determines the pairing method (and thus the security level achieved) based on the BM70 device's capabilities.
Note that in a typical security scenario, the smartphone plays the role of Initiator and since it has both a keyboard and a display, it has a fixed I/O capability (Keyboard Display), while a BM70-based Peripheral device would typically have the ability to Display (Send) a PIN key to the phone for verification (Display Yes/No I/O capability):

Bonding Capability
BM70 is capable of bonding with up to 8 peers. A "link priority" setting is also associated with each key set, indicating how recently the peer was connected with (1 being newest and 8 being oldest).
Applying a Security Level to a Connection
The first step is to establish the desired connection security level for the application.
Next, the characteristic attributes requiring authenticated access need to be configured as such.
Finally, the appropriate BM70 static/dynamic configuration parameters need to be configured in the module to enable a security level change to take place in a connection, and to be automatically applied to all subsequent re-connections.
Flow of Control
The diagram below shows the flow of control between a BM7x (acting as a GATT Server) and a peer device (smartphone, etc.). The BM70 is connected to an MCU Host via the UART interface (BM70-to-Host packets not shown):

Host MCU Interaction with BM70
The status/control messages (packets) that occur between the host and BM7x during the pairing process are based on the type of pairing method selected. The diagram below shows an example of the interaction based on the Passkey Display method with the BM7x being an 'Initiator' or ‘Responder’: