SAMA5D29 Curiosity Board Bare-Metal/MPLAB® Harmony v3 Examples
Last modified by Microchip on 2026/10/27 04:09
| No | Title/Link | Hardware Board/Kit | Description |
|---|---|---|---|
1 | SAMA5D29 Curiosity | Introduction to SAMA5D29 Curiosity Development Board | |
| 2 | SAMA5D29-Curiosity – Features | SAMA5D29 Curiosity | Features of the SAMA5D29 Curiosity Development Board |
| 3 | SAMA5D29-Curiosity – Console Serial Communications | SAMA5D29 Curiosity | Connect a host computer running a terminal emulation program to the SAMA5D29 Curiosity Development Board serial debug port to access the console |
| 4 | Getting Started with the SAMA5D29-Curiosity Board (EV07R15A) | SAMA5D29 Curiosity | Configure the boot sequence to boot from the user-preferred Non-Volatile Memory (NVM) using SAM-BA® ISPP commands for the SAMA5D29-Curiosity board (EV07R15A) |
| 5 | SAMA5D29-Curiosity – Booting Demo Linux Image | SAMA5D29 Curiosity | Boot a demo Linux® image on an microSD™ card |
| 6 | SAMA5D29 Curiosity | SAMA5D29-Curiosity read and write boot configuration word using SAM-BA ISPP | |
| 7 | SAMA5D29-Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SQI™ Flash Memory | SAMA5D29 Curiosity | Configure and build the second stage bootloader to boot an MPLAB® Harmony v3 application from Quad Serial Peripheral Interface (QSPI) (Octa SPI) |
| 8 | SAMA5D29-Curiosity – Configure and Build at91bootstrap for a MPLAB Harmony v3 Project with MPLAB X IDE | SAMA5D29 Curiosity | Configure and build at91bootstrap to debug an MPLAB Harmony v3 project with MPLAB X IDE |
| 9 | SAMA5D29-Curiosity – Configure and Build at91bootstrap to Load a MPLAB Harmony v3 Application from SD Memory Card | SAMA5D29 Curiosity | Configure and build at91bootstrap to load an MPLAB Harmony v3 application from an SD card memory |
| 10 | SAMA5D29-Curiosity – Writing MPLAB Harmony v3 Application and at91bootstrap to SQI™ Flash Memory Using SAM-BA ISPP | SAMA5D29 Curiosity | Write an MPLAB Harmony v3 application and at91bootstrap to a QSPI NOR Flash memory using SAM-BA ISPP |
| 11 | SAMA5D29-Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SD Memory Card | SAMA5D29 Curiosity | Write an MPLAB Harmony v3 application and at91bootstrap to an SD card |
| 12 | SAMA5D29-Curiosity – Getting Started with MPLAB Harmony v3 Development: CSP Application: pio_led_on_off_interrupt | SAMA5D29 Curiosity | Download, configure, and build an MPLAB Harmony v3 software framework application to run on the SAMA7D65-Curiosity kit using MPLAB X IDE |
13 | SAMA5D29 Curiosity | Configure, build, and debug a complementary Pulse-Width Modulation (PWM) application on the SAMA5D29 Curiosity Development Board using MPLAB X IDE | |
| 14 | SAMA5D29 Curiosity | Getting Started on CAN Protocol (CAN-FD) MPLAB Harmony application using MPLAB X IDE on SAMA5D29 Curiosity Development Board | |
| 15 | Application Demo on CAN Protocol (CAN-FD) with LCD on SAMA5D29 Curiosity Development Board | SAMA5D29 Curiosity | MPLAB X IDE-based Harmony application demo on CAN-FD with LCD on SAMA5D29 Curiosity Development Board |
| 16 | SAMA5D29 Curiosity | Explore the process of configuring, building, and debugging a complementary PWM application | |
| 17 | SAMA5D29 Curiosity | Explore the process of configuring, building and debugging a complementary PWM application on the SAMA5D29 Curiosity Development Board using MPLAB X IDE | |
| 18 | eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony V3 (AN5218) | SAM MPUs | Application note describing how to execute a Harmony application from QSPI Flash on board |
| 19 | SAM-BA ISPP | N/A | SAM-BA ISPP and command line interface |