SAMA7D65 Curiosity Board Bare-metal/MPLAB® Harmony v3 Examples

Last modified by Microchip on 2026/10/27 04:11

NoTitle/LinkDescription
1SAMA7D65-Curiosity – Getting Started with MPLAB Harmony v3 Development: RTC ApplicationProvides a step-by-step instruction on how to create an MPLAB® Harmony v3-based Real-Time Clock (RTC) application and debug it
2SAMA7D65 Curiosity Development Board – IntroductionIntroduction to the SAMA7D65 Curiosity Kit
3 SAMA7D65-Curiosity – FeaturesFeatures of the SAMA7D65 Curiosity Kit
4SAMA7D65-Curiosity – Console Serial CommunicationsHow to connect a host computer running a terminal emulation program to the SAMA7D65-Curiosity Kit serial debug port to access the console
5SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NOR Flash (QSPI) MemoryHow to configure and build the second-stage bootloader to boot an MPLAB Harmony v3 application from Quad Serial Peripheral Interface (QSPI) (Octal SPI)
6SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from NAND Flash MemoryHow to configure and build at91bootstrap to load an MPLAB Harmony v3 application from an NAND Flash memory
7SAMA7D65-Curiosity – Configure and Build at91bootstrap to Load an MPLAB Harmony v3 Application from SD Memory CardHow to configure and build at91bootstrap to load an MPLAB Harmony v3 application from SD card memory
8SAMA7D65-Curiosity – Configure and Build at91bootstrap for an MPLAB Harmony v3 Project with MPLAB X IDEHow to configure and build at91bootstrap to debug an MPLAB Harmony v3 project with MPLAB X IDE
9SAMA7D65-Curiosity – Writing MPLAB Harmony v3 Application and at91bootstrap to NAND Flash Memory Using SAM-BA ISPPHow to write an MPLAB Harmony v3 application and at91bootstrap to an NAND Flash memory using SAM-BA® ISPP
10SAMA7D65-Curiosity – Writing MPLAB Harmony v3 Application and at91bootstrap to NOR Flash (QSPI) Memory Using SAM-BA ISPPHow to write an MPLAB Harmony v3 application and at91bootstrap to a QSPI NOR Flash memory using SAM-BA ISPP
11SAMA7D65-Curiosity – Copy MPLAB Harmony v3 Application and at91bootstrap to SD Memory CardHow to write an MPLAB Harmony v3 application and at91bootstrap to an SD card
13Training on how to display the Microchip Graphics Quick Start project template on the AC69T88A - 5" WVGA LVDS Display using the Microchip Graphics Suite (MGS) on the SAMA7D65 Curiosity Kit
14Training on how to download, configure, and build an MPLAB Harmony v3 Software Framework application to run on the SAMA7D65 Curiosity Kit using MPLAB X IDE
15Step-by-step instruction on how to connect the 5.5" MIPI® 720p LCD Display Module to the SAMA7D65 Curiosity Kit
16Step-by-step instructions on how to connect the NewVision 1280x800 10" LVDS LCD Module to the SAMA7D65 Curiosity Kit
17Step-by-step instructions on how to connect the Waveshare® Capacitive Touch Displays for Raspberry Pi®, DSI Interface module to the SAMA7D65 Curiosity Kit
18eXecute-In-Place (XIP) with Serial Flash Memories on MPUs Using MPLAB Harmony v3 (AN5218) Application note describing how to execute an MPLAB Harmony v3 application from QSPI Flash on board
19Power Monitoring (PAC1934) on SAMA7D65 Curiosity Development Board Using an MPLAB Harmony ApplicationLearn how to measure power consumption on the SAMA7D65 Curiosity Development Board using the PAC1934 power monitoring IC
20SAM-BA ISPPSAM-BA ISPP and command line interface

Collaterals